PDK API Guide for J721E
|
This is UDMA driver init, deinit and common API.
Files | |
file | udma.h |
UDMA Driver API/interface file. | |
Data Structures | |
struct | Udma_InitPrms |
UDMA initialization parameters. More... | |
struct | Udma_DrvHandle |
UDMA driver object. More... | |
Functions | |
int32_t | Udma_init (Udma_DrvHandle drvHandle, const Udma_InitPrms *initPrms) |
UDMA init function. More... | |
int32_t | Udma_deinit (Udma_DrvHandle drvHandle) |
UDMA deinit function. More... | |
void | UdmaInitPrms_init (uint32_t instId, Udma_InitPrms *initPrms) |
Udma_InitPrms structure init function. More... | |
static uint64_t | Udma_defaultVirtToPhyFxn (const void *virtAddr, uint32_t chNum, void *appData) |
Default virtual to physical translation function. More... | |
static void * | Udma_defaultPhyToVirtFxn (uint64_t phyAddr, uint32_t chNum, void *appData) |
Default physical to virtual translation function. More... | |
Typedefs | |
typedef uint64_t(* | Udma_VirtToPhyFxn) (const void *virtAddr, uint32_t chNum, void *appData) |
UDMA Virtual to Physical address translation callback function. More... | |
typedef void *(* | Udma_PhyToVirtFxn) (uint64_t phyAddr, uint32_t chNum, void *appData) |
UDMA Physical to Virtual address translation callback function. More... | |
typedef void(* | Udma_PrintFxn) (const char *str) |
UDMA info/debug print function prototype. More... | |
UDMA Ring Local API's function prototypes | |
Function prototypes for various local UDMA Ring API's. For Normal RA / LCDMA RA, function pointers will be used to call the appropriate function. | |
typedef void(* | Udma_ringHandleClearRegsFxn) (Udma_RingHandle ringHandle) |
UDMA Ring handle clear register function protype. More... | |
typedef void(* | Udma_ringSetDoorBellFxn) (Udma_RingHandle ringHandle, int32_t count) |
UDMA Ring set doorbell function protype. More... | |
typedef void(* | Udma_ringPrimeFxn) (Udma_RingHandle ringHandle, uint64_t phyDescMem) |
UDMA Ring prime function protype. More... | |
typedef void(* | Udma_ringPrimeReadFxn) (Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
UDMA Ring prime read function protype. More... | |
typedef void *(* | Udma_ringGetMemPtrFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get mem pointer function protype. More... | |
typedef uint32_t(* | Udma_ringGetModeFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get ring mode function protype. More... | |
typedef uint32_t(* | Udma_ringGetElementCntFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get element count function protype. More... | |
typedef uint32_t(* | Udma_ringGetForwardRingOccFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get forward ring occupancy function protype. More... | |
typedef uint32_t(* | Udma_ringGetReverseRingOccFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get reverse ring occupancy function protype. More... | |
typedef uint32_t(* | Udma_ringGetWrIdxFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get write index value function protype. More... | |
typedef uint32_t(* | Udma_ringGetRdIdxFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get read index value function protype. More... | |
typedef int32_t(* | Udma_ringDequeueRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
UDMA Ring dequeue raw function protype. More... | |
typedef int32_t(* | Udma_ringQueueRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t phyDescMem) |
UDMA Ring queue raw function protype. More... | |
typedef int32_t(* | Udma_ringFlushRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
UDMA Ring flush raw function protype. More... | |
typedef void(* | Udma_ringSetCfgFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, const Udma_RingPrms *ringPrms) |
UDMA Ring set Cfg function protype. More... | |
typedef uint64_t(* Udma_VirtToPhyFxn) (const void *virtAddr, uint32_t chNum, void *appData) |
UDMA Virtual to Physical address translation callback function.
This function is used by the driver to convert virtual address to physical address.
virtAddr | [IN] Virtual address |
chNum | [IN] Channel number passed during channel open |
appData | [IN] Callback pointer passed during channel open |
typedef void*(* Udma_PhyToVirtFxn) (uint64_t phyAddr, uint32_t chNum, void *appData) |
UDMA Physical to Virtual address translation callback function.
This function is used by the driver to convert physical address to virtual address.
phyAddr | [IN] Physical address |
chNum | [IN] Channel number passed during channel open |
appData | [IN] Callback pointer passed during channel open |
typedef void(* Udma_PrintFxn) (const char *str) |
UDMA info/debug print function prototype.
This function is used by the driver to print info/debug messages.
str | [OUT] Info string to print. |
typedef void(* Udma_ringHandleClearRegsFxn) (Udma_RingHandle ringHandle) |
UDMA Ring handle clear register function protype.
typedef void(* Udma_ringSetDoorBellFxn) (Udma_RingHandle ringHandle, int32_t count) |
UDMA Ring set doorbell function protype.
typedef void(* Udma_ringPrimeFxn) (Udma_RingHandle ringHandle, uint64_t phyDescMem) |
UDMA Ring prime function protype.
typedef void(* Udma_ringPrimeReadFxn) (Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
UDMA Ring prime read function protype.
typedef void*(* Udma_ringGetMemPtrFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get mem pointer function protype.
typedef uint32_t(* Udma_ringGetModeFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get ring mode function protype.
typedef uint32_t(* Udma_ringGetElementCntFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get element count function protype.
typedef uint32_t(* Udma_ringGetForwardRingOccFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get forward ring occupancy function protype.
typedef uint32_t(* Udma_ringGetReverseRingOccFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get reverse ring occupancy function protype.
typedef uint32_t(* Udma_ringGetWrIdxFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get write index value function protype.
typedef uint32_t(* Udma_ringGetRdIdxFxn) (Udma_RingHandle ringHandle) |
UDMA Ring get read index value function protype.
typedef int32_t(* Udma_ringDequeueRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
UDMA Ring dequeue raw function protype.
typedef int32_t(* Udma_ringQueueRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t phyDescMem) |
UDMA Ring queue raw function protype.
typedef int32_t(* Udma_ringFlushRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
UDMA Ring flush raw function protype.
typedef void(* Udma_ringSetCfgFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, const Udma_RingPrms *ringPrms) |
UDMA Ring set Cfg function protype.
int32_t Udma_init | ( | Udma_DrvHandle | drvHandle, |
const Udma_InitPrms * | initPrms | ||
) |
UDMA init function.
Initializes the UDMA drivers. This function should be called before calling any of driver API's and should be called only once.
Requirement: DOX_REQ_TAG(PDK-2576)
drvHandle | [IN] UDMA driver handle - static memory needs to allocated by caller. This is used by the driver to maintain the driver states. This cannot be NULL. |
initPrms | [IN] UDMA Initialization parameters. If NULL is passed, the default parameters will be assumed - address translation disabled. |
int32_t Udma_deinit | ( | Udma_DrvHandle | drvHandle | ) |
UDMA deinit function.
Uninitializes the drivers and the hardware and should be called during system shutdown. Should not be called if Udma_init() is not called.
Requirement: DOX_REQ_TAG(PDK-2577)
drvHandle | [IN] UDMA driver handle pointer passed during Udma_init |
void UdmaInitPrms_init | ( | uint32_t | instId, |
Udma_InitPrms * | initPrms | ||
) |
Udma_InitPrms structure init function.
instId | [IN] Udma_InstanceId |
initPrms | [IN] Pointer to Udma_InitPrms structure. |
|
inlinestatic |
Default virtual to physical translation function.
virtAddr | [IN] Virtual address |
chNum | [IN] Channel number passed during channel open. Note: When called for functions which is not channel dependent (like ring alloc), this parameter will be set to UDMA_DMA_CH_INVALID. |
appData | [IN] Callback pointer passed during channel open. Note: When called for functions which is not channel dependent (like ring alloc), this parameter will be set to NULL. |
|
inlinestatic |
Default physical to virtual translation function.
phyAddr | [IN] Physical address |
chNum | [IN] Channel number passed during channel open. Note: When called for functions which is not channel dependent (like ring alloc), this parameter will be set to UDMA_DMA_CH_INVALID. |
appData | [IN] Callback pointer passed during channel open. Note: When called for functions which is not channel dependent (like ring alloc), this parameter will be set to NULL. |