Vision Apps User Guide
APIs
Here is a list of all modules:
[detail level 12]
 Modules for abstracting OpenVX kernel APIsUtility library of modules that provide common set of API's for each OpenVX kernel
 AEWB Node ModuleThis section contains module APIs for the AEWB node tivxAewbNode
 Capture Node ModuleThis section contains module APIs for the TIOVX Capture node tivxHwaCapture
 Display Node ModuleThis section contains module APIs for the TIOVX Display Node tivxHwaDisplay
 LDC Node ModuleThis section contains module APIs for the TIOVX LDC node tivxVpacLdcNode
 MSC HW Mosaic Node ModuleThis section contains module APIs for the MSC HW Mosaic Node tivxImgMosaicNode
 Object Array Split Node ModuleThis section contains module APIs for the Node tivxObjArraySplitNode
 Scaler Node ModuleThis section contains module APIs for the TIOVX Scaler node tivxVpacMscScaleNode
 Sensor ModuleThis section contains module APIs for the image sensor framework
 TIDL Node ModuleThis section contains module APIs for the TIOVX TIDL node tivxTIDLNode
 VISS Node ModuleThis section contains module APIs for the TIOVX VISS node tivxVpacVissNode
 TI defined OpenVX Kernels for Vision AppsTI defined OpenVX Kernels for Vision Apps
 TIVX Example KernelsThis section documents the kernels which are targted to be examples of writing different kernels
 TIVX Kernels for File I/OThis section documents the kernels defined for File I/O
 TIVX Kernels for Image Pre/Post ProcessingThis section documents the kernels defined for Image Pre/Post Processing
 TIVX Kernels for SRVThis section documents the kernels defined for Surroundview processing
 TIVX Kernels for StereoThis section documents the kernels defined for Stereo
 Utility and infrastructure APIsUtility and infrastructure APIs used to create applications and kernels
 (ISP Tuning Tool Server) APIsThis section contains APIs for ISP Tuning Tool Server
 Application Initialization APIsThis section contains APIs for application initialization and de-initialization
 Application RTOS OSAL/DPL APIsThis section contains APIs for providing abstraction between PDK OSAL and MCU+SDK DPL
 Codec Wrapper APIsThis section contains APIs to use CODEC Pipelines within demos
 Display controller remote service APIs (RTOS only)This section contains APIs for display controller remote service
 Display subsystem initialization APIs (RTOS only)This section contains APIs for display initialization
 Font and 2D Drawing APIThis module has the interface for drawing fonts and 2D primitives like lines
 GStreamer Wrapper APIsThis section contains APIs to use GStreamer CODEC Pipelines within demos
 Graphics overlay utility APIsThis section contains APIs to create and draw graphics overlays for demos
 HW accelerator initialization APIs (HLOS only)This section contains APIs for HW accelerator configuration, in particular to configure the frequency of the VPAC and DMPAC from the A-core
 HW accelerator initialization APIs (RTOS only)This section contains APIs for HW accelerator initialization
 ISSThis section contains APIs for ISS
 Inter-processor communication (IPC) APIsThis section contains APIs for Inter-processor communication (IPC)
 Logging APIsThis section contains APIs for logging from remote cores to a central host core which prints all the logs to a common console
 Memory allocation APIsThis section contains APIs for memory allocation
 Miscellaneous utility APIs (RTOS only)This section contains miscellaneous utility APIs
 NetworkCtrl Implementation
 OpenGL APIsThis section contains APIs to use OpenGL within Apps
 OpenMAX Codec Wrapper APIsThis section contains APIs to use OpenMAX CODEC Pipelines within demos
 Performance statistics reporting APIsThese APIs allows user to get performance information of RTOS based remote cores
 Remote Service APIs (RTOS only)These APIs allows user to invoke functions or services on remote cores by abstracting the low level IPC details
 SCICLIENT initialization APIs (RTOS only)This section contains APIs for SCICLIENT initialization
 SCISERVER initialization APIs (RTOS only)This section contains APIs for SCISERVER initialization
 Sensor Initialization API (RTOS only)This section contains APIs for Sensor initialization
 UDMA initialization APIs (RTOS only)This section contains APIs for UDMA initialization