This section contains module APIs for the Node tivxObjArraySplitNode.
◆ app_init_obj_arr_split()
| vx_status app_init_obj_arr_split |
( |
vx_context |
context, |
|
|
ObjArrSplitObj * |
objArrSplitObj, |
|
|
char * |
objName |
|
) |
| |
Obj Arr Split module init helper function.
This obj arr split init helper function will create all the data objects required to create the obj arr split node
- Parameters
-
| [in] | context | OpenVX context which must be created using vxCreateContext |
| [out] | ObjArrSplitObj | Obj Arr Split module object which gets populated with obj arr split node data objects |
| [in] | objName | String of the name of this object |
| [in] | numOutputs | Number of outputs that the input should be split into. The minimum is 2 and maximum is 4 |
◆ app_deinit_obj_arr_split()
Obj Arr Split module deinit helper function.
This obj arr split deinit helper function will release all the data objects created during the app_init_obj_arr_split call
- Parameters
-
| [in,out] | ObjArrSplitObj | Obj Arr Split module object which contains obj arr split node data objects which are released in this function |
◆ app_delete_obj_arr_split()
Obj Arr Split module delete helper function.
This obj arr split delete helper function will delete the obj arr split node that is created during the app_create_graph_obj_arr_split call
- Parameters
-
| [in,out] | objArrSplitObj | Obj Arr Split module object which contains obj arr split node objects which are released in this function |
◆ app_create_graph_obj_arr_split()
| vx_status app_create_graph_obj_arr_split |
( |
vx_graph |
graph, |
|
|
ObjArrSplitObj * |
objArrSplitObj |
|
) |
| |
Obj Arr Split module create helper function.
This obj arr split create helper function will create the node using all the data objects created during the app_init_obj_arr_split call.
- Parameters
-
| [in] | graph | OpenVX graph that has been created using vxCreateGraph and where the obj arr split node is created |
| [in,out] | ObjArrSplitObj | Obj Arr Split module object which contains obj arr split node which is created in this function |