This section documents the kernels which are targted to be examples of writing different kernels.
|
| void | tivxSampleLoadKernels (vx_context context) |
| | Used for the Application to load the sample kernels into the context. More...
|
| |
| void | tivxSampleUnLoadKernels (vx_context context) |
| | Used for the Application to unload the sample kernels from the context. More...
|
| |
| void | tivxSamplePrintPerformance (vx_perf_t performance, uint32_t numPixels, const char *testName) |
| | Used to print the performance of the kernels. More...
|
| |
| VX_API_ENTRY vx_node VX_API_CALL | tivxOpenglMosaicNode (vx_graph graph, vx_user_data_object configuration, vx_object_array input, vx_image output) |
| | [Graph] Creates a OPENGL_MOSAIC Node. More...
|
| |
◆ TIVX_MODULE_NAME_SAMPLE
| #define TIVX_MODULE_NAME_SAMPLE "sample" |
Name for OpenVX Extension kernel module: sample.
◆ TIVX_KERNEL_OPENGL_MOSAIC_NAME
| #define TIVX_KERNEL_OPENGL_MOSAIC_NAME "com.ti.sample.opengl_mosaic" |
The list of kernels supported in sample module.
Each kernel listed here can be used with the vxGetKernelByName call. When programming the parameters, use
VX_INPUT for [in]
VX_OUTPUT for [out]
VX_BIDIRECTIONAL for [in,out]
When programming the parameters, use
VX_TYPE_IMAGE for a vx_image in the size field of vxGetParameterByIndex or vxSetParameterByIndex
VX_TYPE_ARRAY for a vx_array in the size field of vxGetParameterByIndex or vxSetParameterByIndex
- or other appropriate types in vx_type_e.
opengl_mosaic kernel name
◆ TIVX_KERNEL_OPENGL_MOSAIC_TYPE_1x1
| #define TIVX_KERNEL_OPENGL_MOSAIC_TYPE_1x1 (0) |
The configuration data structure used by the TIVX_KERNEL_OPENGL_MOSAIC kernel.
< Mosaic/Render Type - 1x1 (single window) mosaic Mosaic/Render Type - 2x2 (4 window) mosaic
◆ TIVX_KERNEL_OPENGL_MOSAIC_TYPE_2x2
| #define TIVX_KERNEL_OPENGL_MOSAIC_TYPE_2x2 (1) |
◆ tivxSampleLoadKernels()
| void tivxSampleLoadKernels |
( |
vx_context |
context | ) |
|
Used for the Application to load the sample kernels into the context.
◆ tivxSampleUnLoadKernels()
| void tivxSampleUnLoadKernels |
( |
vx_context |
context | ) |
|
Used for the Application to unload the sample kernels from the context.
◆ tivxSamplePrintPerformance()
| void tivxSamplePrintPerformance |
( |
vx_perf_t |
performance, |
|
|
uint32_t |
numPixels, |
|
|
const char * |
testName |
|
) |
| |
Used to print the performance of the kernels.
◆ tivxOpenglMosaicNode()
| VX_API_ENTRY vx_node VX_API_CALL tivxOpenglMosaicNode |
( |
vx_graph |
graph, |
|
|
vx_user_data_object |
configuration, |
|
|
vx_object_array |
input, |
|
|
vx_image |
output |
|
) |
| |
[Graph] Creates a OPENGL_MOSAIC Node.
- Parameters
-
| [in] | graph | The reference to the graph. |
| [in] | configuration | |
| [in] | input | |
| [out] | output | |
- See also
TIVX_KERNEL_OPENGL_MOSAIC_NAME
- Returns
vx_node.
- Return values
-
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |