Task module for the RTOS Porting Interface. More...
#include <stdint.h>#include <stdbool.h>#include <stddef.h>Go to the source code of this file.
Data Structures | |
| struct | TaskP_Params |
| Basic TaskP Parameters. More... | |
Macros | |
| #define | OS_TICKS_IN_MILLI_SEC 1 /* 1000us tick */ |
| Number Ticks by OS in 1 millisecond. More... | |
Typedefs | |
| typedef void * | TaskP_Handle |
| Opaque client reference to an instance of a TaskP. More... | |
| typedef unsigned long | TaskP_Privilege_Mode |
| [SafeRTOS only] Privilege of the task in safertos More... | |
| typedef void(* | TaskP_Fxn) (void *arg0, void *arg1) |
| Prototype for TaskP function. More... | |
Enumerations | |
| enum | TaskP_Status { TaskP_OK = 0 , TaskP_FAILURE = (-(int32_t)1) } |
| Status codes for TaskP APIs. More... | |
Functions | |
| TaskP_Handle | TaskP_create (TaskP_Fxn taskfxn, const TaskP_Params *params) |
| Function to create a task. More... | |
| TaskP_Status | TaskP_delete (TaskP_Handle *handle) |
| Function to delete a task. More... | |
| void | TaskP_Params_init (TaskP_Params *params) |
| Initialize params structure to default values. More... | |
| void | TaskP_sleep (uint32_t timeout) |
| Function for Task sleep in units of OS tick. More... | |
| void | TaskP_sleepInMsecs (uint32_t timeoutInMsecs) |
| Function for Task sleep in units of msecs. More... | |
| void | TaskP_setPrio (TaskP_Handle handle, uint32_t priority) |
| Function to update Task priority. More... | |
| TaskP_Handle | TaskP_self (void) |
| Function returns the Task handle of current task. More... | |
| TaskP_Handle | TaskP_selfmacro (void) |
| Function returns the Task handle of current task.This is an inline function. More... | |
| void | TaskP_yield (void) |
| Function Yield processor to equal priority task. More... | |
| uint32_t | TaskP_isTerminated (TaskP_Handle handle) |
| Check if task is terminated. More... | |
| uint32_t | TaskP_disable (void) |
| Disable the task scheduler. More... | |
| void | TaskP_restore (uint32_t key) |
| Restore Task scheduling state. More... | |
| uint32_t | TaskP_getTaskStackHighWatermark (TaskP_Handle handle) |
| Return the task stack high watermark value (in bytes) More... | |
Task module for the RTOS Porting Interface.
============================================================================