Basic TaskP Parameters. More...
#include <TaskP.h>
Data Fields | |
| const char * | name |
| int8_t | priority |
| uint8_t | padding1 |
| uint16_t | padding2 |
| uint32_t | stacksize |
| void * | pErrBlk |
| void * | arg0 |
| void * | arg1 |
| void * | stack |
| void * | userData |
| TaskP_Privilege_Mode | taskPrivilege |
Basic TaskP Parameters.
Structure that contains the parameters are passed into TaskP_create when creating a TaskP instance.