21 #ifndef DSPLIB_CASCADEBIQUAD_PRIV_H_
22 #define DSPLIB_CASCADEBIQUAD_PRIV_H_
24 #include "../common/DSPLIB_utility.h"
38 #define DSPLIB_CASCADEBIQUAD_PBLOCK_SIZE (6 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
44 #define SE_PARAM_BASE (0x0000)
45 #define SE_SE0_PARAM_OFFSET (SE_PARAM_BASE)
46 #define SE_SE1_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE)
47 #define SE_SA0_PARAM_OFFSET (SE_SE1_PARAM_OFFSET + SE_PARAM_SIZE)
48 #define SE_SA1_PARAM_OFFSET (SE_SA0_PARAM_OFFSET + SE_PARAM_SIZE)
49 #define SE_SA2_PARAM_OFFSET (SE_SA1_PARAM_OFFSET + SE_PARAM_SIZE)
50 #define SE_SA3_PARAM_OFFSET (SE_SA2_PARAM_OFFSET + SE_PARAM_SIZE)
58 void *restrict pFilterCoeff,
59 void *restrict pFilterVar,
92 template <
typename dataType>
130 template <
typename dataType>
163 template <
typename dataType>
166 void *restrict pFilterCoeff,
167 void *restrict pFilterVar,
168 void *restrict pOut);
196 template <
typename dataType>
199 void *restrict pFilterCoeff,
200 void *restrict pFilterVar,
201 void *restrict pOut);
218 template <
typename dataType>
221 void *restrict pFilterCoeff,
222 void *restrict pFilterVar,
223 void *restrict pOut);
251 uint32_t filterCoeffOffset = 0;
#define DSPLIB_CASCADEBIQUAD_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_cascadeBiquad_PrivArgs structure.
DSPLIB_STATUS(* pFxnDSPLIB_cascadeBiquad_exec)(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
This is a function pointer type that conforms to the declaration of DSPLIB_cascadeBiquad_exec_ci and ...
DSPLIB_STATUS DSPLIB_cascadeBiquad_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilterCoeff, const DSPLIB_bufParams2D_t *bufParamsFilterVar, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_cascadeBiquad7Stage_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_cascadeBiquad7Stage_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilterCoeff, const DSPLIB_bufParams2D_t *bufParamsFilterVar, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_cascadeBiquad_init_cn(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsFilterCoeff, DSPLIB_bufParams2D_t *bufParamsFilterVar, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs)
This function is the initialization function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
uint32_t filterCoeff
number of filter coefficients for all stages
uint32_t filterVarPitch
Pitch of filter Variable buffer for different channels DSPLIB_cascadeBiquad_init that will be retriev...
uint32_t dataBufferOutPitch
Pitch of output buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and use...
DSPLIB_cascadeBiquad_InitArgs initArgs
Structure holding initialization parameters
uint32_t dataBufferInPitch
Pitch of input buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and used...
float outGain
b10*b20*b30*... Gain a11, a12 coefficients
pFxnDSPLIB_cascadeBiquad_exec execute
Function pointer to point to the right execution variant between DSPLIB_cascadeBiquad_exec_cn and DSP...