47 #include "../common/c71/DSPLIB_inlines.h"
50 template <
typename dataType>
59 __SE_TEMPLATE_v1 se1Params;
61 __SA_TEMPLATE_v1 sa0Params;
62 __SA_TEMPLATE_v1 sa1Params;
63 __SA_TEMPLATE_v1 sa2Params;
64 __SA_TEMPLATE_v1 sa3Params;
67 uint8_t *pBlock = pKerPrivArgs->
bufPblock;
75 __SE_ELEDUP SE_ELEDUP = __SE_ELEDUP_OFF;
77 typedef typename c7x::make_full_vector<dataType>::type vec;
78 __SE_VECLEN SE_VECLEN = c7x::se_veclen<vec>::value;
79 __SA_VECLEN SA_VECLEN = c7x::sa_veclen<vec>::value;
80 __SE_ELETYPE SE_ELETYPE = c7x::se_eletype<vec>::value;
82 uint32_t eleCount = c7x::element_count_of<vec>::value;
85 printf(
"DSPLIB_DEBUGPRINT Enter DSPLIB_cascadeBiquad7Stage_init_ci\n");
86 printf(
"DSPLIB_DEBUGPRINT SE_VECLEN: %d, SA_VECLEN: %d, SE_ELETYPE: %d numChannels %d numStages %d\n", SE_VECLEN,
87 SA_VECLEN, SE_ELETYPE, numChannels, numStages);
91 SE_ELEDUP = __SE_ELEDUP_16X;
98 printf(
"DSPLIB_DEBUGPRINT SE_VECLEN: %d, SA_VECLEN: %d, SE_ELETYPE: %d SE_ELEDUP %d eleCount %d __SE_ELEDUP_8X %d\n",
99 SE_VECLEN, SA_VECLEN, SE_ELETYPE, SE_ELEDUP, eleCount, __SE_ELEDUP_8X);
102 uint32_t icnt1Param = (numChannels > eleCount) ? eleCount : numChannels;
103 icnt1Param = (icnt1Param == 0) ? 1 : icnt1Param;
104 uint32_t icnt2Param = (numChannels % eleCount == 0) ? (numChannels / eleCount) : (numChannels + eleCount) / eleCount;
109 se1Params = __gen_SE_TEMPLATE_v1();
112 se1Params.ICNT1 = numStages * 2;
113 se1Params.DIM1 = (int32_t) 1;
114 se1Params.ICNT2 = dataSize;
116 se1Params.ICNT3 = icnt2Param;
118 se1Params.ELETYPE = SE_ELETYPE;
119 se1Params.VECLEN = SE_VECLEN;
120 se1Params.DECDIM1_WIDTH = numStages * 2;
121 se1Params.DECDIM1 = __SE_DECDIM_DIM1;
122 se1Params.ELEDUP = SE_ELEDUP;
123 se1Params.DIMFMT = __SE_DIMFMT_4D;
128 sa2Params = __gen_SA_TEMPLATE_v1();
130 sa2Params.ICNT0 = icnt1Param;
131 sa2Params.ICNT1 = dataSize;
132 sa2Params.DIM1 = (int32_t) dataBufferInPitch;
133 sa2Params.ICNT2 = icnt2Param;
134 sa2Params.DIM2 = eleCount;
135 sa2Params.VECLEN = SA_VECLEN;
136 sa2Params.DECDIM1_WIDTH = numChannels;
137 sa2Params.DECDIM1 = __SA_DECDIM_DIM2;
138 sa2Params.DIMFMT = __SA_DIMFMT_3D;
143 sa3Params = __gen_SA_TEMPLATE_v1();
145 sa3Params.ICNT0 = icnt1Param;
146 sa3Params.ICNT1 = numStages * 2;
147 sa3Params.DIM1 = (int32_t) filterVarPitch;
148 sa3Params.ICNT2 = icnt2Param;
149 sa3Params.DIM2 = eleCount;
150 sa3Params.VECLEN = SA_VECLEN;
151 sa3Params.DECDIM1_WIDTH = numChannels;
152 sa3Params.DECDIM1 = __SA_DECDIM_DIM2;
153 sa3Params.DIMFMT = __SA_DIMFMT_3D;
158 sa0Params = __gen_SA_TEMPLATE_v1();
160 sa0Params.ICNT0 = icnt1Param;
161 sa0Params.ICNT1 = dataSize;
162 sa0Params.DIM1 = (int32_t) dataBufferOutPitch;
163 sa0Params.ICNT2 = icnt2Param;
164 sa0Params.DIM2 = eleCount;
165 sa0Params.DECDIM1_WIDTH = numChannels;
166 sa0Params.DECDIM1 = __SA_DECDIM_DIM2;
167 sa0Params.DECDIM2_WIDTH = dataBufferOutPitch * dataSize;
168 sa0Params.DECDIM2 = __SA_DECDIM_DIM2;
169 sa0Params.VECLEN = SA_VECLEN;
170 sa0Params.DIMFMT = __SA_DIMFMT_3D;
175 sa1Params = __gen_SA_TEMPLATE_v1();
177 sa1Params.ICNT0 = icnt1Param;
178 sa1Params.ICNT1 = numStages * 2;
179 sa1Params.DIM1 = (int32_t) filterVarPitch;
180 sa1Params.ICNT2 = icnt2Param;
181 sa1Params.DIM2 = eleCount;
182 sa1Params.DECDIM1_WIDTH = numChannels;
183 sa1Params.DECDIM1 = __SA_DECDIM_DIM2;
184 sa1Params.VECLEN = SA_VECLEN;
185 sa1Params.DIMFMT = __SA_DIMFMT_3D;
208 template <
typename dataType>
211 void *restrict pFilterCoeff,
212 void *restrict pFilterVar,
215 __SE_TEMPLATE_v1 se0Params;
216 __SA_TEMPLATE_v1 sa0Params;
217 __SA_TEMPLATE_v1 sa1Params;
218 __SA_TEMPLATE_v1 sa2Params;
219 __SA_TEMPLATE_v1 sa3Params;
222 uint8_t *pBlock = pKerPrivArgs->
bufPblock;
228 dataType *pInLocal = (dataType *) pIn;
229 dataType *pFilterCoeffLocal = (dataType *) pFilterCoeff;
230 dataType *pFilterVarLocal = (dataType *) pFilterVar;
231 dataType *pOutLocal = (dataType *) pOut;
233 #if DSPLIB_DEBUGPRINT
234 printf(
"Enter DSPLIB_cascadeBiquad7Stage_exec_ci\n");
237 typedef typename c7x::make_full_vector<dataType>::type vec;
239 int eleCount = c7x::element_count_of<vec>::value;
243 vec outGain = (vec) (pKerPrivArgs->
outGain);
245 #if DSPLIB_DEBUGPRINT
246 printf(
"Enter pFilterCoeffLocal %p pFilterVarLocal %p\n", pFilterCoeffLocal, pFilterVarLocal);
251 __SE1_OPEN(pFilterCoeffLocal, se0Params);
252 int32_t offset = ((numStages * 5 + eleCount) / eleCount) * eleCount;
253 __SE0_OPEN(pFilterCoeffLocal + offset, se0Params);
257 __SA0_OPEN(sa0Params);
261 __SA1_OPEN(sa1Params);
265 __SA2_OPEN(sa2Params);
269 __SA3_OPEN(sa3Params);
271 #if DSPLIB_DEBUGPRINT
272 printf(
"DSPLIB_DEBUGPRINT dataSize %d numChannels %d numStages %d pFilterVarLocal %p\n", dataSize, numChannels,
273 numStages, pFilterVarLocal);
276 vec output1, output2, output3;
277 vec output4, output5, output6, output7, output8, output9;
278 vec temp1_mul_1, temp0_mul_1, d0_temp_1, d1_mul_1;
279 vec temp1_mul_2, temp0_mul_2, d0_temp_2, d1_mul_2;
280 vec temp1_mul_3, temp0_mul_3, d0_temp_3, d1_mul_3;
281 vec temp1_mul_4, temp0_mul_4, d0_temp_4, d1_mul_4;
282 vec temp1_mul_5, temp0_mul_5, d0_temp_5, d1_mul_5;
283 vec temp1_mul_6, temp0_mul_6, d0_temp_6, d1_mul_6;
284 vec temp1_mul_7, temp0_mul_7, d0_temp_7, d1_mul_7;
285 vec temp1_mul_8, temp0_mul_8, d0_temp_8, d1_mul_8;
286 vec temp1_mul_9, temp0_mul_9, d0_temp_9, d1_mul_9;
287 vec temp1_add_1, temp1_add_2, temp1_add_3;
288 vec temp1_add_4, temp1_add_5, temp1_add_6, temp1_add_7, temp1_add_8, temp1_add_9;
290 vec b11_a11, b21_a21, b31_a31, b41_a41, b51_a51, b61_a61, b71_a71, b81_a81, b91_a91;
291 vec b12_a12, b22_a22, b32_a32, b42_a42, b52_a52, b62_a62, b72_a72, b82_a82, b92_a92;
292 vec a11, a12, a22, a21, a31, a32, a41, a42, a51, a52, a61, a62, a71, a72, a81, a82, a91, a92;
294 #if DSPLIB_DEBUGPRINT
306 for (uint32_t chCount = 0; chCount < numChannels; chCount += eleCount) {
308 __vpred filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
309 vec *VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
310 vec filtVars_d0_1 = __vload_pred(filtVars, VB4);
311 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
312 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
313 vec filtVars_d1_1 = __vload_pred(filtVars, VB4);
315 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
316 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
317 vec filtVars_d0_2 = __vload_pred(filtVars, VB4);
318 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
319 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
320 vec filtVars_d1_2 = __vload_pred(filtVars, VB4);
322 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
323 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
324 vec filtVars_d0_3 = __vload_pred(filtVars, VB4);
325 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
326 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
327 vec filtVars_d1_3 = __vload_pred(filtVars, VB4);
329 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
330 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
331 vec filtVars_d0_4 = __vload_pred(filtVars, VB4);
332 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
333 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
334 vec filtVars_d1_4 = __vload_pred(filtVars, VB4);
336 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
337 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
338 vec filtVars_d0_5 = __vload_pred(filtVars, VB4);
339 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
340 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
341 vec filtVars_d1_5 = __vload_pred(filtVars, VB4);
343 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
344 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
345 vec filtVars_d0_6 = __vload_pred(filtVars, VB4);
346 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
347 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
348 vec filtVars_d1_6 = __vload_pred(filtVars, VB4);
350 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
351 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
352 vec filtVars_d0_7 = __vload_pred(filtVars, VB4);
353 filtVars = c7x::strm_agen<3, c7x::float_vec>::get_vpred();
354 VB4 = c7x::strm_agen<3, c7x::float_vec>::get_adv(pFilterVarLocal);
355 vec filtVars_d1_7 = __vload_pred(filtVars, VB4);
357 #if DSPLIB_DEBUGPRINT
358 DSPLIB_debugPrintVector(filtVars_d0_1);
359 DSPLIB_debugPrintVector(filtVars_d1_1);
360 DSPLIB_debugPrintVector(filtVars_d0_2);
361 DSPLIB_debugPrintVector(filtVars_d1_2);
362 DSPLIB_debugPrintVector(filtVars_d0_3);
363 DSPLIB_debugPrintVector(filtVars_d1_3);
364 DSPLIB_debugPrintVector(filtVars_d0_4);
365 DSPLIB_debugPrintVector(filtVars_d1_4);
366 DSPLIB_debugPrintVector(filtVars_d0_5);
367 DSPLIB_debugPrintVector(filtVars_d1_5);
368 DSPLIB_debugPrintVector(filtVars_d0_6);
369 DSPLIB_debugPrintVector(filtVars_d1_6);
370 DSPLIB_debugPrintVector(filtVars_d0_7);
371 DSPLIB_debugPrintVector(filtVars_d1_7);
373 for (uint32_t samp = 0; samp < dataSize; samp++) {
375 __vpred tmpld = c7x::strm_agen<2, c7x::float_vec>::get_vpred();
376 c7x::float_vec *VB3 = c7x::strm_agen<2, c7x::float_vec>::get_adv(pInLocal);
377 c7x::float_vec tmp2 = __vload_pred(tmpld, VB3);
379 output1 = tmp2 + filtVars_d0_1;
380 b11_a11 = c7x::strm_eng<1, vec>::get_adv();
382 temp1_mul_1 = tmp2 * b11_a11;
383 temp1_add_1 = temp1_mul_1 + filtVars_d1_1;
384 a12 = c7x::strm_eng<0, vec>::get_adv();
385 temp0_mul_1 = a12 * filtVars_d0_1;
386 a11 = c7x::strm_eng<0, vec>::get_adv();
387 d0_temp_1 = a11 * filtVars_d0_1;
388 filtVars_d0_1 = d0_temp_1 + temp1_add_1;
389 b12_a12 = c7x::strm_eng<1, vec>::get_adv();
390 d1_mul_1 = b12_a12 * tmp2;
391 filtVars_d1_1 = d1_mul_1 + temp0_mul_1;
393 #if DSPLIB_DEBUGPRINT
395 DSPLIB_debugPrintVector(tmp2);
396 DSPLIB_debugPrintVector(b11_a11);
397 DSPLIB_debugPrintVector(b12_a12);
398 DSPLIB_debugPrintVector(a12);
399 DSPLIB_debugPrintVector(a11);
400 DSPLIB_debugPrintVector(temp1_add_1);
401 DSPLIB_debugPrintVector(temp0_mul_1);
402 DSPLIB_debugPrintVector(filtVars_d0_1);
403 DSPLIB_debugPrintVector(filtVars_d1_1);
407 output2 = output1 + filtVars_d0_2;
408 b21_a21 = c7x::strm_eng<1, vec>::get_adv();
409 temp1_mul_2 = b21_a21 * output1;
410 temp1_add_2 = temp1_mul_2 + filtVars_d1_2;
411 a22 = c7x::strm_eng<0, vec>::get_adv();
412 temp0_mul_2 = a22 * filtVars_d0_2;
413 a21 = c7x::strm_eng<0, vec>::get_adv();
414 d0_temp_2 = a21 * filtVars_d0_2;
415 filtVars_d0_2 = d0_temp_2 + temp1_add_2;
416 b22_a22 = c7x::strm_eng<1, vec>::get_adv();
417 d1_mul_2 = b22_a22 * output1;
418 filtVars_d1_2 = d1_mul_2 + temp0_mul_2;
421 output3 = output2 + filtVars_d0_3;
422 b31_a31 = c7x::strm_eng<1, vec>::get_adv();
423 temp1_mul_3 = b31_a31 * output2;
424 temp1_add_3 = temp1_mul_3 + filtVars_d1_3;
425 a32 = c7x::strm_eng<0, vec>::get_adv();
426 temp0_mul_3 = a32 * filtVars_d0_3;
427 a31 = c7x::strm_eng<0, vec>::get_adv();
428 d0_temp_3 = a31 * filtVars_d0_3;
429 filtVars_d0_3 = d0_temp_3 + temp1_add_3;
430 b32_a32 = c7x::strm_eng<1, vec>::get_adv();
431 d1_mul_3 = b32_a32 * output2;
432 filtVars_d1_3 = d1_mul_3 + temp0_mul_3;
435 output4 = output3 + filtVars_d0_4;
436 b41_a41 = c7x::strm_eng<1, vec>::get_adv();
437 temp1_mul_4 = b41_a41 * output3;
438 temp1_add_4 = temp1_mul_4 + filtVars_d1_4;
439 a42 = c7x::strm_eng<0, vec>::get_adv();
440 temp0_mul_4 = a42 * filtVars_d0_4;
441 a41 = c7x::strm_eng<0, vec>::get_adv();
442 d0_temp_4 = a41 * filtVars_d0_4;
443 filtVars_d0_4 = d0_temp_4 + temp1_add_4;
444 b42_a42 = c7x::strm_eng<1, vec>::get_adv();
445 d1_mul_4 = b42_a42 * output3;
446 filtVars_d1_4 = d1_mul_4 + temp0_mul_4;
449 output5 = output4 + filtVars_d0_5;
450 b51_a51 = c7x::strm_eng<1, vec>::get_adv();
451 temp1_mul_5 = b51_a51 * output4;
452 temp1_add_5 = temp1_mul_5 + filtVars_d1_5;
453 a52 = c7x::strm_eng<0, vec>::get_adv();
454 temp0_mul_5 = a52 * filtVars_d0_5;
455 a51 = c7x::strm_eng<0, vec>::get_adv();
456 d0_temp_5 = a51 * filtVars_d0_5;
457 filtVars_d0_5 = d0_temp_5 + temp1_add_5;
458 b52_a52 = c7x::strm_eng<1, vec>::get_adv();
459 d1_mul_5 = b52_a52 * output4;
460 filtVars_d1_5 = d1_mul_5 + temp0_mul_5;
463 output6 = output5 + filtVars_d0_6;
464 b61_a61 = c7x::strm_eng<1, vec>::get_adv();
465 temp1_mul_6 = b61_a61 * output5;
466 temp1_add_6 = temp1_mul_6 + filtVars_d1_6;
467 a62 = c7x::strm_eng<0, vec>::get_adv();
468 temp0_mul_6 = a62 * filtVars_d0_6;
469 a61 = c7x::strm_eng<0, vec>::get_adv();
470 d0_temp_6 = a61 * filtVars_d0_6;
471 filtVars_d0_6 = d0_temp_6 + temp1_add_6;
472 b62_a62 = c7x::strm_eng<1, vec>::get_adv();
473 d1_mul_6 = b62_a62 * output5;
474 filtVars_d1_6 = d1_mul_6 + temp0_mul_6;
477 output7 = output6 + filtVars_d0_7;
478 b71_a71 = c7x::strm_eng<1, vec>::get_adv();
479 temp1_mul_7 = b71_a71 * output6;
480 temp1_add_7 = temp1_mul_7 + filtVars_d1_7;
481 a72 = c7x::strm_eng<0, vec>::get_adv();
482 temp0_mul_7 = a72 * filtVars_d0_7;
483 a71 = c7x::strm_eng<0, vec>::get_adv();
484 d0_temp_7 = a71 * filtVars_d0_7;
485 filtVars_d0_7 = d0_temp_7 + temp1_add_7;
486 b72_a72 = c7x::strm_eng<1, vec>::get_adv();
487 d1_mul_7 = b72_a72 * output6;
488 filtVars_d1_7 = d1_mul_7 + temp0_mul_7;
490 vec output = output7 * outGain;
491 __vpred tmp = c7x::strm_agen<0, vec>::get_vpred();
492 vec *VB1 = c7x::strm_agen<0, vec>::get_adv(pOutLocal);
493 __vstore_pred(tmp, VB1, output);
494 #if DSPLIB_DEBUGPRINT
496 DSPLIB_debugPrintVector(tmp2);
497 DSPLIB_debugPrintVector(output1);
498 DSPLIB_debugPrintVector(output2);
499 DSPLIB_debugPrintVector(output3);
500 DSPLIB_debugPrintVector(output7);
509 __vpred tmp1 = c7x::strm_agen<1, vec>::get_vpred();
510 vec *VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
511 __vstore_pred(tmp1, VB2, filtVars_d0_1);
513 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
514 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
515 __vstore_pred(tmp1, VB2, filtVars_d1_1);
517 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
518 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
519 __vstore_pred(tmp1, VB2, filtVars_d0_2);
521 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
522 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
523 __vstore_pred(tmp1, VB2, filtVars_d1_2);
525 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
526 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
527 __vstore_pred(tmp1, VB2, filtVars_d0_3);
529 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
530 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
531 __vstore_pred(tmp1, VB2, filtVars_d1_3);
533 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
534 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
535 __vstore_pred(tmp1, VB2, filtVars_d0_4);
537 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
538 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
539 __vstore_pred(tmp1, VB2, filtVars_d1_4);
541 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
542 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
543 __vstore_pred(tmp1, VB2, filtVars_d0_5);
545 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
546 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
547 __vstore_pred(tmp1, VB2, filtVars_d1_5);
549 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
550 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
551 __vstore_pred(tmp1, VB2, filtVars_d0_6);
553 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
554 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
555 __vstore_pred(tmp1, VB2, filtVars_d1_6);
557 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
558 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
559 __vstore_pred(tmp1, VB2, filtVars_d0_7);
561 tmp1 = c7x::strm_agen<1, vec>::get_vpred();
562 VB2 = c7x::strm_agen<1, vec>::get_adv(pFilterVarLocal);
563 __vstore_pred(tmp1, VB2, filtVars_d1_7);
575 void *restrict pFilterCoeff,
576 void *restrict pFilterVar,
577 void *restrict pOut);
#define SE_SA0_PARAM_OFFSET
#define SE_SE1_PARAM_OFFSET
template DSPLIB_STATUS DSPLIB_cascadeBiquad7Stage_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilterCoeff, const DSPLIB_bufParams2D_t *bufParamsFilterVar, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_cascadeBiquad7Stage_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
template DSPLIB_STATUS DSPLIB_cascadeBiquad7Stage_exec_ci< float >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
DSPLIB_STATUS DSPLIB_cascadeBiquad7Stage_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilterCoeff, const DSPLIB_bufParams2D_t *bufParamsFilterVar, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_cascadeBiquad.
#define SE_SA2_PARAM_OFFSET
#define SE_SA3_PARAM_OFFSET
#define SE_SA1_PARAM_OFFSET
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
uint32_t dataSize
Size of input data
uint32_t numChannels
number of channels
uint32_t numStages
Size of batch in terms of number of channels of input data
Structure that is reserved for internal use by the kernel.
uint8_t bufPblock[DSPLIB_CASCADEBIQUAD_PBLOCK_SIZE]
uint32_t filterVarPitch
Pitch of filter Variable buffer for different channels DSPLIB_cascadeBiquad_init that will be retriev...
uint32_t dataBufferOutPitch
Pitch of output buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and use...
DSPLIB_cascadeBiquad_InitArgs initArgs
Structure holding initialization parameters
uint32_t dataBufferInPitch
Pitch of input buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and used...
float outGain
b10*b20*b30*... Gain a11, a12 coefficients