![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 228 of file DSPLIB_cascadeBiquad_priv.h.
Data Fields | |
| DSPLIB_cascadeBiquad_InitArgs | initArgs |
| Structure holding initialization parameters More... | |
| pFxnDSPLIB_cascadeBiquad_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_cascadeBiquad_exec_cn and DSPLIB_cascadeBiquad_exec_ci. More... | |
| uint32_t | dataBufferInPitch |
| Pitch of input buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and used by DSPLIB_cascadeBiquad_exec More... | |
| uint32_t | dataBufferOutPitch |
| Pitch of output buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and used by DSPLIB_cascadeBiquad_exec More... | |
| uint32_t | filterVarPitch |
| Pitch of filter Variable buffer for different channels DSPLIB_cascadeBiquad_init that will be retrieved and used by DSPLIB_cascadeBiquad_exec More... | |
| uint32_t | filterCoeff |
| number of filter coefficients for all stages More... | |
| uint32_t | filterCoeffOffset = 0 |
| number of filter coefficients offset between b11_a11, b12_a12 and a11, a12 coefficients More... | |
| float | outGain |
| b10*b20*b30*... Gain a11, a12 coefficients More... | |
| uint8_t | bufPblock [DSPLIB_CASCADEBIQUAD_PBLOCK_SIZE] |
| DSPLIB_cascadeBiquad_InitArgs DSPLIB_cascadeBiquad_PrivArgs::initArgs |
Structure holding initialization parameters
Definition at line 230 of file DSPLIB_cascadeBiquad_priv.h.
| pFxnDSPLIB_cascadeBiquad_exec DSPLIB_cascadeBiquad_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_cascadeBiquad_exec_cn and DSPLIB_cascadeBiquad_exec_ci.
Definition at line 234 of file DSPLIB_cascadeBiquad_priv.h.
| uint32_t DSPLIB_cascadeBiquad_PrivArgs::dataBufferInPitch |
Pitch of input buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and used by DSPLIB_cascadeBiquad_exec
Definition at line 238 of file DSPLIB_cascadeBiquad_priv.h.
| uint32_t DSPLIB_cascadeBiquad_PrivArgs::dataBufferOutPitch |
Pitch of output buffer for different batches DSPLIB_cascadeBiquad_init that will be retrieved and used by DSPLIB_cascadeBiquad_exec
Definition at line 242 of file DSPLIB_cascadeBiquad_priv.h.
| uint32_t DSPLIB_cascadeBiquad_PrivArgs::filterVarPitch |
Pitch of filter Variable buffer for different channels DSPLIB_cascadeBiquad_init that will be retrieved and used by DSPLIB_cascadeBiquad_exec
Definition at line 246 of file DSPLIB_cascadeBiquad_priv.h.
| uint32_t DSPLIB_cascadeBiquad_PrivArgs::filterCoeff |
number of filter coefficients for all stages
Definition at line 248 of file DSPLIB_cascadeBiquad_priv.h.
| uint32_t DSPLIB_cascadeBiquad_PrivArgs::filterCoeffOffset = 0 |
number of filter coefficients offset between b11_a11, b12_a12 and a11, a12 coefficients
Definition at line 251 of file DSPLIB_cascadeBiquad_priv.h.
| float DSPLIB_cascadeBiquad_PrivArgs::outGain |
b10*b20*b30*... Gain a11, a12 coefficients
Definition at line 254 of file DSPLIB_cascadeBiquad_priv.h.
| uint8_t DSPLIB_cascadeBiquad_PrivArgs::bufPblock[DSPLIB_CASCADEBIQUAD_PBLOCK_SIZE] |
Definition at line 256 of file DSPLIB_cascadeBiquad_priv.h.