![]() |
![]() |
TI-RTOS Drivers
tidrivers_msp43x_2_16_00_08
|
![]() |
Macros | |
#define | NVS_STATUS_SUCCESS 0 |
Successful status code returned by NVS_control(). More... | |
#define | NVS_STATUS_ERROR -1 |
Generic error status code returned by NVS_control(). More... | |
#define | NVS_STATUS_UNDEFINEDCMD -2 |
An error status code returned by NVS_control() for undefined command codes. More... | |
NVS_STATUS_* macros are general status codes returned by NVS_control()
#define NVS_STATUS_SUCCESS 0 |
Successful status code returned by NVS_control().
NVS_control() returns NVS_STATUS_SUCCESS if the control code was executed successfully.
#define NVS_STATUS_ERROR -1 |
Generic error status code returned by NVS_control().
NVS_control() returns NVS_STATUS_ERROR if the control code was not executed successfully.
#define NVS_STATUS_UNDEFINEDCMD -2 |
An error status code returned by NVS_control() for undefined command codes.
NVS_control() returns NVS_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.