TI-RTOS Drivers  tidrivers_msp43x_2_16_00_08
ff.h
Go to the documentation of this file.
1 /*---------------------------------------------------------------------------/
2 / FatFs - FAT file system module include R0.11a (C)ChaN, 2015
3 /----------------------------------------------------------------------------/
4 / FatFs module is a free software that opened under license policy of
5 / following conditions.
6 /
7 / Copyright (C) 2015, ChaN, all right reserved.
8 /
9 / 1. Redistributions of source code must retain the above copyright notice,
10 / this condition and the following disclaimer.
11 /
12 / This software is provided by the copyright holder and contributors "AS IS"
13 / and any warranties related to this software are DISCLAIMED.
14 / The copyright owner or contributors be NOT LIABLE for any damages caused
15 / by use of this software.
16 /---------------------------------------------------------------------------*/
17 
18 
19 #ifndef _FATFS
20 #define _FATFS 64180 /* Revision ID */
21 
22 #ifdef __cplusplus
23 extern "C" {
24 #endif
25 
26 #include "integer.h" /* Basic integer types */
27 #include "ffconf.h" /* FatFs configuration options */
28 #if _FATFS != _FFCONF
29 #error Wrong configuration file (ffconf.h).
30 #endif
31 
32 
33 
34 /* Definitions of volume management */
35 
36 #if _MULTI_PARTITION /* Multiple partition configuration */
37 typedef struct {
38  BYTE pd; /* Physical drive number */
39  BYTE pt; /* Partition: 0:Auto detect, 1-4:Forced partition) */
40 } PARTITION;
41 extern PARTITION VolToPart[]; /* Volume - Partition resolution table */
42 #define LD2PD(vol) (VolToPart[vol].pd) /* Get physical drive number */
43 #define LD2PT(vol) (VolToPart[vol].pt) /* Get partition index */
44 
45 #else /* Single partition configuration */
46 #define LD2PD(vol) (BYTE)(vol) /* Each logical drive is bound to the same physical drive number */
47 #define LD2PT(vol) 0 /* Find first valid partition or in SFD */
48 
49 #endif
50 
51 
52 
53 /* Type of path name strings on FatFs API */
54 
55 #if _LFN_UNICODE /* Unicode string */
56 #if !_USE_LFN
57 #error _LFN_UNICODE must be 0 at non-LFN cfg.
58 #endif
59 #ifndef _INC_TCHAR
60 typedef WCHAR TCHAR;
61 #define _T(x) L ## x
62 #define _TEXT(x) L ## x
63 #endif
64 
65 #else /* ANSI/OEM string */
66 #ifndef _INC_TCHAR
67 typedef char TCHAR;
68 #define _T(x) x
69 #define _TEXT(x) x
70 #endif
71 
72 #endif
73 
74 
75 
76 /* File system object structure (FATFS) */
77 
78 typedef struct {
79  BYTE fs_type; /* FAT sub-type (0:Not mounted) */
80  BYTE drv; /* Physical drive number */
81  BYTE csize; /* Sectors per cluster (1,2,4...128) */
82  BYTE n_fats; /* Number of FAT copies (1 or 2) */
83  BYTE wflag; /* win[] flag (b0:dirty) */
84  BYTE fsi_flag; /* FSINFO flags (b7:disabled, b0:dirty) */
85  WORD id; /* File system mount ID */
86  WORD n_rootdir; /* Number of root directory entries (FAT12/16) */
87 #if _MAX_SS != _MIN_SS
88  WORD ssize; /* Bytes per sector (512, 1024, 2048 or 4096) */
89 #endif
90 #if _FS_REENTRANT
91  _SYNC_t sobj; /* Identifier of sync object */
92 #endif
93 #if !_FS_READONLY
94  DWORD last_clust; /* Last allocated cluster */
95  DWORD free_clust; /* Number of free clusters */
96 #endif
97 #if _FS_RPATH
98  DWORD cdir; /* Current directory start cluster (0:root) */
99 #endif
100  DWORD n_fatent; /* Number of FAT entries, = number of clusters + 2 */
101  DWORD fsize; /* Sectors per FAT */
102  DWORD volbase; /* Volume start sector */
103  DWORD fatbase; /* FAT start sector */
104  DWORD dirbase; /* Root directory start sector (FAT32:Cluster#) */
105  DWORD database; /* Data start sector */
106  DWORD winsect; /* Current sector appearing in the win[] */
107  BYTE win[_MAX_SS]; /* Disk access window for Directory, FAT (and file data at tiny cfg) */
108 } FATFS;
109 
110 
111 
112 /* File object structure (FIL) */
113 
114 typedef struct {
115  FATFS* fs; /* Pointer to the related file system object (**do not change order**) */
116  WORD id; /* Owner file system mount ID (**do not change order**) */
117  BYTE flag; /* Status flags */
118  BYTE err; /* Abort flag (error code) */
119  DWORD fptr; /* File read/write pointer (Zeroed on file open) */
120  DWORD fsize; /* File size */
121  DWORD sclust; /* File start cluster (0:no cluster chain, always 0 when fsize is 0) */
122  DWORD clust; /* Current cluster of fpter (not valid when fprt is 0) */
123  DWORD dsect; /* Sector number appearing in buf[] (0:invalid) */
124 #if !_FS_READONLY
125  DWORD dir_sect; /* Sector number containing the directory entry */
126  BYTE* dir_ptr; /* Pointer to the directory entry in the win[] */
127 #endif
128 #if _USE_FASTSEEK
129  DWORD* cltbl; /* Pointer to the cluster link map table (Nulled on file open) */
130 #endif
131 #if _FS_LOCK
132  UINT lockid; /* File lock ID origin from 1 (index of file semaphore table Files[]) */
133 #endif
134 #if !_FS_TINY
135  BYTE buf[_MAX_SS]; /* File private data read/write window */
136 #endif
137 } FIL;
138 
139 
140 
141 /* Directory object structure (DIR) */
142 
143 typedef struct {
144  FATFS* fs; /* Pointer to the owner file system object (**do not change order**) */
145  WORD id; /* Owner file system mount ID (**do not change order**) */
146  WORD index; /* Current read/write index number */
147  DWORD sclust; /* Table start cluster (0:Root dir) */
148  DWORD clust; /* Current cluster */
149  DWORD sect; /* Current sector */
150  BYTE* dir; /* Pointer to the current SFN entry in the win[] */
151  BYTE* fn; /* Pointer to the SFN (in/out) {file[8],ext[3],status[1]} */
152 #if _FS_LOCK
153  UINT lockid; /* File lock ID (index of file semaphore table Files[]) */
154 #endif
155 #if _USE_LFN
156  WCHAR* lfn; /* Pointer to the LFN working buffer */
157  WORD lfn_idx; /* Last matched LFN index number (0xFFFF:No LFN) */
158 #endif
159 #if _USE_FIND
160  const TCHAR* pat; /* Pointer to the name matching pattern */
161 #endif
162 } DIR;
163 
164 
165 
166 /* File information structure (FILINFO) */
167 
168 typedef struct {
169  DWORD fsize; /* File size */
170  WORD fdate; /* Last modified date */
171  WORD ftime; /* Last modified time */
172  BYTE fattrib; /* Attribute */
173  TCHAR fname[13]; /* Short file name (8.3 format) */
174 #if _USE_LFN
175  TCHAR* lfname; /* Pointer to the LFN buffer */
176  UINT lfsize; /* Size of LFN buffer in TCHAR */
177 #endif
178 } FILINFO;
179 
180 
181 
182 /* File function return code (FRESULT) */
183 
184 typedef enum {
185  FR_OK = 0, /* (0) Succeeded */
186  FR_DISK_ERR, /* (1) A hard error occurred in the low level disk I/O layer */
187  FR_INT_ERR, /* (2) Assertion failed */
188  FR_NOT_READY, /* (3) The physical drive cannot work */
189  FR_NO_FILE, /* (4) Could not find the file */
190  FR_NO_PATH, /* (5) Could not find the path */
191  FR_INVALID_NAME, /* (6) The path name format is invalid */
192  FR_DENIED, /* (7) Access denied due to prohibited access or directory full */
193  FR_EXIST, /* (8) Access denied due to prohibited access */
194  FR_INVALID_OBJECT, /* (9) The file/directory object is invalid */
195  FR_WRITE_PROTECTED, /* (10) The physical drive is write protected */
196  FR_INVALID_DRIVE, /* (11) The logical drive number is invalid */
197  FR_NOT_ENABLED, /* (12) The volume has no work area */
198  FR_NO_FILESYSTEM, /* (13) There is no valid FAT volume */
199  FR_MKFS_ABORTED, /* (14) The f_mkfs() aborted due to any parameter error */
200  FR_TIMEOUT, /* (15) Could not get a grant to access the volume within defined period */
201  FR_LOCKED, /* (16) The operation is rejected according to the file sharing policy */
202  FR_NOT_ENOUGH_CORE, /* (17) LFN working buffer could not be allocated */
203  FR_TOO_MANY_OPEN_FILES, /* (18) Number of open files > _FS_LOCK */
204  FR_INVALID_PARAMETER /* (19) Given parameter is invalid */
205 } FRESULT;
206 
207 
208 
209 /*--------------------------------------------------------------*/
210 /* FatFs module application interface */
211 
212 FRESULT f_open (FIL* fp, const TCHAR* path, BYTE mode); /* Open or create a file */
213 FRESULT f_close (FIL* fp); /* Close an open file object */
214 FRESULT f_read (FIL* fp, void* buff, UINT btr, UINT* br); /* Read data from a file */
215 FRESULT f_write (FIL* fp, const void* buff, UINT btw, UINT* bw); /* Write data to a file */
216 FRESULT f_forward (FIL* fp, UINT(*func)(const BYTE*,UINT), UINT btf, UINT* bf); /* Forward data to the stream */
217 FRESULT f_lseek (FIL* fp, DWORD ofs); /* Move file pointer of a file object */
218 FRESULT f_truncate (FIL* fp); /* Truncate file */
219 FRESULT f_sync (FIL* fp); /* Flush cached data of a writing file */
220 FRESULT f_opendir (DIR* dp, const TCHAR* path); /* Open a directory */
221 FRESULT f_closedir (DIR* dp); /* Close an open directory */
222 FRESULT f_readdir (DIR* dp, FILINFO* fno); /* Read a directory item */
223 FRESULT f_findfirst (DIR* dp, FILINFO* fno, const TCHAR* path, const TCHAR* pattern); /* Find first file */
224 FRESULT f_findnext (DIR* dp, FILINFO* fno); /* Find next file */
225 FRESULT f_mkdir (const TCHAR* path); /* Create a sub directory */
226 FRESULT f_unlink (const TCHAR* path); /* Delete an existing file or directory */
227 FRESULT f_rename (const TCHAR* path_old, const TCHAR* path_new); /* Rename/Move a file or directory */
228 FRESULT f_stat (const TCHAR* path, FILINFO* fno); /* Get file status */
229 FRESULT f_chmod (const TCHAR* path, BYTE attr, BYTE mask); /* Change attribute of the file/dir */
230 FRESULT f_utime (const TCHAR* path, const FILINFO* fno); /* Change times-tamp of the file/dir */
231 FRESULT f_chdir (const TCHAR* path); /* Change current directory */
232 FRESULT f_chdrive (const TCHAR* path); /* Change current drive */
233 FRESULT f_getcwd (TCHAR* buff, UINT len); /* Get current directory */
234 FRESULT f_getfree (const TCHAR* path, DWORD* nclst, FATFS** fatfs); /* Get number of free clusters on the drive */
235 FRESULT f_getlabel (const TCHAR* path, TCHAR* label, DWORD* vsn); /* Get volume label */
236 FRESULT f_setlabel (const TCHAR* label); /* Set volume label */
237 FRESULT f_mount (FATFS* fs, const TCHAR* path, BYTE opt); /* Mount/Unmount a logical drive */
238 FRESULT f_mkfs (const TCHAR* path, BYTE sfd, UINT au); /* Create a file system on the volume */
239 FRESULT f_fdisk (BYTE pdrv, const DWORD szt[], void* work); /* Divide a physical drive into some partitions */
240 int f_putc (TCHAR c, FIL* fp); /* Put a character to the file */
241 int f_puts (const TCHAR* str, FIL* cp); /* Put a string to the file */
242 int f_printf (FIL* fp, const TCHAR* str, ...); /* Put a formatted string to the file */
243 TCHAR* f_gets (TCHAR* buff, int len, FIL* fp); /* Get a string from the file */
244 
245 #define f_eof(fp) ((int)((fp)->fptr == (fp)->fsize))
246 #define f_error(fp) ((fp)->err)
247 #define f_tell(fp) ((fp)->fptr)
248 #define f_size(fp) ((fp)->fsize)
249 #define f_rewind(fp) f_lseek((fp), 0)
250 #define f_rewinddir(dp) f_readdir((dp), 0)
251 
252 #ifndef EOF
253 #define EOF (-1)
254 #endif
255 
256 
257 
258 
259 /*--------------------------------------------------------------*/
260 /* Additional user defined functions */
261 
262 /* RTC function */
263 #if !_FS_READONLY && !_FS_NORTC
264 DWORD get_fattime (void);
265 #endif
266 
267 /* Unicode support functions */
268 #if _USE_LFN /* Unicode - OEM code conversion */
269 WCHAR ff_convert (WCHAR chr, UINT dir); /* OEM-Unicode bidirectional conversion */
270 WCHAR ff_wtoupper (WCHAR chr); /* Unicode upper-case conversion */
271 #if _USE_LFN == 3 /* Memory functions */
272 void* ff_memalloc (UINT msize); /* Allocate memory block */
273 void ff_memfree (void* mblock); /* Free memory block */
274 #endif
275 #endif
276 
277 /* Sync functions */
278 #if _FS_REENTRANT
279 int ff_cre_syncobj (BYTE vol, _SYNC_t* sobj); /* Create a sync object */
280 int ff_req_grant (_SYNC_t sobj); /* Lock sync object */
281 void ff_rel_grant (_SYNC_t sobj); /* Unlock sync object */
282 int ff_del_syncobj (_SYNC_t sobj); /* Delete a sync object */
283 #endif
284 
285 
286 
287 
288 /*--------------------------------------------------------------*/
289 /* Flags and offset address */
290 
291 
292 /* File access control and file status flags (FIL.flag) */
293 
294 #define FA_READ 0x01
295 #define FA_OPEN_EXISTING 0x00
296 
297 #if !_FS_READONLY
298 #define FA_WRITE 0x02
299 #define FA_CREATE_NEW 0x04
300 #define FA_CREATE_ALWAYS 0x08
301 #define FA_OPEN_ALWAYS 0x10
302 #define FA__WRITTEN 0x20
303 #define FA__DIRTY 0x40
304 #endif
305 
306 
307 /* FAT sub type (FATFS.fs_type) */
308 
309 #define FS_FAT12 1
310 #define FS_FAT16 2
311 #define FS_FAT32 3
312 
313 
314 /* File attribute bits for directory entry */
315 
316 #define AM_RDO 0x01 /* Read only */
317 #define AM_HID 0x02 /* Hidden */
318 #define AM_SYS 0x04 /* System */
319 #define AM_VOL 0x08 /* Volume label */
320 #define AM_LFN 0x0F /* LFN entry */
321 #define AM_DIR 0x10 /* Directory */
322 #define AM_ARC 0x20 /* Archive */
323 #define AM_MASK 0x3F /* Mask of defined bits */
324 
325 
326 /* Fast seek feature */
327 #define CREATE_LINKMAP 0xFFFFFFFF
328 
329 
330 
331 /*--------------------------------*/
332 /* Multi-byte word access macros */
333 
334 #if _WORD_ACCESS == 1 /* Enable word access to the FAT structure */
335 #define LD_WORD(ptr) (WORD)(*(WORD*)(BYTE*)(ptr))
336 #define LD_DWORD(ptr) (DWORD)(*(DWORD*)(BYTE*)(ptr))
337 #define ST_WORD(ptr,val) *(WORD*)(BYTE*)(ptr)=(WORD)(val)
338 #define ST_DWORD(ptr,val) *(DWORD*)(BYTE*)(ptr)=(DWORD)(val)
339 #else /* Use byte-by-byte access to the FAT structure */
340 #define LD_WORD(ptr) (WORD)(((WORD)*((BYTE*)(ptr)+1)<<8)|(WORD)*(BYTE*)(ptr))
341 #define LD_DWORD(ptr) (DWORD)(((DWORD)*((BYTE*)(ptr)+3)<<24)|((DWORD)*((BYTE*)(ptr)+2)<<16)|((WORD)*((BYTE*)(ptr)+1)<<8)|*(BYTE*)(ptr))
342 #define ST_WORD(ptr,val) *(BYTE*)(ptr)=(BYTE)(val); *((BYTE*)(ptr)+1)=(BYTE)((WORD)(val)>>8)
343 #define ST_DWORD(ptr,val) *(BYTE*)(ptr)=(BYTE)(val); *((BYTE*)(ptr)+1)=(BYTE)((WORD)(val)>>8); *((BYTE*)(ptr)+2)=(BYTE)((DWORD)(val)>>16); *((BYTE*)(ptr)+3)=(BYTE)((DWORD)(val)>>24)
344 #endif
345 
346 #ifdef __cplusplus
347 }
348 #endif
349 
350 #endif /* _FATFS */
FATFS * fs
Definition: ff.h:115
FRESULT f_chdrive(const TCHAR *path)
DWORD winsect
Definition: ff.h:106
int f_puts(const TCHAR *str, FIL *cp)
unsigned short WORD
Definition: integer.h:20
unsigned short WCHAR
Definition: integer.h:21
DWORD sclust
Definition: ff.h:121
int f_putc(TCHAR c, FIL *fp)
DWORD clust
Definition: ff.h:148
#define _MAX_SS
Definition: ffconf.h:163
int ff_req_grant(_SYNC_t sobj)
Definition: ff.h:191
WORD ftime
Definition: ff.h:171
Definition: ff.h:114
DWORD n_fatent
Definition: ff.h:100
BYTE err
Definition: ff.h:118
FRESULT f_fdisk(BYTE pdrv, const DWORD szt[], void *work)
FRESULT f_mount(FATFS *fs, const TCHAR *path, BYTE opt)
Definition: ff.h:143
Definition: ff.h:78
FRESULT f_getlabel(const TCHAR *path, TCHAR *label, DWORD *vsn)
BYTE csize
Definition: ff.h:81
char TCHAR
Definition: ff.h:67
Definition: ff.h:196
DWORD dir_sect
Definition: ff.h:125
Definition: ff.h:192
BYTE * dir
Definition: ff.h:150
FRESULT f_chdir(const TCHAR *path)
FRESULT f_chmod(const TCHAR *path, BYTE attr, BYTE mask)
FRESULT f_readdir(DIR *dp, FILINFO *fno)
FRESULT f_read(FIL *fp, void *buff, UINT btr, UINT *br)
DWORD fsize
Definition: ff.h:120
FRESULT f_getfree(const TCHAR *path, DWORD *nclst, FATFS **fatfs)
FRESULT f_mkdir(const TCHAR *path)
FATFS * fs
Definition: ff.h:144
Definition: ff.h:187
FRESULT f_close(FIL *fp)
BYTE fsi_flag
Definition: ff.h:84
Definition: ff.h:186
unsigned long DWORD
Definition: integer.h:29
FRESULT f_lseek(FIL *fp, DWORD ofs)
int ff_cre_syncobj(BYTE vol, _SYNC_t *sobj)
Definition: ff.h:193
DWORD dsect
Definition: ff.h:123
FRESULT f_truncate(FIL *fp)
void ff_rel_grant(_SYNC_t sobj)
FRESULT f_forward(FIL *fp, UINT(*func)(const BYTE *, UINT), UINT btf, UINT *bf)
Definition: ff.h:189
unsigned char BYTE
Definition: integer.h:16
WORD n_rootdir
Definition: ff.h:86
BYTE flag
Definition: ff.h:117
WORD id
Definition: ff.h:145
FRESULT f_closedir(DIR *dp)
Definition: ff.h:190
FRESULT f_stat(const TCHAR *path, FILINFO *fno)
FRESULT f_rename(const TCHAR *path_old, const TCHAR *path_new)
DWORD last_clust
Definition: ff.h:94
FRESULT f_write(FIL *fp, const void *buff, UINT btw, UINT *bw)
_SYNC_t sobj
Definition: ff.h:91
FRESULT
Definition: ff.h:184
DWORD fsize
Definition: ff.h:101
BYTE fs_type
Definition: ff.h:79
Definition: ff.h:197
FRESULT f_sync(FIL *fp)
FRESULT f_open(FIL *fp, const TCHAR *path, BYTE mode)
BYTE n_fats
Definition: ff.h:82
DWORD fptr
Definition: ff.h:119
FRESULT f_mkfs(const TCHAR *path, BYTE sfd, UINT au)
DWORD sect
Definition: ff.h:149
Definition: ff.h:200
WORD id
Definition: ff.h:116
DWORD get_fattime(void)
DWORD sclust
Definition: ff.h:147
BYTE drv
Definition: ff.h:80
Definition: ff.h:203
BYTE fattrib
Definition: ff.h:172
Definition: ff.h:199
unsigned int UINT
Definition: integer.h:25
FRESULT f_setlabel(const TCHAR *label)
#define _SYNC_t
Definition: ffconf.h:231
Definition: ff.h:201
FRESULT f_findfirst(DIR *dp, FILINFO *fno, const TCHAR *path, const TCHAR *pattern)
BYTE * dir_ptr
Definition: ff.h:126
DWORD clust
Definition: ff.h:122
WORD id
Definition: ff.h:85
FRESULT f_utime(const TCHAR *path, const FILINFO *fno)
DWORD free_clust
Definition: ff.h:95
TCHAR * f_gets(TCHAR *buff, int len, FIL *fp)
BYTE wflag
Definition: ff.h:83
BYTE * fn
Definition: ff.h:151
int f_printf(FIL *fp, const TCHAR *str,...)
Definition: ff.h:185
DWORD volbase
Definition: ff.h:102
DWORD dirbase
Definition: ff.h:104
Definition: ff.h:168
Definition: ff.h:202
Definition: ff.h:204
Definition: ff.h:188
DWORD fsize
Definition: ff.h:169
DWORD database
Definition: ff.h:105
FRESULT f_findnext(DIR *dp, FILINFO *fno)
FRESULT f_opendir(DIR *dp, const TCHAR *path)
FRESULT f_unlink(const TCHAR *path)
FRESULT f_getcwd(TCHAR *buff, UINT len)
Definition: ff.h:198
Definition: ff.h:194
DWORD fatbase
Definition: ff.h:103
int ff_del_syncobj(_SYNC_t sobj)
WORD index
Definition: ff.h:146
WORD fdate
Definition: ff.h:170
Definition: ff.h:195
Copyright 2016, Texas Instruments Incorporated