49 #ifndef ti_drivers_uart_UARTCC3200DMA__include
50 #define ti_drivers_uart_UARTCC3200DMA__include
UART_STOP
UART stop bit settings.
Definition: UART.h:396
unsigned int readTimeout
Definition: UARTCC3200DMA.h:159
UART_Echo readEcho
Definition: UARTCC3200DMA.h:170
Clock interface for the RTOS Porting Interface.
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:514
UART_PAR
UART parity type settings.
Definition: UART.h:406
UART_DataMode writeDataMode
Definition: UARTCC3200DMA.h:165
struct UARTCC3200DMA_Object UARTCC3200DMA_Object
UARTCC3200DMA Object.
UART_Mode
UART mode settings.
Definition: UART.h:308
UART_DataMode
UART data mode settings.
Definition: UART.h:356
struct UARTCC3200DMA_HWAttrs UARTCC3200DMA_HWAttrs
UARTCC3200DMA Hardware attributes.
UART_ReturnMode
UART return mode settings.
Definition: UART.h:341
Power_NotifyObj postNotify
Definition: UARTCC3200DMA.h:190
size_t readCount
Definition: UARTCC3200DMA.h:179
UART_Echo
UART echo settings.
Definition: UART.h:374
uint32_t baudRate
Definition: UARTCC3200DMA.h:166
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
UART_DataMode readDataMode
Definition: UARTCC3200DMA.h:164
ClockP_Handle txFifoEmptyClk
Definition: UARTCC3200DMA.h:189
SemaphoreP_Handle readSem
Definition: UARTCC3200DMA.h:184
size_t writeSize
Definition: UARTCC3200DMA.h:175
void * readBuf
Definition: UARTCC3200DMA.h:178
UART_Mode readMode
Definition: UARTCC3200DMA.h:157
unsigned int intNum
Definition: UARTCC3200DMA.h:140
Power notify object structure.
Definition: Power.h:112
UART_STOP stopBits
Definition: UARTCC3200DMA.h:168
SemaphoreP_Handle writeSem
Definition: UARTCC3200DMA.h:183
UART_LEN dataLength
Definition: UARTCC3200DMA.h:167
unsigned int intPriority
Definition: UARTCC3200DMA.h:142
const UART_FxnTable UARTCC3200DMA_fxnTable
const void * writeBuf
Definition: UARTCC3200DMA.h:173
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:301
UART_PAR parityType
Definition: UARTCC3200DMA.h:169
UARTCC3200DMA Hardware attributes.
Definition: UARTCC3200DMA.h:136
unsigned long rxChannelIndex
Definition: UARTCC3200DMA.h:144
unsigned int writeTimeout
Definition: UARTCC3200DMA.h:160
HwiP_Handle hwiHandle
Definition: UARTCC3200DMA.h:186
unsigned int baseAddr
Definition: UARTCC3200DMA.h:138
size_t readSize
Definition: UARTCC3200DMA.h:180
UART_LEN
UART data length settings.
Definition: UART.h:384
UART_Callback writeCallback
Definition: UARTCC3200DMA.h:162
size_t writeCount
Definition: UARTCC3200DMA.h:174
unsigned int powerMgrId
Definition: UARTCC3200DMA.h:191
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
UART_ReturnMode readReturnMode
Definition: UARTCC3200DMA.h:163
UARTCC3200DMA Object.
Definition: UARTCC3200DMA.h:154
struct UARTCC3200DMA_Object * UARTCC3200DMA_Handle
UART_Callback readCallback
Definition: UARTCC3200DMA.h:161
unsigned long txChannelIndex
Definition: UARTCC3200DMA.h:146
Hardware Interrupt module for the RTOS Porting Interface.
bool opened
Definition: UARTCC3200DMA.h:156
UART_Mode writeMode
Definition: UARTCC3200DMA.h:158
void * ClockP_Handle
Opaque client reference to an instance of a ClockP.
Definition: ClockP.h:91