108 #ifndef ti_drivers_spi_SPIMSP432DMA__include
109 #define ti_drivers_spi_SPIMSP432DMA__include
SPI_TransferMode transferMode
Definition: SPIMSP432DMA.h:198
uint32_t baseAddr
Definition: SPIMSP432DMA.h:174
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:264
uint16_t clockPhase
Definition: SPIMSP432DMA.h:205
SPI_Mode spiMode
Definition: SPIMSP432DMA.h:199
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:298
uint8_t defaultTxBufValue
Definition: SPIMSP432DMA.h:178
struct SPIMSP432DMA_HWAttrs SPIMSP432DMA_HWAttrs
SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverl...
HwiP_Handle hwiHandle
Definition: SPIMSP432DMA.h:193
uint32_t txDMAChannelIndex
Definition: SPIMSP432DMA.h:183
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
uint8_t clockSource
Definition: SPIMSP432DMA.h:176
SPIMSP432DMA Object.
Definition: SPIMSP432DMA.h:191
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:384
SPI_Transaction * transaction
Definition: SPIMSP432DMA.h:196
uint16_t bitOrder
Definition: SPIMSP432DMA.h:175
struct SPIMSP432DMA_Object SPIMSP432DMA_Object
SPIMSP432DMA Object.
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:244
SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverl...
Definition: SPIMSP432DMA.h:173
Power notify object structure.
Definition: Power.h:112
SPI_Mode
Definitions for various SPI modes of operation.
Definition: SPI.h:270
uint8_t scratchBuffer
Definition: SPIMSP432DMA.h:200
uint16_t clockPolarity
Definition: SPIMSP432DMA.h:206
uint32_t intPriority
Definition: SPIMSP432DMA.h:181
Power_NotifyObj perfChangeNotify
Definition: SPIMSP432DMA.h:208
uint32_t perfConstraintMask
Definition: SPIMSP432DMA.h:209
uint32_t bitRate
Definition: SPIMSP432DMA.h:204
const SPI_FxnTable SPIMSP432DMA_fxnTable
SPI_CallbackFxn transferCallbackFxn
Definition: SPIMSP432DMA.h:195
SemaphoreP_Handle transferComplete
Definition: SPIMSP432DMA.h:192
uint8_t dmaIntNum
Definition: SPIMSP432DMA.h:180
bool isOpen
Definition: SPIMSP432DMA.h:202
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
struct SPIMSP432DMA_Object * SPIMSP432DMA_Handle
Hardware Interrupt module for the RTOS Porting Interface.
uint32_t rxDMAChannelIndex
Definition: SPIMSP432DMA.h:182