CC13xx Driver Library
rom.h File Reference
#include <inc/hw_types.h>

Go to the source code of this file.

Data Structures

struct  HARD_API_T
 

Macros

#define __HAPI_H__
 
#define ROM_HAPI_TABLE_ADDR   0x10000048
 
#define P_HARD_API   ((HARD_API_T*) ROM_HAPI_TABLE_ADDR)
 
#define HapiCrc32(a, b, c)    P_HARD_API->Crc32(a,b,c)
 
#define HapiGetFlashSize()    P_HARD_API->FlashGetSize()
 
#define HapiGetChipId()    P_HARD_API->GetChipId()
 
#define HapiSectorErase(a)    MemBusWrkAroundHapiEraseSector(a)
 
#define HapiProgramFlash(a, b, c)    MemBusWrkAroundHapiProgramFlash(a,b,c)
 
#define HapiResetDevice()    P_HARD_API->ResetDevice()
 
#define HapiFletcher32(a, b, c)    P_HARD_API->Fletcher32(a,b,c)
 
#define HapiMinValue(a, b)    P_HARD_API->MinValue(a,b)
 
#define HapiMaxValue(a, b)    P_HARD_API->MaxValue(a,b)
 
#define HapiMeanValue(a, b)    P_HARD_API->MeanValue(a,b)
 
#define HapiStandDeviationValue(a, b)   P_HARD_API->StandDeviationValue(a,b)
 
#define HapiHFSourceSafeSwitch()    P_HARD_API->HFSourceSafeSwitch()
 
#define HapiSelectCompAInput(a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectCompAInput , a )
 
#define HapiSelectCompARef(a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectCompARef , a )
 
#define HapiSelectADCCompBInput(a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectADCCompBInput, a )
 
#define HapiSelectCompBRef(a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectCompBRef , a )
 
#define COMPA_IN_NC   0x00
 
#define COMPA_IN_AUXIO7   0x09
 
#define COMPA_IN_AUXIO6   0x0A
 
#define COMPA_IN_AUXIO5   0x0B
 
#define COMPA_IN_AUXIO4   0x0C
 
#define COMPA_IN_AUXIO3   0x0D
 
#define COMPA_IN_AUXIO2   0x0E
 
#define COMPA_IN_AUXIO1   0x0F
 
#define COMPA_IN_AUXIO0   0x10
 
#define COMPA_REF_NC   0x00
 
#define COMPA_REF_DCOUPL   0x01
 
#define COMPA_REF_VSS   0x02
 
#define COMPA_REF_VDDS   0x03
 
#define COMPA_REF_ADCVREFP   0x04
 
#define COMPA_REF_AUXIO7   0x09
 
#define COMPA_REF_AUXIO6   0x0A
 
#define COMPA_REF_AUXIO5   0x0B
 
#define COMPA_REF_AUXIO4   0x0C
 
#define COMPA_REF_AUXIO3   0x0D
 
#define COMPA_REF_AUXIO2   0x0E
 
#define COMPA_REF_AUXIO1   0x0F
 
#define COMPA_REF_AUXIO0   0x10
 
#define ADC_COMPB_IN_NC   0x00
 
#define ADC_COMPB_IN_DCOUPL   0x03
 
#define ADC_COMPB_IN_VSS   0x04
 
#define ADC_COMPB_IN_VDDS   0x05
 
#define ADC_COMPB_IN_AUXIO7   0x09
 
#define ADC_COMPB_IN_AUXIO6   0x0A
 
#define ADC_COMPB_IN_AUXIO5   0x0B
 
#define ADC_COMPB_IN_AUXIO4   0x0C
 
#define ADC_COMPB_IN_AUXIO3   0x0D
 
#define ADC_COMPB_IN_AUXIO2   0x0E
 
#define ADC_COMPB_IN_AUXIO1   0x0F
 
#define ADC_COMPB_IN_AUXIO0   0x10
 
#define COMPB_REF_NC   0x00
 
#define COMPB_REF_DCOUPL   0x01
 
#define COMPB_REF_VSS   0x02
 
#define COMPB_REF_VDDS   0x03
 
#define ROM_APITABLE   ((uint32_t *)0x10000180)
 
#define ROM_VERSION   (ROM_APITABLE[0])
 
#define ROM_AON_EVENTTABLE   ((uint32_t *)(ROM_APITABLE[1]))
 
#define ROM_AON_IOCTABLE   ((uint32_t *)(ROM_APITABLE[2]))
 
#define ROM_AON_RTCTABLE   ((uint32_t *)(ROM_APITABLE[3]))
 
#define ROM_AON_WUCTABLE   ((uint32_t *)(ROM_APITABLE[4]))
 
#define ROM_AUX_CTRLTABLE   ((uint32_t *)(ROM_APITABLE[5]))
 
#define ROM_AUX_TDCTABLE   ((uint32_t *)(ROM_APITABLE[6]))
 
#define ROM_AUX_TIMERTABLE   ((uint32_t *)(ROM_APITABLE[7]))
 
#define ROM_AUX_WUCTABLE   ((uint32_t *)(ROM_APITABLE[8]))
 
#define ROM_DDITABLE   ((uint32_t *)(ROM_APITABLE[9]))
 
#define ROM_FLASHTABLE   ((uint32_t *)(ROM_APITABLE[10]))
 
#define ROM_I2CTABLE   ((uint32_t *)(ROM_APITABLE[11]))
 
#define ROM_INTERRUPTTABLE   ((uint32_t *)(ROM_APITABLE[12]))
 
#define ROM_IOCTABLE   ((uint32_t *)(ROM_APITABLE[13]))
 
#define ROM_PRCMTABLE   ((uint32_t *)(ROM_APITABLE[14]))
 
#define ROM_SMPHTABLE   ((uint32_t *)(ROM_APITABLE[15]))
 
#define ROM_SPISTABLE   ((uint32_t *)(ROM_APITABLE[16]))
 
#define ROM_SSITABLE   ((uint32_t *)(ROM_APITABLE[17]))
 
#define ROM_TIMERTABLE   ((uint32_t *)(ROM_APITABLE[18]))
 
#define ROM_TRNGTABLE   ((uint32_t *)(ROM_APITABLE[19]))
 
#define ROM_UARTTABLE   ((uint32_t *)(ROM_APITABLE[20]))
 
#define ROM_UDMATABLE   ((uint32_t *)(ROM_APITABLE[21]))
 
#define ROM_VIMSTABLE   ((uint32_t *)(ROM_APITABLE[22]))
 
#define ROM_AONEventMcuWakeUpSet
 
#define ROM_AONEventMcuWakeUpGet   ((uint32_t (*)(uint32_t ui32MCUWUEvent))ROM_AON_EVENTTABLE[1])
 
#define ROM_AONEventAuxWakeUpSet
 
#define ROM_AONEventAuxWakeUpGet   ((uint32_t (*)(uint32_t ui32AUXWUEvent))ROM_AON_EVENTTABLE[3])
 
#define ROM_AONEventMcuSet
 
#define ROM_AONEventMcuGet   ((uint32_t (*)(uint32_t ui32MCUEvent))ROM_AON_EVENTTABLE[5])
 
#define ROM_AONIOCDriveStrengthSet
 
#define ROM_AONIOCDriveStrengthGet   ((uint32_t (*)(uint32_t ui32DriveLevel))ROM_AON_IOCTABLE[1])
 
#define ROM_AONWUCAuxReset   ((void (*)(void))ROM_AON_WUCTABLE[3])
 
#define ROM_AONWUCRechargeCtrlConfigSet
 
#define ROM_AONWUCOscConfig   ((void (*)(uint32_t ui32Period))ROM_AON_WUCTABLE[5])
 
#define ROM_AUXTDCConfigSet
 
#define ROM_AUXTDCMeasurementDone   ((uint32_t (*)(uint32_t ui32Base))ROM_AUX_TDCTABLE[1])
 
#define ROM_AUXTimerConfigure
 
#define ROM_AUXTimerStart   ((void (*)(uint32_t ui32Timer))ROM_AUX_TIMERTABLE[1])
 
#define ROM_AUXTimerStop   ((void (*)(uint32_t ui32Timer))ROM_AUX_TIMERTABLE[2])
 
#define ROM_AUXTimerPrescaleSet
 
#define ROM_AUXTimerPrescaleGet   ((uint32_t (*)(uint32_t ui32Timer))ROM_AUX_TIMERTABLE[4])
 
#define ROM_AUXWUCClockEnable   ((void (*)(uint32_t ui32Clocks))ROM_AUX_WUCTABLE[0])
 
#define ROM_AUXWUCClockDisable   ((void (*)(uint32_t ui32Clocks))ROM_AUX_WUCTABLE[1])
 
#define ROM_AUXWUCClockStatus   ((uint32_t (*)(uint32_t ui32Clocks))ROM_AUX_WUCTABLE[2])
 
#define ROM_AUXWUCPowerCtrl   ((void (*)(uint32_t ui32PowerMode))ROM_AUX_WUCTABLE[3])
 
#define ROM_DDI16BitWrite
 
#define ROM_DDI16BitfieldWrite
 
#define ROM_DDI16BitRead
 
#define ROM_DDI16BitfieldRead
 
#define ROM_FlashPowerModeGet   ((uint32_t (*)(void))ROM_FLASHTABLE[1])
 
#define ROM_FlashProtectionSet
 
#define ROM_FlashProtectionGet   ((uint32_t (*)(uint32_t ui32SectorAddress))ROM_FLASHTABLE[3])
 
#define ROM_FlashProtectionSave   ((uint32_t (*)(uint32_t ui32SectorAddress))ROM_FLASHTABLE[4])
 
#define ROM_FlashEfuseReadRow
 
#define ROM_FlashDisableSectorsForWrite   ((void (*)(void))ROM_FLASHTABLE[9])
 
#define ROM_I2CMasterInitExpClk
 
#define ROM_I2CMasterErr   ((uint32_t (*)(uint32_t ui32Base))ROM_I2CTABLE[1])
 
#define ROM_IntPriorityGroupingSet   ((void (*)(uint32_t ui32Bits))ROM_INTERRUPTTABLE[0])
 
#define ROM_IntPriorityGroupingGet   ((uint32_t (*)(void))ROM_INTERRUPTTABLE[1])
 
#define ROM_IntPrioritySet
 
#define ROM_IntPriorityGet   ((int32_t (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[3])
 
#define ROM_IntEnable   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[4])
 
#define ROM_IntDisable   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[5])
 
#define ROM_IntPendSet   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[6])
 
#define ROM_IntPendGet   ((bool (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[7])
 
#define ROM_IntPendClear   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[8])
 
#define ROM_IOCPortConfigureSet
 
#define ROM_IOCPortConfigureGet   ((uint32_t (*)(uint32_t ui32IOId))ROM_IOCTABLE[1])
 
#define ROM_IOCIOShutdownSet
 
#define ROM_IOCIOModeSet
 
#define ROM_IOCIOIntSet
 
#define ROM_IOCIOPortPullSet
 
#define ROM_IOCIOHystSet
 
#define ROM_IOCIOInputSet
 
#define ROM_IOCIOSlewCtrlSet
 
#define ROM_IOCIODrvStrengthSet
 
#define ROM_IOCIOPortIdSet
 
#define ROM_IOCIntEnable   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[12])
 
#define ROM_IOCIntDisable   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[13])
 
#define ROM_IOCPinTypeGpioInput   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[14])
 
#define ROM_IOCPinTypeGpioOutput   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[15])
 
#define ROM_IOCPinTypeUart
 
#define ROM_IOCPinTypeSsiMaster
 
#define ROM_IOCPinTypeSsiSlave
 
#define ROM_IOCPinTypeI2c
 
#define ROM_IOCPinTypeSpis
 
#define ROM_IOCPinTypeAux   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[21])
 
#define ROM_PRCMInfClockConfigureSet
 
#define ROM_PRCMInfClockConfigureGet   ((uint32_t (*)(uint32_t ui32PowerMode))ROM_PRCMTABLE[1])
 
#define ROM_PRCMAudioClockConfigSet
 
#define ROM_PRCMPowerDomainOn   ((void (*)(uint32_t ui32Domains))ROM_PRCMTABLE[5])
 
#define ROM_PRCMPowerDomainOff   ((void (*)(uint32_t ui32Domains))ROM_PRCMTABLE[6])
 
#define ROM_PRCMPeripheralRunEnable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[7])
 
#define ROM_PRCMPeripheralRunDisable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[8])
 
#define ROM_PRCMPeripheralSleepEnable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[9])
 
#define ROM_PRCMPeripheralSleepDisable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[10])
 
#define ROM_PRCMPeripheralDeepSleepEnable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[11])
 
#define ROM_PRCMPeripheralDeepSleepDisable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[12])
 
#define ROM_PRCMPowerDomainStatus   ((uint32_t (*)(uint32_t ui32Domains))ROM_PRCMTABLE[13])
 
#define ROM_PRCMDeepSleep   ((void (*)(void))ROM_PRCMTABLE[14])
 
#define ROM_SMPHAcquire   ((void (*)(uint32_t ui32Semaphore))ROM_SMPHTABLE[0])
 
#define ROM_SSIConfigSetExpClk
 
#define ROM_SSIDataPut
 
#define ROM_SSIDataPutNonBlocking
 
#define ROM_SSIDataGet
 
#define ROM_SSIDataGetNonBlocking
 
#define ROM_TimerConfigure
 
#define ROM_TimerLevelControl
 
#define ROM_TimerStallControl
 
#define ROM_TimerWaitOnTriggerControl
 
#define ROM_TRNGNumberGet   ((uint32_t (*)(uint32_t ui32Word))ROM_TRNGTABLE[1])
 
#define ROM_UARTFIFOLevelGet
 
#define ROM_UARTConfigSetExpClk
 
#define ROM_UARTConfigGetExpClk
 
#define ROM_UARTDisable   ((void (*)(uint32_t ui32Base))ROM_UARTTABLE[3])
 
#define ROM_UARTCharGetNonBlocking   ((int32_t (*)(uint32_t ui32Base))ROM_UARTTABLE[4])
 
#define ROM_UARTCharGet   ((int32_t (*)(uint32_t ui32Base))ROM_UARTTABLE[5])
 
#define ROM_UARTCharPutNonBlocking
 
#define ROM_UARTCharPut
 
#define ROM_uDMAChannelAttributeEnable
 
#define ROM_uDMAChannelAttributeDisable
 
#define ROM_uDMAChannelAttributeGet
 
#define ROM_uDMAChannelControlSet
 
#define ROM_uDMAChannelScatterGatherSet
 
#define ROM_uDMAChannelSizeGet
 
#define ROM_uDMAChannelModeGet
 
#define ROM_VIMSConfigure
 
#define ROM_VIMSModeSet
 

Typedefs

typedef uint32_t(* FPTR_CRC32_T) (uint8_t *, uint32_t, uint32_t)
 
typedef uint32_t(* FPTR_GETFLSIZE_T) (void)
 
typedef uint32_t(* FPTR_GETCHIPID_T) (void)
 
typedef uint32_t(* FPTR_RESERVED1_T) (uint32_t)
 
typedef uint32_t(* FPTR_RESERVED2_T) (void)
 
typedef uint32_t(* FPTR_RESERVED3_T) (uint8_t *, uint32_t, uint32_t)
 
typedef void(* FPTR_RESETDEV_T) (void)
 
typedef uint32_t(* FPTR_FLETCHER32_T) (uint16_t *, uint16_t, uint16_t)
 
typedef uint32_t(* FPTR_MINVAL_T) (uint32_t *, uint32_t)
 
typedef uint32_t(* FPTR_MAXVAL_T) (uint32_t *, uint32_t)
 
typedef uint32_t(* FPTR_MEANVAL_T) (uint32_t *, uint32_t)
 
typedef uint32_t(* FPTR_STDDVAL_T) (uint32_t *, uint32_t)
 
typedef void(* FPTR_HFSOURCESAFESWITCH_T) (void)
 
typedef void(* FPTR_RESERVED4_T) (uint32_t)
 
typedef void(* FPTR_RESERVED5_T) (uint32_t)
 
typedef void(* FPTR_COMPAIN_T) (uint8_t)
 
typedef void(* FPTR_COMPAREF_T) (uint8_t)
 
typedef void(* FPTR_ADCCOMPBIN_T) (uint8_t)
 
typedef void(* FPTR_COMPBREF_T) (uint8_t)
 

Functions

uint32_t MemBusWrkAroundHapiProgramFlash (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
 
uint32_t MemBusWrkAroundHapiEraseSector (uint32_t ui32Address)
 
void SafeHapiAuxAdiSelect (FPTR_VOID_UINT8_T fPtr, uint8_t ut8Signal)
 

Macro Definition Documentation

#define __HAPI_H__

Definition at line 56 of file rom.h.

#define ADC_COMPB_IN_AUXIO0   0x10

Definition at line 219 of file rom.h.

#define ADC_COMPB_IN_AUXIO1   0x0F

Definition at line 218 of file rom.h.

#define ADC_COMPB_IN_AUXIO2   0x0E

Definition at line 217 of file rom.h.

#define ADC_COMPB_IN_AUXIO3   0x0D

Definition at line 216 of file rom.h.

#define ADC_COMPB_IN_AUXIO4   0x0C

Definition at line 215 of file rom.h.

#define ADC_COMPB_IN_AUXIO5   0x0B

Definition at line 214 of file rom.h.

#define ADC_COMPB_IN_AUXIO6   0x0A

Definition at line 213 of file rom.h.

#define ADC_COMPB_IN_AUXIO7   0x09

Definition at line 212 of file rom.h.

#define ADC_COMPB_IN_DCOUPL   0x03

Definition at line 209 of file rom.h.

#define ADC_COMPB_IN_NC   0x00

Definition at line 208 of file rom.h.

#define ADC_COMPB_IN_VDDS   0x05

Definition at line 211 of file rom.h.

#define ADC_COMPB_IN_VSS   0x04

Definition at line 210 of file rom.h.

#define COMPA_IN_AUXIO0   0x10

Definition at line 184 of file rom.h.

#define COMPA_IN_AUXIO1   0x0F

Definition at line 183 of file rom.h.

#define COMPA_IN_AUXIO2   0x0E

Definition at line 182 of file rom.h.

#define COMPA_IN_AUXIO3   0x0D

Definition at line 181 of file rom.h.

#define COMPA_IN_AUXIO4   0x0C

Definition at line 180 of file rom.h.

#define COMPA_IN_AUXIO5   0x0B

Definition at line 179 of file rom.h.

#define COMPA_IN_AUXIO6   0x0A

Definition at line 178 of file rom.h.

#define COMPA_IN_AUXIO7   0x09

Definition at line 177 of file rom.h.

#define COMPA_IN_NC   0x00

Definition at line 176 of file rom.h.

#define COMPA_REF_ADCVREFP   0x04

Definition at line 194 of file rom.h.

#define COMPA_REF_AUXIO0   0x10

Definition at line 202 of file rom.h.

#define COMPA_REF_AUXIO1   0x0F

Definition at line 201 of file rom.h.

#define COMPA_REF_AUXIO2   0x0E

Definition at line 200 of file rom.h.

#define COMPA_REF_AUXIO3   0x0D

Definition at line 199 of file rom.h.

#define COMPA_REF_AUXIO4   0x0C

Definition at line 198 of file rom.h.

#define COMPA_REF_AUXIO5   0x0B

Definition at line 197 of file rom.h.

#define COMPA_REF_AUXIO6   0x0A

Definition at line 196 of file rom.h.

#define COMPA_REF_AUXIO7   0x09

Definition at line 195 of file rom.h.

#define COMPA_REF_DCOUPL   0x01

Definition at line 191 of file rom.h.

#define COMPA_REF_NC   0x00

Definition at line 190 of file rom.h.

#define COMPA_REF_VDDS   0x03

Definition at line 193 of file rom.h.

#define COMPA_REF_VSS   0x02

Definition at line 192 of file rom.h.

#define COMPB_REF_DCOUPL   0x01

Definition at line 226 of file rom.h.

#define COMPB_REF_NC   0x00

Definition at line 225 of file rom.h.

#define COMPB_REF_VDDS   0x03

Definition at line 228 of file rom.h.

#define COMPB_REF_VSS   0x02

Definition at line 227 of file rom.h.

#define HapiCrc32 (   a,
  b,
 
)    P_HARD_API->Crc32(a,b,c)

Definition at line 155 of file rom.h.

#define HapiFletcher32 (   a,
  b,
 
)    P_HARD_API->Fletcher32(a,b,c)

Definition at line 161 of file rom.h.

#define HapiGetChipId ( )    P_HARD_API->GetChipId()

Definition at line 157 of file rom.h.

#define HapiGetFlashSize ( )    P_HARD_API->FlashGetSize()

Definition at line 156 of file rom.h.

#define HapiHFSourceSafeSwitch ( )    P_HARD_API->HFSourceSafeSwitch()

Definition at line 166 of file rom.h.

Referenced by OSCHfSourceSwitch().

#define HapiMaxValue (   a,
 
)    P_HARD_API->MaxValue(a,b)

Definition at line 163 of file rom.h.

#define HapiMeanValue (   a,
 
)    P_HARD_API->MeanValue(a,b)

Definition at line 164 of file rom.h.

#define HapiMinValue (   a,
 
)    P_HARD_API->MinValue(a,b)

Definition at line 162 of file rom.h.

#define HapiProgramFlash (   a,
  b,
 
)    MemBusWrkAroundHapiProgramFlash(a,b,c)

Definition at line 159 of file rom.h.

#define HapiResetDevice ( )    P_HARD_API->ResetDevice()

Definition at line 160 of file rom.h.

#define HapiSectorErase (   a)    MemBusWrkAroundHapiEraseSector(a)

Definition at line 158 of file rom.h.

#define HapiSelectADCCompBInput (   a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectADCCompBInput, a )

Definition at line 169 of file rom.h.

Referenced by AUXADCSelectInput().

#define HapiSelectCompAInput (   a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectCompAInput , a )

Definition at line 167 of file rom.h.

#define HapiSelectCompARef (   a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectCompARef , a )

Definition at line 168 of file rom.h.

#define HapiSelectCompBRef (   a)    SafeHapiAuxAdiSelect( P_HARD_API->SelectCompBRef , a )

Definition at line 170 of file rom.h.

#define HapiStandDeviationValue (   a,
 
)    P_HARD_API->StandDeviationValue(a,b)

Definition at line 165 of file rom.h.

#define P_HARD_API   ((HARD_API_T*) ROM_HAPI_TABLE_ADDR)

Definition at line 148 of file rom.h.

#define ROM_AON_EVENTTABLE   ((uint32_t *)(ROM_APITABLE[1]))

Definition at line 239 of file rom.h.

#define ROM_AON_IOCTABLE   ((uint32_t *)(ROM_APITABLE[2]))

Definition at line 240 of file rom.h.

#define ROM_AON_RTCTABLE   ((uint32_t *)(ROM_APITABLE[3]))

Definition at line 241 of file rom.h.

#define ROM_AON_WUCTABLE   ((uint32_t *)(ROM_APITABLE[4]))

Definition at line 242 of file rom.h.

#define ROM_AONEventAuxWakeUpGet   ((uint32_t (*)(uint32_t ui32AUXWUEvent))ROM_AON_EVENTTABLE[3])

Definition at line 278 of file rom.h.

#define ROM_AONEventAuxWakeUpSet
Value:
((void (*)(uint32_t ui32AUXWUEvent, \
uint32_t ui32EventSrc))ROM_AON_EVENTTABLE[2])
#define ROM_AON_EVENTTABLE
Definition: rom.h:239

Definition at line 274 of file rom.h.

#define ROM_AONEventMcuGet   ((uint32_t (*)(uint32_t ui32MCUEvent))ROM_AON_EVENTTABLE[5])

Definition at line 285 of file rom.h.

#define ROM_AONEventMcuSet
Value:
((void (*)(uint32_t ui32MCUEvent, \
uint32_t ui32EventSrc))ROM_AON_EVENTTABLE[4])
#define ROM_AON_EVENTTABLE
Definition: rom.h:239

Definition at line 281 of file rom.h.

#define ROM_AONEventMcuWakeUpGet   ((uint32_t (*)(uint32_t ui32MCUWUEvent))ROM_AON_EVENTTABLE[1])

Definition at line 271 of file rom.h.

#define ROM_AONEventMcuWakeUpSet
Value:
((void (*)(uint32_t ui32MCUWUEvent, \
uint32_t ui32EventSrc))ROM_AON_EVENTTABLE[0])
#define ROM_AON_EVENTTABLE
Definition: rom.h:239

Definition at line 267 of file rom.h.

#define ROM_AONIOCDriveStrengthGet   ((uint32_t (*)(uint32_t ui32DriveLevel))ROM_AON_IOCTABLE[1])

Definition at line 298 of file rom.h.

#define ROM_AONIOCDriveStrengthSet
Value:
((void (*)(uint32_t ui32LowDrvStr, \
uint32_t ui32MedDrvStr, \
uint32_t ui32MaxDrvStr))ROM_AON_IOCTABLE[0])
#define ROM_AON_IOCTABLE
Definition: rom.h:240

Definition at line 293 of file rom.h.

#define ROM_AONWUCAuxReset   ((void (*)(void))ROM_AON_WUCTABLE[3])

Definition at line 313 of file rom.h.

#define ROM_AONWUCOscConfig   ((void (*)(uint32_t ui32Period))ROM_AON_WUCTABLE[5])

Definition at line 322 of file rom.h.

#define ROM_AONWUCRechargeCtrlConfigSet
Value:
((void (*)(bool bAdaptEnable, \
uint32_t ui32AdaptRate, \
uint32_t ui32Period, \
uint32_t ui32MaxPeriod))ROM_AON_WUCTABLE[4])
#define ROM_AON_WUCTABLE
Definition: rom.h:242

Definition at line 316 of file rom.h.

#define ROM_APITABLE   ((uint32_t *)0x10000180)

Definition at line 237 of file rom.h.

#define ROM_AUX_CTRLTABLE   ((uint32_t *)(ROM_APITABLE[5]))

Definition at line 243 of file rom.h.

#define ROM_AUX_TDCTABLE   ((uint32_t *)(ROM_APITABLE[6]))

Definition at line 244 of file rom.h.

#define ROM_AUX_TIMERTABLE   ((uint32_t *)(ROM_APITABLE[7]))

Definition at line 245 of file rom.h.

#define ROM_AUX_WUCTABLE   ((uint32_t *)(ROM_APITABLE[8]))

Definition at line 246 of file rom.h.

#define ROM_AUXTDCConfigSet
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32StartCondition, \
uint32_t ui32StopCondition))ROM_AUX_TDCTABLE[0])
#define ROM_AUX_TDCTABLE
Definition: rom.h:244

Definition at line 331 of file rom.h.

#define ROM_AUXTDCMeasurementDone   ((uint32_t (*)(uint32_t ui32Base))ROM_AUX_TDCTABLE[1])

Definition at line 336 of file rom.h.

#define ROM_AUXTimerConfigure
Value:
((void (*)(uint32_t ui32Timer, \
uint32_t ui32Config))ROM_AUX_TIMERTABLE[0])
#define ROM_AUX_TIMERTABLE
Definition: rom.h:245

Definition at line 344 of file rom.h.

#define ROM_AUXTimerPrescaleGet   ((uint32_t (*)(uint32_t ui32Timer))ROM_AUX_TIMERTABLE[4])

Definition at line 358 of file rom.h.

#define ROM_AUXTimerPrescaleSet
Value:
((void (*)(uint32_t ui32Timer, \
uint32_t ui32PrescaleDiv))ROM_AUX_TIMERTABLE[3])
#define ROM_AUX_TIMERTABLE
Definition: rom.h:245

Definition at line 354 of file rom.h.

#define ROM_AUXTimerStart   ((void (*)(uint32_t ui32Timer))ROM_AUX_TIMERTABLE[1])

Definition at line 348 of file rom.h.

#define ROM_AUXTimerStop   ((void (*)(uint32_t ui32Timer))ROM_AUX_TIMERTABLE[2])

Definition at line 351 of file rom.h.

#define ROM_AUXWUCClockDisable   ((void (*)(uint32_t ui32Clocks))ROM_AUX_WUCTABLE[1])

Definition at line 369 of file rom.h.

#define ROM_AUXWUCClockEnable   ((void (*)(uint32_t ui32Clocks))ROM_AUX_WUCTABLE[0])

Definition at line 366 of file rom.h.

#define ROM_AUXWUCClockStatus   ((uint32_t (*)(uint32_t ui32Clocks))ROM_AUX_WUCTABLE[2])

Definition at line 372 of file rom.h.

#define ROM_AUXWUCPowerCtrl   ((void (*)(uint32_t ui32PowerMode))ROM_AUX_WUCTABLE[3])

Definition at line 375 of file rom.h.

#define ROM_DDI16BitfieldRead
Value:
((uint16_t (*)(uint32_t ui32Base, \
uint32_t ui32Reg, \
uint32_t ui32Mask, \
uint32_t ui32Shift))ROM_DDITABLE[3])
#define ROM_DDITABLE
Definition: rom.h:247

Definition at line 401 of file rom.h.

#define ROM_DDI16BitfieldWrite
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Reg, \
uint32_t ui32Mask, \
uint32_t ui32Shift, \
uint16_t ui32Data))ROM_DDITABLE[1])
#define ROM_DDITABLE
Definition: rom.h:247

Definition at line 389 of file rom.h.

#define ROM_DDI16BitRead
Value:
((uint16_t (*)(uint32_t ui32Base, \
uint32_t ui32Reg, \
uint32_t ui32Mask))ROM_DDITABLE[2])
#define ROM_DDITABLE
Definition: rom.h:247

Definition at line 396 of file rom.h.

#define ROM_DDI16BitWrite
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Reg, \
uint32_t ui32Mask, \
uint32_t ui32WrData))ROM_DDITABLE[0])
#define ROM_DDITABLE
Definition: rom.h:247

Definition at line 383 of file rom.h.

#define ROM_DDITABLE   ((uint32_t *)(ROM_APITABLE[9]))

Definition at line 247 of file rom.h.

#define ROM_FlashDisableSectorsForWrite   ((void (*)(void))ROM_FLASHTABLE[9])

Definition at line 430 of file rom.h.

#define ROM_FlashEfuseReadRow
Value:
((bool (*)(uint32_t *pui32EfuseData, \
uint32_t ui32RowAddress))ROM_FLASHTABLE[8])
#define ROM_FLASHTABLE
Definition: rom.h:248

Definition at line 426 of file rom.h.

#define ROM_FlashPowerModeGet   ((uint32_t (*)(void))ROM_FLASHTABLE[1])

Definition at line 413 of file rom.h.

#define ROM_FlashProtectionGet   ((uint32_t (*)(uint32_t ui32SectorAddress))ROM_FLASHTABLE[3])

Definition at line 420 of file rom.h.

#define ROM_FlashProtectionSave   ((uint32_t (*)(uint32_t ui32SectorAddress))ROM_FLASHTABLE[4])

Definition at line 423 of file rom.h.

#define ROM_FlashProtectionSet
Value:
((void (*)(uint32_t ui32SectorAddress, \
uint32_t ui32ProtectMode))ROM_FLASHTABLE[2])
#define ROM_FLASHTABLE
Definition: rom.h:248

Definition at line 416 of file rom.h.

#define ROM_FLASHTABLE   ((uint32_t *)(ROM_APITABLE[10]))

Definition at line 248 of file rom.h.

Referenced by FlashProgram(), and FlashSectorErase().

#define ROM_HAPI_TABLE_ADDR   0x10000048

Definition at line 61 of file rom.h.

Referenced by MemBusWrkAroundHapiEraseSector(), and MemBusWrkAroundHapiProgramFlash().

#define ROM_I2CMasterErr   ((uint32_t (*)(uint32_t ui32Base))ROM_I2CTABLE[1])

Definition at line 443 of file rom.h.

#define ROM_I2CMasterInitExpClk
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32I2CClk, \
bool bFast))ROM_I2CTABLE[0])
#define ROM_I2CTABLE
Definition: rom.h:249

Definition at line 438 of file rom.h.

#define ROM_I2CTABLE   ((uint32_t *)(ROM_APITABLE[11]))

Definition at line 249 of file rom.h.

#define ROM_IntDisable   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[5])

Definition at line 467 of file rom.h.

#define ROM_IntEnable   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[4])

Definition at line 464 of file rom.h.

#define ROM_INTERRUPTTABLE   ((uint32_t *)(ROM_APITABLE[12]))

Definition at line 250 of file rom.h.

#define ROM_IntPendClear   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[8])

Definition at line 476 of file rom.h.

#define ROM_IntPendGet   ((bool (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[7])

Definition at line 473 of file rom.h.

#define ROM_IntPendSet   ((void (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[6])

Definition at line 470 of file rom.h.

#define ROM_IntPriorityGet   ((int32_t (*)(uint32_t ui32Interrupt))ROM_INTERRUPTTABLE[3])

Definition at line 461 of file rom.h.

#define ROM_IntPriorityGroupingGet   ((uint32_t (*)(void))ROM_INTERRUPTTABLE[1])

Definition at line 454 of file rom.h.

#define ROM_IntPriorityGroupingSet   ((void (*)(uint32_t ui32Bits))ROM_INTERRUPTTABLE[0])

Definition at line 451 of file rom.h.

#define ROM_IntPrioritySet
Value:
((void (*)(uint32_t ui32Interrupt, \
uint8_t ui8Priority))ROM_INTERRUPTTABLE[2])
#define ROM_INTERRUPTTABLE
Definition: rom.h:250

Definition at line 457 of file rom.h.

#define ROM_IOCIntDisable   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[13])

Definition at line 534 of file rom.h.

#define ROM_IOCIntEnable   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[12])

Definition at line 531 of file rom.h.

#define ROM_IOCIODrvStrengthSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32IOCurrent, \
uint32_t ui32DrvStrength))ROM_IOCTABLE[10])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 522 of file rom.h.

#define ROM_IOCIOHystSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32Hysteresis))ROM_IOCTABLE[7])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 510 of file rom.h.

#define ROM_IOCIOInputSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32Input))ROM_IOCTABLE[8])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 514 of file rom.h.

#define ROM_IOCIOIntSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32Int, \
uint32_t ui32EdgeDet))ROM_IOCTABLE[5])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 501 of file rom.h.

#define ROM_IOCIOModeSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32IOMode))ROM_IOCTABLE[4])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 497 of file rom.h.

#define ROM_IOCIOPortIdSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32PortId))ROM_IOCTABLE[11])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 527 of file rom.h.

#define ROM_IOCIOPortPullSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32Pull))ROM_IOCTABLE[6])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 506 of file rom.h.

#define ROM_IOCIOShutdownSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32IOShutdown))ROM_IOCTABLE[2])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 492 of file rom.h.

#define ROM_IOCIOSlewCtrlSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32SlewEnable))ROM_IOCTABLE[9])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 518 of file rom.h.

#define ROM_IOCPinTypeAux   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[21])

Definition at line 575 of file rom.h.

#define ROM_IOCPinTypeGpioInput   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[14])

Definition at line 537 of file rom.h.

#define ROM_IOCPinTypeGpioOutput   ((void (*)(uint32_t ui32IOId))ROM_IOCTABLE[15])

Definition at line 540 of file rom.h.

#define ROM_IOCPinTypeI2c
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Data, \
uint32_t ui32Clk))ROM_IOCTABLE[19])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 564 of file rom.h.

#define ROM_IOCPinTypeSpis
Value:
((void (*)(uint32_t ui32Rx, \
uint32_t ui32Tx, \
uint32_t ui32Fss, \
uint32_t ui32Clk))ROM_IOCTABLE[20])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 569 of file rom.h.

#define ROM_IOCPinTypeSsiMaster
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Rx, \
uint32_t ui32Tx, \
uint32_t ui32Fss, \
uint32_t ui32Clk))ROM_IOCTABLE[17])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 550 of file rom.h.

#define ROM_IOCPinTypeSsiSlave
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Rx, \
uint32_t ui32Tx, \
uint32_t ui32Fss, \
uint32_t ui32Clk))ROM_IOCTABLE[18])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 557 of file rom.h.

#define ROM_IOCPinTypeUart
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Rx, \
uint32_t ui32Tx, \
uint32_t ui32Cts, \
uint32_t ui32Rts))ROM_IOCTABLE[16])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 543 of file rom.h.

#define ROM_IOCPortConfigureGet   ((uint32_t (*)(uint32_t ui32IOId))ROM_IOCTABLE[1])

Definition at line 489 of file rom.h.

#define ROM_IOCPortConfigureSet
Value:
((void (*)(uint32_t ui32IOId, \
uint32_t ui32PortId, \
uint32_t ui32IOConfig))ROM_IOCTABLE[0])
#define ROM_IOCTABLE
Definition: rom.h:251

Definition at line 484 of file rom.h.

#define ROM_IOCTABLE   ((uint32_t *)(ROM_APITABLE[13]))

Definition at line 251 of file rom.h.

#define ROM_PRCMAudioClockConfigSet
Value:
((void (*)(uint32_t ui32ClkConfig, \
uint32_t ui32SampleRate))ROM_PRCMTABLE[4])
#define ROM_PRCMTABLE
Definition: rom.h:252

Definition at line 591 of file rom.h.

#define ROM_PRCMDeepSleep   ((void (*)(void))ROM_PRCMTABLE[14])

Definition at line 622 of file rom.h.

#define ROM_PRCMInfClockConfigureGet   ((uint32_t (*)(uint32_t ui32PowerMode))ROM_PRCMTABLE[1])

Definition at line 587 of file rom.h.

#define ROM_PRCMInfClockConfigureSet
Value:
((void (*)(uint32_t ui32ClkDiv, \
uint32_t ui32PowerMode))ROM_PRCMTABLE[0])
#define ROM_PRCMTABLE
Definition: rom.h:252

Definition at line 583 of file rom.h.

#define ROM_PRCMPeripheralDeepSleepDisable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[12])

Definition at line 616 of file rom.h.

#define ROM_PRCMPeripheralDeepSleepEnable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[11])

Definition at line 613 of file rom.h.

#define ROM_PRCMPeripheralRunDisable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[8])

Definition at line 604 of file rom.h.

#define ROM_PRCMPeripheralRunEnable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[7])

Definition at line 601 of file rom.h.

#define ROM_PRCMPeripheralSleepDisable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[10])

Definition at line 610 of file rom.h.

#define ROM_PRCMPeripheralSleepEnable   ((void (*)(uint32_t ui32Peripheral))ROM_PRCMTABLE[9])

Definition at line 607 of file rom.h.

#define ROM_PRCMPowerDomainOff   ((void (*)(uint32_t ui32Domains))ROM_PRCMTABLE[6])

Definition at line 598 of file rom.h.

#define ROM_PRCMPowerDomainOn   ((void (*)(uint32_t ui32Domains))ROM_PRCMTABLE[5])

Definition at line 595 of file rom.h.

#define ROM_PRCMPowerDomainStatus   ((uint32_t (*)(uint32_t ui32Domains))ROM_PRCMTABLE[13])

Definition at line 619 of file rom.h.

#define ROM_PRCMTABLE   ((uint32_t *)(ROM_APITABLE[14]))

Definition at line 252 of file rom.h.

#define ROM_SMPHAcquire   ((void (*)(uint32_t ui32Semaphore))ROM_SMPHTABLE[0])

Definition at line 631 of file rom.h.

#define ROM_SMPHTABLE   ((uint32_t *)(ROM_APITABLE[15]))

Definition at line 253 of file rom.h.

#define ROM_SPISTABLE   ((uint32_t *)(ROM_APITABLE[16]))

Definition at line 254 of file rom.h.

#define ROM_SSIConfigSetExpClk
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32SSIClk, \
uint32_t ui32Protocol, \
uint32_t ui32Mode, \
uint32_t ui32BitRate, \
uint32_t ui32DataWidth))ROM_SSITABLE[0])
#define ROM_SSITABLE
Definition: rom.h:255

Definition at line 640 of file rom.h.

#define ROM_SSIDataGet
Value:
((void (*)(uint32_t ui32Base, \
uint32_t *pui32Data))ROM_SSITABLE[3])
#define ROM_SSITABLE
Definition: rom.h:255

Definition at line 656 of file rom.h.

#define ROM_SSIDataGetNonBlocking
Value:
((int32_t (*)(uint32_t ui32Base, \
uint32_t *pui32Data))ROM_SSITABLE[4])
#define ROM_SSITABLE
Definition: rom.h:255

Definition at line 660 of file rom.h.

#define ROM_SSIDataPut
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Data))ROM_SSITABLE[1])
#define ROM_SSITABLE
Definition: rom.h:255

Definition at line 648 of file rom.h.

#define ROM_SSIDataPutNonBlocking
Value:
((int32_t (*)(uint32_t ui32Base, \
uint32_t ui32Data))ROM_SSITABLE[2])
#define ROM_SSITABLE
Definition: rom.h:255

Definition at line 652 of file rom.h.

#define ROM_SSITABLE   ((uint32_t *)(ROM_APITABLE[17]))

Definition at line 255 of file rom.h.

#define ROM_TimerConfigure
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Config))ROM_TIMERTABLE[0])
#define ROM_TIMERTABLE
Definition: rom.h:256

Definition at line 669 of file rom.h.

#define ROM_TimerLevelControl
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Timer, \
bool bInvert))ROM_TIMERTABLE[1])
#define ROM_TIMERTABLE
Definition: rom.h:256

Definition at line 673 of file rom.h.

#define ROM_TimerStallControl
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Timer, \
bool bStall))ROM_TIMERTABLE[3])
#define ROM_TIMERTABLE
Definition: rom.h:256

Definition at line 678 of file rom.h.

#define ROM_TIMERTABLE   ((uint32_t *)(ROM_APITABLE[18]))

Definition at line 256 of file rom.h.

#define ROM_TimerWaitOnTriggerControl
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Timer, \
bool bWait))ROM_TIMERTABLE[4])
#define ROM_TIMERTABLE
Definition: rom.h:256

Definition at line 683 of file rom.h.

#define ROM_TRNGNumberGet   ((uint32_t (*)(uint32_t ui32Word))ROM_TRNGTABLE[1])

Definition at line 694 of file rom.h.

#define ROM_TRNGTABLE   ((uint32_t *)(ROM_APITABLE[19]))

Definition at line 257 of file rom.h.

#define ROM_UARTCharGet   ((int32_t (*)(uint32_t ui32Base))ROM_UARTTABLE[5])

Definition at line 725 of file rom.h.

#define ROM_UARTCharGetNonBlocking   ((int32_t (*)(uint32_t ui32Base))ROM_UARTTABLE[4])

Definition at line 722 of file rom.h.

#define ROM_UARTCharPut
Value:
((void (*)(uint32_t ui32Base, \
uint8_t ui8Data))ROM_UARTTABLE[7])
#define ROM_UARTTABLE
Definition: rom.h:258

Definition at line 732 of file rom.h.

#define ROM_UARTCharPutNonBlocking
Value:
((bool (*)(uint32_t ui32Base, \
uint8_t ui8Data))ROM_UARTTABLE[6])
#define ROM_UARTTABLE
Definition: rom.h:258

Definition at line 728 of file rom.h.

#define ROM_UARTConfigGetExpClk
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32UARTClk, \
uint32_t *pui32Baud, \
uint32_t *pui32Config))ROM_UARTTABLE[2])
#define ROM_UARTTABLE
Definition: rom.h:258

Definition at line 713 of file rom.h.

#define ROM_UARTConfigSetExpClk
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32UARTClk, \
uint32_t ui32Baud, \
uint32_t ui32Config))ROM_UARTTABLE[1])
#define ROM_UARTTABLE
Definition: rom.h:258

Definition at line 707 of file rom.h.

#define ROM_UARTDisable   ((void (*)(uint32_t ui32Base))ROM_UARTTABLE[3])

Definition at line 719 of file rom.h.

#define ROM_UARTFIFOLevelGet
Value:
((void (*)(uint32_t ui32Base, \
uint32_t *pui32TxLevel, \
uint32_t *pui32RxLevel))ROM_UARTTABLE[0])
#define ROM_UARTTABLE
Definition: rom.h:258

Definition at line 702 of file rom.h.

#define ROM_UARTTABLE   ((uint32_t *)(ROM_APITABLE[20]))

Definition at line 258 of file rom.h.

#define ROM_uDMAChannelAttributeDisable
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32ChannelNum, \
uint32_t ui32Attr))ROM_UDMATABLE[1])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 746 of file rom.h.

#define ROM_uDMAChannelAttributeEnable
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32ChannelNum, \
uint32_t ui32Attr))ROM_UDMATABLE[0])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 741 of file rom.h.

#define ROM_uDMAChannelAttributeGet
Value:
((uint32_t (*)(uint32_t ui32Base, \
uint32_t ui32ChannelNum))ROM_UDMATABLE[2])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 751 of file rom.h.

#define ROM_uDMAChannelControlSet
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32ChannelStructIndex, \
uint32_t ui32Control))ROM_UDMATABLE[3])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 755 of file rom.h.

#define ROM_uDMAChannelModeGet
Value:
((uint32_t (*)(uint32_t ui32Base, \
uint32_t ui32ChannelStructIndex))ROM_UDMATABLE[7])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 771 of file rom.h.

#define ROM_uDMAChannelScatterGatherSet
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32ChannelNum, \
uint32_t ui32TaskCount, \
void *pvTaskList, \
uint32_t ui32IsPeriphSG))ROM_UDMATABLE[5])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 760 of file rom.h.

#define ROM_uDMAChannelSizeGet
Value:
((uint32_t (*)(uint32_t ui32Base, \
uint32_t ui32ChannelStructIndex))ROM_UDMATABLE[6])
#define ROM_UDMATABLE
Definition: rom.h:259

Definition at line 767 of file rom.h.

#define ROM_UDMATABLE   ((uint32_t *)(ROM_APITABLE[21]))

Definition at line 259 of file rom.h.

#define ROM_VERSION   (ROM_APITABLE[0])

Definition at line 238 of file rom.h.

#define ROM_VIMSConfigure
Value:
((void (*)(uint32_t ui32Base, \
bool bRoundRobin, \
bool bPrefetch))ROM_VIMSTABLE[0])
#define ROM_VIMSTABLE
Definition: rom.h:260

Definition at line 780 of file rom.h.

#define ROM_VIMSModeSet
Value:
((void (*)(uint32_t ui32Base, \
uint32_t ui32Mode))ROM_VIMSTABLE[1])
#define ROM_VIMSTABLE
Definition: rom.h:260

Definition at line 785 of file rom.h.

#define ROM_VIMSTABLE   ((uint32_t *)(ROM_APITABLE[22]))

Definition at line 260 of file rom.h.

Typedef Documentation

typedef void(* FPTR_ADCCOMPBIN_T) (uint8_t)

Definition at line 109 of file rom.h.

typedef void(* FPTR_COMPAIN_T) (uint8_t)

Definition at line 105 of file rom.h.

typedef void(* FPTR_COMPAREF_T) (uint8_t)

Definition at line 107 of file rom.h.

typedef void(* FPTR_COMPBREF_T) (uint8_t)

Definition at line 111 of file rom.h.

typedef uint32_t(* FPTR_CRC32_T) (uint8_t *, uint32_t, uint32_t)

Definition at line 66 of file rom.h.

typedef uint32_t(* FPTR_FLETCHER32_T) (uint16_t *, uint16_t, uint16_t)

Definition at line 83 of file rom.h.

typedef uint32_t(* FPTR_GETCHIPID_T) (void)

Definition at line 72 of file rom.h.

typedef uint32_t(* FPTR_GETFLSIZE_T) (void)

Definition at line 70 of file rom.h.

typedef void(* FPTR_HFSOURCESAFESWITCH_T) (void)

Definition at line 99 of file rom.h.

typedef uint32_t(* FPTR_MAXVAL_T) (uint32_t *, uint32_t)

Definition at line 90 of file rom.h.

typedef uint32_t(* FPTR_MEANVAL_T) (uint32_t *, uint32_t)

Definition at line 93 of file rom.h.

typedef uint32_t(* FPTR_MINVAL_T) (uint32_t *, uint32_t)

Definition at line 87 of file rom.h.

typedef uint32_t(* FPTR_RESERVED1_T) (uint32_t)

Definition at line 74 of file rom.h.

typedef uint32_t(* FPTR_RESERVED2_T) (void)

Definition at line 76 of file rom.h.

typedef uint32_t(* FPTR_RESERVED3_T) (uint8_t *, uint32_t, uint32_t)

Definition at line 78 of file rom.h.

typedef void(* FPTR_RESERVED4_T) (uint32_t)

Definition at line 101 of file rom.h.

typedef void(* FPTR_RESERVED5_T) (uint32_t)

Definition at line 103 of file rom.h.

typedef void(* FPTR_RESETDEV_T) (void)

Definition at line 81 of file rom.h.

typedef uint32_t(* FPTR_STDDVAL_T) (uint32_t *, uint32_t)

Definition at line 96 of file rom.h.

Function Documentation

uint32_t MemBusWrkAroundHapiEraseSector ( uint32_t  ui32Address)

Definition at line 745 of file flash.c.

uint32_t MemBusWrkAroundHapiProgramFlash ( uint8_t *  pui8DataBuffer,
uint32_t  ui32Address,
uint32_t  ui32Count 
)

Definition at line 715 of file flash.c.

void SafeHapiAuxAdiSelect ( FPTR_VOID_UINT8_T  fPtr,
uint8_t  ut8Signal 
)

Definition at line 53 of file adi.c.

Here is the call graph for this function: