CC13xx Driver Library
[flash] Flash

Functions

static uint32_t FlashSectorSizeGet (void)
 Get size of a flash sector in number of bytes. More...
 
static uint32_t FlashSizeGet (void)
 Get the size of the flash. More...
 
void FlashPowerModeSet (uint32_t ui32PowerMode, uint32_t ui32BankGracePeriode, uint32_t ui32PumpGracePeriode)
 Set power mode. More...
 
uint32_t FlashPowerModeGet (void)
 Get current configured power mode. More...
 
void FlashProtectionSet (uint32_t ui32SectorAddress, uint32_t ui32ProtectMode)
 Set sector protection. More...
 
uint32_t FlashProtectionGet (uint32_t ui32SectorAddress)
 Get sector protection. More...
 
uint32_t FlashProtectionSave (uint32_t ui32SectorAddress)
 Save sector protection to make it permanent. More...
 
static uint32_t FlashCheckFsmForError (void)
 Checks if the Flash state machine has detected an error. More...
 
static uint32_t FlashCheckFsmForReady (void)
 Checks if the Flash state machine is ready. More...
 
static void FlashIntRegister (void(*pfnHandler)(void))
 Registers an interrupt handler for the flash interrupt. More...
 
static void FlashIntUnregister (void)
 Unregisters the interrupt handler for the flash interrupt. More...
 
static void FlashIntEnable (uint32_t ui32IntFlags)
 Enables flash controller interrupt sources. More...
 
static void FlashIntDisable (uint32_t ui32IntFlags)
 Disables individual flash controller interrupt sources. More...
 
static uint32_t FlashIntStatus (void)
 Gets the current interrupt status. More...
 
static void FlashIntClear (uint32_t ui32IntFlags)
 Clears flash controller interrupt source. More...
 
uint32_t FlashSectorErase (uint32_t ui32SectorAddress)
 Erase a flash sector. More...
 
uint32_t FlashProgram (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
 Programs unprotected main bank flash sectors. More...
 
bool FlashEfuseReadRow (uint32_t *pui32EfuseData, uint32_t ui32RowAddress)
 Reads efuse data from specified row. More...
 
void FlashDisableSectorsForWrite (void)
 Disables all sectors for erase and programming on the active bank. More...
 

Enumerations

enum  tFlashStateCommandsType {
  FAPI_PROGRAM_DATA = 0x0002, FAPI_ERASE_SECTOR = 0x0006, FAPI_ERASE_BANK = 0x0008, FAPI_VALIDATE_SECTOR = 0x000E,
  FAPI_CLEAR_STATUS = 0x0010, FAPI_PROGRAM_RESUME = 0x0014, FAPI_ERASE_RESUME = 0x0016, FAPI_CLEAR_MORE = 0x0018,
  FAPI_PROGRAM_SECTOR = 0x0020, FAPI_ERASE_OTP = 0x0030
}
 Defined values for Flash State Machine commands. More...
 

Detailed Description

Function Documentation

static uint32_t FlashCheckFsmForError ( void  )
inlinestatic

Checks if the Flash state machine has detected an error.

This function returns the status of the Flash State Machine indicating if an error is detected or not. Primary use is to check if an Erase or Program operation has failed.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased. This function must be called from ROM or SRAM while any part of the flash is being programmed or erased.
Returns
Returns status of Flash state machine:

Definition at line 436 of file flash.h.

static uint32_t FlashCheckFsmForReady ( void  )
inlinestatic

Checks if the Flash state machine is ready.

This function returns the status of the Flash State Machine indicating if it is ready to accept a new command or not. Primary use is to check if an Erase or Program operation has finished.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased. This function must be called from ROM or SRAMh while any part of the flash is being programmed or erased.
Returns
Returns readiness status of Flash state machine:

Definition at line 466 of file flash.h.

void FlashDisableSectorsForWrite ( void  )

Disables all sectors for erase and programming on the active bank.

This function disables all sectors for erase and programming on the active bank and enables the Idle Reading Power reduction mode if no low power mode is configured. Furthermore, an additional level of protection from erase is enabled.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased.
Returns
None

Definition at line 518 of file flash.c.

Referenced by FlashsafeDisableSectorsForWrite().

Here is the call graph for this function:

bool FlashEfuseReadRow ( uint32_t *  pui32EfuseData,
uint32_t  ui32RowAddress 
)

Reads efuse data from specified row.

This function will read one efuse row. It is assumed that any previous efuse operation has finished.

Parameters
pui32EfuseDatais pointer to variable to be updated with efuse data.
ui32RowAddressis the efuse row number to be read. First row is row number 0.
Returns
Returns the status of the efuse read operation.
  • false : OK status.
  • true : Error status

Definition at line 433 of file flash.c.

static void FlashIntClear ( uint32_t  ui32IntFlags)
inlinestatic

Clears flash controller interrupt source.

The flash controller interrupt source is cleared, so that it no longer asserts. This must be done in the interrupt handler to keep it from being called again immediately upon exit.

Note
Because there is a write buffer in the System CPU, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately re-entered (because the interrupt controller still sees the interrupt source asserted).
Parameters
ui32IntFlagsis the bit mask of the interrupt sources to be cleared. Can be any of:
Returns
None

Definition at line 645 of file flash.h.

Referenced by FlashsafeIntClear().

static void FlashIntDisable ( uint32_t  ui32IntFlags)
inlinestatic

Disables individual flash controller interrupt sources.

This function disables the flash controller interrupt sources.

Parameters
ui32IntFlagsis the bit mask of the interrupt sources to be disabled. The parameter is the bitwise OR of any of the following:
Returns
None

Definition at line 576 of file flash.h.

static void FlashIntEnable ( uint32_t  ui32IntFlags)
inlinestatic

Enables flash controller interrupt sources.

This function enables the flash controller interrupt sources.

Parameters
ui32IntFlagsis the bit mask of the interrupt sources to be enabled. The parameter is the bitwise OR of any of the following:
Returns
None

Definition at line 554 of file flash.h.

static void FlashIntRegister ( void(*)(void)  pfnHandler)
inlinestatic

Registers an interrupt handler for the flash interrupt.

This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller; specific FLASH interrupts must be enabled via FlashIntEnable(). It is the interrupt handler's responsibility to clear the interrupt source.

Parameters
pfnHandleris a pointer to the function to be called when the flash interrupt occurs.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.

Definition at line 497 of file flash.h.

Here is the call graph for this function:

static uint32_t FlashIntStatus ( void  )
inlinestatic

Gets the current interrupt status.

This function returns the interrupt status for the Flash.

Returns
Returns the current interrupt status as values described in FlashIntEnable().

Definition at line 594 of file flash.h.

Referenced by FlashsafeIntStatus().

static void FlashIntUnregister ( void  )
inlinestatic

Unregisters the interrupt handler for the flash interrupt.

This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a FLASH interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

Returns
None
See also
IntRegister() for important information about registering interrupt handlers.

Definition at line 526 of file flash.h.

Here is the call graph for this function:

uint32_t FlashPowerModeGet ( void  )

Get current configured power mode.

This function will return the current configured power mode.

Returns
Returns the current configured power mode. The defined power modes are:

Definition at line 192 of file flash.c.

Referenced by FlashsafePowerModeGet().

void FlashPowerModeSet ( uint32_t  ui32PowerMode,
uint32_t  ui32BankGracePeriode,
uint32_t  ui32PumpGracePeriode 
)

Set power mode.

This function will set the specified power mode.

Any access to the bank causes a reload of the specified bank grace periode input value into the bank down counter. After the last access to the flash bank, the down counter delays from 0 to 255 prescaled HCLK clock cycles before putting the bank into one of the fallback power modes as determined by ui32PowerMode. This value must be greater than 1 when the fallback mode is not FLASH_PWR_ACTIVE_MODE.

Note: The prescaled clock used for the down counter is a clock divided by 16 from input HCLK. The ui32BankGracePeriode parameter is ignored if ui32PowerMode is equal to FLASH_PWR_ACTIVE_MODE. Any access to flash memory causes the pump grace periode down counter to reload with value of ui32PumpGracePeriode. After the bank has gone to sleep, the down counter delays this number of prescaled HCLK clock cycles before entering one of the charge pump fallback power modes as determined by ui32PowerMode. The prescaled clock used for the pump grace periode down counter is a clock divided by 16 from input HCLK. This parameter is ignored if ui32PowerMode is equal to FLASH_PWR_ACTIVE_MODE.

Changing the power mode of the flash module must be a part within a device power mode transition requiring configuration of multiple modules. Refer to documents describing the device power modes.

Parameters
ui32PowerModeis the wanted power mode. The defined flash power modes are:
ui32BankGracePeriodeis the starting count value for the bank grace periode down counter.
ui32PumpGracePeriodeis the starting count value for the pump grace periode down counter.
Returns
None

Definition at line 101 of file flash.c.

Referenced by FlashsafePowerModeSet().

uint32_t FlashProgram ( uint8_t *  pui8DataBuffer,
uint32_t  ui32Address,
uint32_t  ui32Count 
)

Programs unprotected main bank flash sectors.

This function will program a sequence of bytes into the on-chip flash. Programming each location consists of the result of an AND operation of the new data and the existing data; in other words bits that contain 1 can remain 1 or be changed to 0, but bits that are 0 cannot be changed to 1. Therefore, a byte can be programmed multiple times as long as these rules are followed; if a program operation attempts to change a 0 bit to a 1 bit, that bit will not have its value changed.

This function will not return until the data has been programmed or an programming error has occurred.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased. This function must only be executed from ROM or SRAM.

The pui8DataBuffer pointer can not point to flash.

Parameters
pui8DataBufferis a pointer to the data to be programmed.
ui32Addressis the starting address in flash to be programmed.
ui32Countis the number of bytes to be programmed.
Returns
Returns status of the flash programming:

Definition at line 399 of file flash.c.

Referenced by FlashProtectionSave(), and FlashsafeProgram().

Here is the call graph for this function:

uint32_t FlashProtectionGet ( uint32_t  ui32SectorAddress)

Get sector protection.

This return the protection mode for the specified flash bank sector.

Parameters
ui32SectorAddressis the start address of the desired sector.
Returns
Returns the sector protection:

Definition at line 265 of file flash.c.

Referenced by FlashProtectionSave(), and FlashsafeProtectionGet().

Here is the call graph for this function:

uint32_t FlashProtectionSave ( uint32_t  ui32SectorAddress)

Save sector protection to make it permanent.

This function will save the current protection mode for the specified flash bank sector.

This function must only be executed from ROM or SRAM.

Note
A write protected sector will become permanent write protected!! A device reset will not change the write protection!
Parameters
ui32SectorAddressis the start address of the sector to be protected.
Returns
Returns the status of the sector protection:

Definition at line 308 of file flash.c.

Referenced by FlashsafeProtectionSave().

Here is the call graph for this function:

void FlashProtectionSet ( uint32_t  ui32SectorAddress,
uint32_t  ui32ProtectMode 
)

Set sector protection.

This function will set the specified protection on specified flash bank sector. A sector can either have no protection or have write protection which guards for both program and erase of that sector. Sector protection can only be changed from FLASH_NO_PROTECT to FLASH_WRITE_PROTECT! After write protecting a sector this sector can only be set back to unprotected by a device reset.

Parameters
ui32SectorAddressis the start address of the sector to protect.
ui32ProtectModeis the enumerated sector protection mode.
Returns
None

Definition at line 225 of file flash.c.

Referenced by FlashsafeProtectionSet().

Here is the call graph for this function:

uint32_t FlashSectorErase ( uint32_t  ui32SectorAddress)

Erase a flash sector.

This function will erase the specified flash sector. The function will not return until the flash sector has been erased or an error condition occurred. If flash top sector is erased the function will program the the device security data bytes with default values. The device security data located in the customer configuration area of the flash top sector, must have valid values at all times. These values affect the configuration of the device during boot.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased. This function must only be executed from ROM or SRAM.
Parameters
ui32SectorAddressis the starting address in flash of the sector to be erased.
Returns
Returns the status of the sector erase:

Definition at line 362 of file flash.c.

Referenced by FlashsafeSectorErase().

Here is the call graph for this function:

static uint32_t FlashSectorSizeGet ( void  )
inlinestatic

Get size of a flash sector in number of bytes.

This function will return the size of a flash sector in number of bytes.

Returns
Returns size of a flash sector in number of bytes.

Definition at line 259 of file flash.h.

Referenced by FlashProtectionGet(), FlashProtectionSave(), FlashProtectionSet(), FlashsafeSectorSizeGet(), FlashSectorErase(), and FlashSizeGet().

static uint32_t FlashSizeGet ( void  )
inlinestatic

Get the size of the flash.

This function returns the size of the flash main bank in number of bytes.

Returns
Returns the flash size in number of bytes.

Definition at line 283 of file flash.h.

Referenced by FlashProgram(), FlashProtectionGet(), FlashProtectionSave(), FlashProtectionSet(), FlashsafeSizeGet(), and FlashSectorErase().

Here is the call graph for this function:

Macro Definition Documentation

#define ADDR_OFFSET   (0x1F800000 - FLASHMEM_BASE)

Definition at line 143 of file flash.h.

#define CCFG_OFFSET_SECT_PROT   0x00000FF0

Definition at line 245 of file flash.h.

Referenced by FlashProtectionSave().

#define CCFG_OFFSET_SECURITY   0x00000FD8

Definition at line 244 of file flash.h.

#define CCFG_SIZE_SECT_PROT   0x00000004

Definition at line 247 of file flash.h.

Referenced by FlashProtectionSave().

#define CCFG_SIZE_SECURITY   0x00000014

Definition at line 246 of file flash.h.

#define DUMPWORD_INSTR   0x04

Definition at line 230 of file flash.h.

Referenced by FlashEfuseReadRow().

#define FAPI_STATUS_FSM_BUSY   0x00000001

Definition at line 104 of file flash.h.

Referenced by FlashCheckFsmForReady(), and FlashsafeCheckFsmForReady().

#define FAPI_STATUS_FSM_ERROR   0x00000004

Definition at line 108 of file flash.h.

Referenced by FlashCheckFsmForError(), and FlashsafeCheckFsmForError().

#define FAPI_STATUS_FSM_READY   0x00000002

Definition at line 105 of file flash.h.

Referenced by FlashCheckFsmForReady(), and FlashsafeCheckFsmForReady().

#define FAPI_STATUS_INCORRECT_DATABUFFER_LENGTH   0x00000003

Definition at line 106 of file flash.h.

#define FAPI_STATUS_SUCCESS   0x00000000

Definition at line 103 of file flash.h.

Referenced by FlashCheckFsmForError(), FlashProtectionSave(), and FlashsafeCheckFsmForError().

#define FBFALLBACK_ACTIVE   3

Definition at line 193 of file flash.h.

Referenced by FlashPowerModeSet().

#define FBFALLBACK_DEEP_STDBY   1

Definition at line 192 of file flash.h.

Referenced by FlashPowerModeGet(), and FlashPowerModeSet().

#define FBFALLBACK_SLEEP   0

Definition at line 191 of file flash.h.

Referenced by FlashPowerModeGet().

#define FCFG1_OFFSET   0x1000

Definition at line 150 of file flash.h.

Referenced by SetReadMode().

#define FLASH_BAGP   0x14

Definition at line 200 of file flash.h.

#define FLASH_CMD_EXEC   0x15

Definition at line 237 of file flash.h.

#define FLASH_INT_FSM_DONE   0x00400000

Definition at line 116 of file flash.h.

Referenced by FlashIntClear(), and FlashIntStatus().

#define FLASH_INT_RV   0x00010000

Definition at line 117 of file flash.h.

Referenced by FlashIntClear(), and FlashIntStatus().

#define FLASH_MODULE_CLK_FREQ   48

Definition at line 157 of file flash.h.

#define FLASH_NO_PROTECT   0x00000000

Definition at line 134 of file flash.h.

Referenced by FlashProtectionGet().

#define FLASH_PAGP   0x14

Definition at line 201 of file flash.h.

#define FLASH_PWR_ACTIVE_MODE   0x00000000

Definition at line 124 of file flash.h.

Referenced by FlashPowerModeGet(), FlashPowerModeSet(), and FlashsafePowerModeSet().

#define FLASH_PWR_DEEP_STDBY_MODE   0x00000002

Definition at line 126 of file flash.h.

Referenced by FlashPowerModeGet(), FlashPowerModeSet(), and FlashsafePowerModeSet().

#define FLASH_PWR_OFF_MODE   0x00000001

Definition at line 125 of file flash.h.

Referenced by FlashPowerModeGet(), FlashPowerModeSet(), and FlashsafePowerModeSet().

#define FLASH_WRITE_PROTECT   0x00000001

Definition at line 135 of file flash.h.

Referenced by FlashProtectionGet(), FlashProtectionSave(), and FlashProtectionSet().

#define FSM_REG_WRT_DISABLE   2
#define FSM_REG_WRT_ENABLE   5
#define FW_WRT_TRIMMED   0x00000001

Definition at line 215 of file flash.h.

#define FWPWRITE_BYTE_ADDRESS   ((tFwpWriteByte *)((FLASH_BASE + FLASH_O_FWPWRITE0)))

Definition at line 223 of file flash.h.

#define PATTERN_BITS   0x20

Definition at line 208 of file flash.h.

Enumeration Type Documentation

Defined values for Flash State Machine commands.

Enumerator
FAPI_PROGRAM_DATA 

Program data.

FAPI_ERASE_SECTOR 

Erase sector.

FAPI_ERASE_BANK 

Erase bank.

FAPI_VALIDATE_SECTOR 

Validate sector.

FAPI_CLEAR_STATUS 

Clear status.

FAPI_PROGRAM_RESUME 

Program resume.

FAPI_ERASE_RESUME 

Erase resume.

FAPI_CLEAR_MORE 

Clear more.

FAPI_PROGRAM_SECTOR 

Program sector.

FAPI_ERASE_OTP 

Erase OTP.

Definition at line 164 of file flash.h.