CC13xx Driver Library
[flashsafe] Flash Safe

Functions

static bool FlashsafeSMPHTryAcquire (void)
 Aquire the flash semaphore. More...
 
static void FlashsafeSMPHRelease (void)
 Release the flash semaphore. More...
 
uint32_t FlashsafeSizeGet (void)
 Get the size of the flash. More...
 
uint32_t FlashsafeSectorSizeGet (void)
 Get size of a flash sector in no of bytes. More...
 
uint32_t FlashsafePowerModeSet (uint32_t ui32PowerMode, uint32_t ui32BankGracePeriode, uint32_t ui32PumpGracePeriode)
 Set power mode. More...
 
uint32_t FlashsafePowerModeGet (void)
 Get current configured power mode. More...
 
uint32_t FlashsafeProtectionSet (uint32_t ui32SectorAddress, uint32_t ui32ProtectMode)
 Set sector protection. More...
 
uint32_t FlashsafeProtectionGet (uint32_t ui32SectorAddress)
 Get sector protection. More...
 
uint32_t FlashsafeProtectionSave (uint32_t ui32SectorAddress)
 Save sector protection to make it permanent. More...
 
uint32_t FlashsafeCheckFsmForError (void)
 Checks if the Flashsafe state machine has detected an error. More...
 
uint32_t FlashsafeCheckFsmForReady (void)
 Checks if the Flash state machine is ready. More...
 
uint32_t FlashsafeIntRegister (void(*pfnHandler)(void))
 Registers an interrupt handler for the flash interrupt. More...
 
uint32_t FlashsafeIntUnregister (void)
 Unregisters the interrupt handler for the flash interrupt. More...
 
uint32_t FlashsafeIntEnable (uint32_t ui32IntFlags)
 Enables flash controller interrupt sources. More...
 
uint32_t FlashsafeIntDisable (uint32_t ui32IntFlags)
 Disables individual flash controller interrupt sources. More...
 
uint32_t FlashsafeIntStatus (void)
 Gets the current interrupt status. More...
 
uint32_t FlashsafeIntClear (uint32_t ui32IntFlags)
 Clears flash controller interrupt source. More...
 
uint32_t FlashsafeSectorErase (uint32_t ui32SectorAddress)
 Erase a flash sector. More...
 
uint32_t FlashsafeProgram (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
 Programs unprotected main bank flash sectors. More...
 
uint32_t FlashsafeDisableSectorsForWrite (void)
 Disables all sectors for erase and programming on the active bank. More...
 

Detailed Description

Function Documentation

uint32_t FlashsafeCheckFsmForError ( void  )

Checks if the Flashsafe state machine has detected an error.

This function returns the status of the Flashsafe State Machine indicating if an error is detected or not. Primary use is to check if an Erase or Program operation has failed.

Returns
Returns status of Flashsafe state machine:

Definition at line 243 of file flashsafe.c.

uint32_t FlashsafeCheckFsmForReady ( void  )

Checks if the Flash state machine is ready.

This function returns the status of the Flash State Machine indicating if it is ready to accept a new command or not. Primary use is to check if an Erase or Program operation has finished.

Returns
Returns readiness status of Flash state machine:

Definition at line 261 of file flashsafe.c.

uint32_t FlashsafeDisableSectorsForWrite ( void  )

Disables all sectors for erase and programming on the active bank.

This function disables all sectors for erase and programming on the active bank and enables the Idle Reading Power reduction mode if no low power mode is configured. Furthermore, an additional level of protection from erase is enabled.

Returns
Returns the status of the flash sector erase disable:

Definition at line 457 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeIntClear ( uint32_t  ui32IntFlags)

Clears flash controller interrupt source.

The flash controller interrupt source is cleared, so that it no longer assert. This must be done in the interrupt handler to keep it from being called again immediately upon exit.

Note
Because there is a write buffer in the System CPU, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately reentered (because the interrupt controller still sees the interrupt source asserted).
Parameters
ui32IntFlagsis the bit mask of the interrupt sources to be cleared. Can be any of:
Returns
Returns status of the flash interrupt source clearing:

Definition at line 385 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeIntDisable ( uint32_t  ui32IntFlags)

Disables individual flash controller interrupt sources.

This function disables the flash controller interrupt sources.

Parameters
ui32IntFlagsis the bit mask of the interrupt sources to be disabled. The parameter is the bitwise OR of any of the following:
Returns
Returns status of function call:

Definition at line 354 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeIntEnable ( uint32_t  ui32IntFlags)

Enables flash controller interrupt sources.

This function enables the flash controller interrupt sources.

Parameters
ui32IntFlagsis the bit mask of the interrupt sources to be enabled. The parameter is the bitwise OR of any of the following:
Returns
Returns status of the function call:

Definition at line 333 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeIntRegister ( void(*)(void)  pfnHandler)

Registers an interrupt handler for the flash interrupt.

This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller; specific FLASH interrupts must be enabled via FlashsafeIntEnable(). It is the interrupt handler's responsibility to clear the interrupt source.

Parameters
pfnHandleris a pointer to the function to be called when the flash interrupt occurs.
Returns
Returns the status of the flash registering:
See also
IntRegister() for important information about registering interrupt handlers.

Definition at line 279 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeIntStatus ( void  )

Gets the current interrupt status.

This function returns the interrupt status for the Flash.

Returns
Returns the current interrupt status:

Definition at line 374 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeIntUnregister ( void  )

Unregisters the interrupt handler for the flash interrupt.

This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a FLASH interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

Returns
Returns status of the flash unregistering:
See also
IntRegister() for important information about registering interrupt handlers.

Definition at line 306 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafePowerModeGet ( void  )

Get current configured power mode.

This function will return the current configured power mode.

Returns
Returns FLASHSAFE_ACCESS_DENIED if flash is blocked by another thread, otherwise the current configured power mode:

Definition at line 144 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafePowerModeSet ( uint32_t  ui32PowerMode,
uint32_t  ui32BankGracePeriode,
uint32_t  ui32PumpGracePeriode 
)

Set power mode.

This function will set the specified power mode.

Any access to the bank causes a reload of the specified bank grace periode input value into the bank down counter. After the last access to the flash bank, the down counter delays from 0 to 255 prescaled HCLK clock cycles before putting the bank into one of the fallback power modes as determined by ui32PowerMode. This value must be greater than 1 when the fallback mode is not FLASH_PWR_ACTIVE_MODE.

Note: The prescaled clock used for the down counter is a clock divided by 16 from input HCLK. The ui32BankGracePeriode parameter is ignored if ui32PowerMode is equal to FLASH_PWR_ACTIVE_MODE. Any access to flash memory causes the pump grace periode down counter to reload with value of ui32PumpGracePeriode. After the bank has gone to sleep, the down counter delays this number of prescaled HCLK clock cycles before entering one of the charge pump fallback power modes as determined by ui32PowerMode. The prescaled clock used for the pump grace periode down counter is a clock divided by 16 from input HCLK. This parameter is ignored if ui32PowerMode is equal to FLASH_PWR_ACTIVE_MODE.

In current flash module design the SW application has to call the FlashsafePowerModeSet() funtion with the FLASH_PWR_ACTIVE_MODE input parameter value if the flash modules comes out of any of the two low power modes, in in order to reestablish the factory configured idle reading power reduction mode.

Changing the power mode of the flash module must be a part within a device power mode transition requiring configuration of multiple modules. Refer to documents describing the device power modes.

Parameters
ui32PowerModeis the wanted power mode. The defined power modes are:
ui32BankGracePeriodeis the starting count value for the bank grace periode down counter.
ui32PumpGracePeriodeis the starting count value for the pump grace periode down counter.
Returns
Returns the status of the power mode setting:

Definition at line 115 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeProgram ( uint8_t *  pui8DataBuffer,
uint32_t  ui32Address,
uint32_t  ui32Count 
)

Programs unprotected main bank flash sectors.

This function will program a sequence of bytes into the on-chip flash. Programming each location consists of the result of an AND operation of the new data and the existing data; in other words bits that contain 1 can remain 1 or be changed to 0, but bits that are 0 cannot be changed to 1. Therefore, a byte can be programmed multiple times as long as these rules are followed; if a program operation attempts to change a 0 bit to a 1 bit, that bit will not have its value changed.

This function will not return until the data has been programmed or an programming error has occurred.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased. The actual programming function called by this function must only be executed from ROM or SRAM.

The pui8DataBuffer pointer can not point to flash.

Parameters
pui8DataBufferis a pointer to the data to be programmed.
ui32Addressis the starting address in flash to be programmed.
ui32Countis the number of bytes to be programmed.
Returns
Returns status of flash sector program:

Definition at line 431 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeProtectionGet ( uint32_t  ui32SectorAddress)

Get sector protection.

This return the protection mode for the specified flash bank sector.

Parameters
ui32SectorAddressis the start address of the desired sector.
Returns
Returns FLASHSAFE_ACCESS_DENIED if flash is used by another thread, else the sector protection:

Definition at line 189 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeProtectionSave ( uint32_t  ui32SectorAddress)

Save sector protection to make it permanent.

This function will save the the current protection mode for the specified flash bank sector. A write protected sector will become permanent write protected!! A device reset will not change the write protection!

Note
The actual protection save function called by this function must only be executed from ROM or SRAM.
Parameters
ui32SectorAddressis the start address of the sector to be protected.
Returns
Returns status of the flash sector protection:

Definition at line 216 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeProtectionSet ( uint32_t  ui32SectorAddress,
uint32_t  ui32ProtectMode 
)

Set sector protection.

This function will set the specified protection on specified flash bank sector. A sector can either have no protection or have write protection which guards for both program and erase of that sector. Sector protection can only be changed from FLASH_NO_PROTECT to FLASH_WRITE_PROTECT!

Note
After write protecting a sector this sector can only be set back to unprotected by a device reset.
Parameters
ui32SectorAddressis the start address of the sector to protect.
ui32ProtectModeis the enumerated sector protection mode. The defined sector protection modes are:
Returns
Returns status of the sector protection:

Definition at line 164 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeSectorErase ( uint32_t  ui32SectorAddress)

Erase a flash sector.

This function will erase the specified flash sector. The function will not return until the flash sector has been erased or an error condition occurred. If flash top sector is erased the function will program the the device security data bytes with default values. The device security data located in the customer configuration area of the flash top sector, must have valid values at all times. These values affects the configuration of the device during boot.

Note
Please note that code can not execute in flash while any part of the flash is being programmed or erased. The actual erase function called by this function must only be executed from ROM or SRAM.
Parameters
ui32SectorAddressis the starting address in flash of the sector to be erased.
Returns
Returns status of flash sector erase:

Definition at line 403 of file flashsafe.c.

Here is the call graph for this function:

uint32_t FlashsafeSectorSizeGet ( void  )

Get size of a flash sector in no of bytes.

This function will return the size of a flash sector in number of bytes.

Returns
Returns size of a flash sector in number of bytes.

Definition at line 104 of file flashsafe.c.

Referenced by FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().

Here is the call graph for this function:

uint32_t FlashsafeSizeGet ( void  )

Get the size of the flash.

This function returns the size of the flash main bank in number of bytes.

Returns
Returns the flash size in number of bytes.

Definition at line 93 of file flashsafe.c.

Referenced by FlashsafeProgram(), FlashsafeProtectionGet(), FlashsafeProtectionSave(), FlashsafeProtectionSet(), and FlashsafeSectorErase().

Here is the call graph for this function:

static void FlashsafeSMPHRelease ( void  )
inlinestatic
static bool FlashsafeSMPHTryAcquire ( void  )
inlinestatic

Macro Definition Documentation

#define FAPI_STATUS_FSM_BUSY   0x00000001

Definition at line 126 of file flashsafe.h.

#define FAPI_STATUS_FSM_ERROR   0x00000004

Definition at line 130 of file flashsafe.h.

#define FAPI_STATUS_FSM_READY   0x00000002

Definition at line 127 of file flashsafe.h.

#define FAPI_STATUS_INCORRECT_DATABUFFER_LENGTH   0x00000003

Definition at line 128 of file flashsafe.h.

#define FAPI_STATUS_SUCCESS   0x00000000

Definition at line 125 of file flashsafe.h.

#define FLASH_INT_FSM_DONE   0x00400000

Definition at line 138 of file flashsafe.h.

#define FLASH_INT_RV   0x00010000

Definition at line 139 of file flashsafe.h.

#define FLASH_NO_PROTECT   0x00000000

Definition at line 156 of file flashsafe.h.

#define FLASH_PWR_ACTIVE_MODE   0x00000000

Definition at line 146 of file flashsafe.h.

#define FLASH_PWR_DEEP_STDBY_MODE   0x00000002

Definition at line 148 of file flashsafe.h.

#define FLASH_PWR_OFF_MODE   0x00000001

Definition at line 147 of file flashsafe.h.

#define FLASH_WRITE_PROTECT   0x00000001

Definition at line 157 of file flashsafe.h.

#define FSM_REG_WRT_DISABLE   2

Definition at line 166 of file flashsafe.h.

#define FSM_REG_WRT_ENABLE   5

Definition at line 165 of file flashsafe.h.

#define SMPH_ALLOC_FLASH   1

Definition at line 118 of file flashsafe.h.

Referenced by FlashsafeSMPHRelease(), and FlashsafeSMPHTryAcquire().