![]() |
![]() |
SysLink API Reference
2.21.01.05
|
RingIOShm shared memory based physical transport for communication with another client.
This file contains the declarations of types and APIs as part of interface of the RingIOShm shared memory transport.
Go to the source code of this file.
Data Structures | |
struct | RingIOShm_Params_Tag |
Structure defining parameters for creating the RingIOShm instances. More... |
Macros | |
#define | RingIOShm_MODULEID (0x3bff) |
Unique module ID. | |
#define | RingIOShm_E_INVALIDARG RingIO_E_INVALIDARG |
Argument passed to a function is invalid. | |
#define | RingIOShm_E_INVALIDSTATE RingIO_E_INVALIDSTATE |
Module is not initialized. | |
#define | RingIOShm_E_BADVERSION RingIO_E_BADVERSION |
Versions don't match. | |
#define | RingIOShm_E_FAIL RingIO_E_FAIL |
General Failure. | |
#define | RingIOShm_E_MEMORY RingIO_E_MEMORY |
Memory allocation failed. | |
#define | RingIOShm_E_OSFAILURE RingIO_E_OSFAILURE |
Failure in OS call. | |
#define | RingIOShm_E_BUFWRAP RingIO_E_BUFWRAP |
Indicates that the amount of data requested could not be serviced due to the ring buffer getting wrapped. | |
#define | RingIOShm_E_BUFEMPTY RingIO_E_BUFEMPTY |
Indicates that there is no data in the buffer for reading. | |
#define | RingIOShm_E_BUFFULL RingIO_E_BUFFULL |
Indicates that the buffer is full. | |
#define | RingIOShm_E_PENDINGDATA RingIO_E_PENDINGDATA |
Indicates that there is no attribute at the current offset, but attributes are present at a future offset. | |
#define | RingIOShm_E_VARIABLEATTRIBUTE RingIO_E_VARIABLEATTRIBUTE |
Indicates that getAttribute() failed, need to extract variable length message using getvAttribute() | |
#define | RingIOShm_E_WRONGSTATE RingIO_E_WRONGSTATE |
Indicates that the RingIO is in a wrong state. | |
#define | RingIOShm_E_INVALIDPROCID RingIO_E_INVALIDPROCID |
Indicates that an invalid proc id has been specified. | |
#define | RingIOShm_E_INVALIDCONTEXT RingIO_E_INVALIDCONTEXT |
Indicates that the api is called with wrong handle. | |
#define | RingIOShm_S_SUCCESS RingIO_S_SUCCESS |
Operation successful. | |
#define | RingIOShm_S_ALREADYSETUP RingIO_S_ALREADYSETUP |
The module has been already setup. | |
#define | RingIOShm_S_PENDINGATTRIBUTE RingIO_S_PENDINGATTRIBUTE |
Indicates that either: 1) The amount of data requested could not be serviced due to the presence of an attribute 2) During an attribute read if another is also present at the same offset. |
Typedefs | |
typedef struct RingIOShm_Params_Tag | RingIOShm_Params |
Structure defining parameters for creating the RingIOShm instances. |
Functions | |
Void | RingIOShm_Params_init (Void *params) |
Function to initialize the parameters for the RingIOShm instance. |
#define RingIOShm_MODULEID (0x3bff) |
Unique module ID.
#define RingIOShm_E_INVALIDARG RingIO_E_INVALIDARG |
Argument passed to a function is invalid.
#define RingIOShm_E_INVALIDSTATE RingIO_E_INVALIDSTATE |
Module is not initialized.
#define RingIOShm_E_BADVERSION RingIO_E_BADVERSION |
Versions don't match.
#define RingIOShm_E_FAIL RingIO_E_FAIL |
General Failure.
#define RingIOShm_E_MEMORY RingIO_E_MEMORY |
Memory allocation failed.
#define RingIOShm_E_OSFAILURE RingIO_E_OSFAILURE |
Failure in OS call.
#define RingIOShm_E_BUFWRAP RingIO_E_BUFWRAP |
Indicates that the amount of data requested could not be serviced due to the ring buffer getting wrapped.
#define RingIOShm_E_BUFEMPTY RingIO_E_BUFEMPTY |
Indicates that there is no data in the buffer for reading.
#define RingIOShm_E_BUFFULL RingIO_E_BUFFULL |
Indicates that the buffer is full.
#define RingIOShm_E_PENDINGDATA RingIO_E_PENDINGDATA |
Indicates that there is no attribute at the current offset, but attributes are present at a future offset.
#define RingIOShm_E_VARIABLEATTRIBUTE RingIO_E_VARIABLEATTRIBUTE |
Indicates that getAttribute() failed, need to extract variable length message using getvAttribute()
#define RingIOShm_E_WRONGSTATE RingIO_E_WRONGSTATE |
Indicates that the RingIO is in a wrong state.
#define RingIOShm_E_INVALIDPROCID RingIO_E_INVALIDPROCID |
Indicates that an invalid proc id has been specified.
#define RingIOShm_E_INVALIDCONTEXT RingIO_E_INVALIDCONTEXT |
Indicates that the api is called with wrong handle.
#define RingIOShm_S_SUCCESS RingIO_S_SUCCESS |
Operation successful.
#define RingIOShm_S_ALREADYSETUP RingIO_S_ALREADYSETUP |
The module has been already setup.
#define RingIOShm_S_PENDINGATTRIBUTE RingIO_S_PENDINGATTRIBUTE |
Indicates that either: 1) The amount of data requested could not be serviced due to the presence of an attribute 2) During an attribute read if another is also present at the same offset.
typedef struct RingIOShm_Params_Tag RingIOShm_Params |
Structure defining parameters for creating the RingIOShm instances.
Function to initialize the parameters for the RingIOShm instance.
This function can be called by the application to get their configuration parameter to RingIO_create filled in by the RingIOShm module with the default parameters.
params | Pointer to the RingIOShm instance params structure in which the default params is to be returned. |
None |