![]() |
![]() |
SysLink API Reference
2.21.01.05
|
This will have definitions of standard data types for platform abstraction.
Go to the source code of this file.
Macros | |
#define | Void void |
#define | TRUE 1 |
#define | FALSE 0 |
#define | Error_init(eb) *eb = 0 |
Typedefs | |
typedef char | Char |
typedef unsigned char | UChar |
typedef short | Short |
typedef unsigned short | UShort |
typedef int | Int |
typedef unsigned int | UInt |
typedef long | Long |
typedef unsigned long | ULong |
typedef float | Float |
typedef double | Double |
typedef long double | LDouble |
typedef unsigned short | Bool |
typedef void * | Ptr |
typedef char * | String |
typedef const char * | CString |
typedef int * | IArg |
typedef unsigned int * | UArg |
typedef char | Int8 |
typedef short | Int16 |
typedef int | Int32 |
typedef unsigned char | UInt8 |
typedef unsigned short | UInt16 |
typedef unsigned int | UInt32 |
typedef unsigned int | SizeT |
typedef unsigned char | Bits8 |
typedef unsigned short | Bits16 |
typedef UInt32 | Bits32 |
typedef UInt32 | Error_Block |
#define Void void |
#define TRUE 1 |
#define FALSE 0 |
#define Error_init | ( | eb | ) | *eb = 0 |
Initialize error block
typedef char Char |
typedef unsigned char UChar |
typedef short Short |
typedef unsigned short UShort |
typedef int Int |
typedef unsigned int UInt |
typedef long Long |
typedef unsigned long ULong |
typedef float Float |
typedef double Double |
typedef long double LDouble |
typedef unsigned short Bool |
typedef void* Ptr |
typedef char* String |
typedef const char* CString |
typedef int* IArg |
typedef unsigned int* UArg |
typedef char Int8 |
typedef short Int16 |
typedef int Int32 |
typedef unsigned char UInt8 |
typedef unsigned short UInt16 |
typedef unsigned int UInt32 |
typedef unsigned int SizeT |
typedef unsigned char Bits8 |
typedef unsigned short Bits16 |
typedef UInt32 Error_Block |
Data type for errors