enum Flash_2xx.ACCVIFG_t |
![](../../../../../Arrow_up.png) |
Access violation interrupt flag
XDCscript usage |
meta-domain |
values of type Flash_2xx.ACCVIFG_t
const Flash_2xx.ACCVIFG_OFF;
const Flash_2xx.ACCVIFG;
enum Flash_2xx.BLKWRT_t |
![](../../../../../Arrow_up.png) |
Block write mode
XDCscript usage |
meta-domain |
values of type Flash_2xx.BLKWRT_t
const Flash_2xx.BLKWRT_OFF;
const Flash_2xx.BLKWRT;
enum Flash_2xx.BUSY_t |
![](../../../../../Arrow_up.png) |
Busy
XDCscript usage |
meta-domain |
values of type Flash_2xx.BUSY_t
const Flash_2xx.BUSY_OFF;
const Flash_2xx.BUSY;
enum Flash_2xx.EEIEX_t |
![](../../../../../Arrow_up.png) |
Enable Emergency Interrupt Exit
XDCscript usage |
meta-domain |
values of type Flash_2xx.EEIEX_t
const Flash_2xx.EEIEX_OFF;
const Flash_2xx.EEIEX;
enum Flash_2xx.EEI_t |
![](../../../../../Arrow_up.png) |
Enable Erase Interrupts
XDCscript usage |
meta-domain |
values of type Flash_2xx.EEI_t
const Flash_2xx.EEI_OFF;
const Flash_2xx.EEI;
enum Flash_2xx.EMEX_t |
![](../../../../../Arrow_up.png) |
Emergency exit
XDCscript usage |
meta-domain |
values of type Flash_2xx.EMEX_t
const Flash_2xx.EMEX_OFF;
const Flash_2xx.EMEX;
enum Flash_2xx.ERASE_t |
![](../../../../../Arrow_up.png) |
Erase
XDCscript usage |
meta-domain |
values of type Flash_2xx.ERASE_t
const Flash_2xx.ERASE_OFF;
const Flash_2xx.ERASE;
enum Flash_2xx.FAIL_t |
![](../../../../../Arrow_up.png) |
Operation failure
XDCscript usage |
meta-domain |
values of type Flash_2xx.FAIL_t
const Flash_2xx.FAIL_OFF;
const Flash_2xx.FAIL;
enum Flash_2xx.FN0_t |
![](../../../../../Arrow_up.png) |
Flash controller clock divider bit 0
XDCscript usage |
meta-domain |
values of type Flash_2xx.FN0_t
const Flash_2xx.FN0_OFF;
const Flash_2xx.FN0;
enum Flash_2xx.FN1_t |
![](../../../../../Arrow_up.png) |
Flash controller clock divider bit 1
XDCscript usage |
meta-domain |
values of type Flash_2xx.FN1_t
const Flash_2xx.FN1_OFF;
const Flash_2xx.FN1;
enum Flash_2xx.FN2_t |
![](../../../../../Arrow_up.png) |
Flash controller clock divider bit 2
XDCscript usage |
meta-domain |
values of type Flash_2xx.FN2_t
const Flash_2xx.FN2_OFF;
const Flash_2xx.FN2;
enum Flash_2xx.FN3_t |
![](../../../../../Arrow_up.png) |
Flash controller clock divider bit 3
XDCscript usage |
meta-domain |
values of type Flash_2xx.FN3_t
const Flash_2xx.FN3_OFF;
const Flash_2xx.FN3;
enum Flash_2xx.FN4_t |
![](../../../../../Arrow_up.png) |
Flash controller clock divider bit 4
XDCscript usage |
meta-domain |
values of type Flash_2xx.FN4_t
const Flash_2xx.FN4_OFF;
const Flash_2xx.FN4;
enum Flash_2xx.FN5_t |
![](../../../../../Arrow_up.png) |
Flash controller clock divider bit 5
XDCscript usage |
meta-domain |
values of type Flash_2xx.FN5_t
const Flash_2xx.FN5_OFF;
const Flash_2xx.FN5;
enum Flash_2xx.FSSEL_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type Flash_2xx.FSSEL_t
const Flash_2xx.FSSEL_0;
// ACLK
const Flash_2xx.FSSEL_1;
// MCLK
const Flash_2xx.FSSEL_2;
// SMCLK
const Flash_2xx.FSSEL_3;
// SMCLK
enum Flash_2xx.FWKEY_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type Flash_2xx.FWKEY_t
const Flash_2xx.FWKEY_OFF;
const Flash_2xx.FWKEY;
enum Flash_2xx.KEYV_t |
![](../../../../../Arrow_up.png) |
Flash security key violation
XDCscript usage |
meta-domain |
values of type Flash_2xx.KEYV_t
const Flash_2xx.KEYV_OFF;
const Flash_2xx.KEYV;
enum Flash_2xx.LOCKA_t |
![](../../../../../Arrow_up.png) |
SegmentA and Info lock
XDCscript usage |
meta-domain |
values of type Flash_2xx.LOCKA_t
const Flash_2xx.LOCKA_OFF;
const Flash_2xx.LOCKA;
enum Flash_2xx.LOCK_t |
![](../../../../../Arrow_up.png) |
Lock
XDCscript usage |
meta-domain |
values of type Flash_2xx.LOCK_t
const Flash_2xx.LOCK_OFF;
const Flash_2xx.LOCK;
enum Flash_2xx.MERAS_t |
![](../../../../../Arrow_up.png) |
Mass erase
XDCscript usage |
meta-domain |
values of type Flash_2xx.MERAS_t
const Flash_2xx.MERAS_OFF;
const Flash_2xx.MERAS;
enum Flash_2xx.WAIT_t |
![](../../../../../Arrow_up.png) |
Wait
XDCscript usage |
meta-domain |
values of type Flash_2xx.WAIT_t
const Flash_2xx.WAIT_OFF;
const Flash_2xx.WAIT;
enum Flash_2xx.WRT_t |
![](../../../../../Arrow_up.png) |
Write
XDCscript usage |
meta-domain |
values of type Flash_2xx.WRT_t
const Flash_2xx.WRT_OFF;
const Flash_2xx.WRT;
struct Flash_2xx.FCTL1_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new Flash_2xx.FCTL1_t;
// FCTLx password
// Block write mode
// Write
// Enable Emergency Interrupt Exit
// Enable Erase Interrupts
// Mass erase
// Erase
struct Flash_2xx.FCTL2_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new Flash_2xx.FCTL2_t;
// FCTLx password
// Flash controller clock source select
// Flash controller clock divider bit 5
// Flash controller clock divider bit 4
// Flash controller clock divider bit 3
// Flash controller clock divider bit 2
// Flash controller clock divider bit 1
// Flash controller clock divider bit 0
struct Flash_2xx.FCTL3_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new Flash_2xx.FCTL3_t;
// FCTLx password. Always read as 096h. Must be written as 0A5h or a PUC
will be generated
// FAIL Bit 7 Operation failure. This bit is set if the fFTG clock source fails, or a flash
operation is aborted from an interrupt when EEIEX = 1. FAIL must be reset
with software.
0 No failure
1 Failure
// SegmentA and Info lock. Write a 1 to this bit to change its state. Writing 0 has
no effect.
0 Segment A unlocked and all information memory is erased during a
mass erase.
1 Segment A locked and all information memory is protected from erasure
during a mass erase
// Emergency exit
0 No emergency exit
1 Emergency exit
// Lock. This bit unlocks the flash memory for writing or erasing. The LOCK bit
can be set anytime during a byte/word write or erase operation and the
operation will complete normally. In the block write mode if the LOCK bit is set
while BLKWRT=WAIT=1, then BLKWRT and WAIT are reset and the mode
ends normally.
0 Unlocked
1 Locked
// Wait. Indicates the flash memory is being written to.
0 The flash memory is not ready for the next byte/word write
1 The flash memory is ready for the next byte/word write
// Access violation interrupt flag
0 No interrupt pending
1 Interrupt pending
// Flash security key violation. This bit indicates an incorrect FCTLx password
was written to any flash control register and generates a PUC when set. KEYV
must be reset with software.
0 FCTLx password was written correctly
1 FCTLx password was written incorrectly
// Busy. This bit indicates the status of the flash timing generator.
0 Not Busy
1 Busy
struct Flash_2xx.ForceSetDefaultRegister_t |
![](../../../../../Arrow_up.png) |
Force Set Default Register
XDCscript usage |
meta-domain |
var obj = new Flash_2xx.ForceSetDefaultRegister_t;
obj.register = String ...
obj.regForceSet = Bool ...
DETAILS
Type to store if each register needs to be forced initialized
even if the register is in default state.
SEE
Flash_2xx.addPeripheralsMap() // module-wide |
![](../../../../../Arrow_up.png) |
Create a map of all peripherals available on a device
XDCscript usage |
meta-domain |
ARGUMENTS
DETAILS
The config parameter
peripherals is by default undefined in an
xdc.platform.ICpuDataSheet instance. This function gathers
all instance configuration parameters that are of the type
xdc.platform.IPeripheral into the map
peripherals.
Flash_2xx.getAll() // module-wide |
![](../../../../../Arrow_up.png) |
Find all peripherals of a certain type
XDCscript usage |
meta-domain |
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
Flash_2xx.getRegisters() // module-wide |
![](../../../../../Arrow_up.png) |
Find all registers defined by the peripheral
XDCscript usage |
meta-domain |
Flash_2xx.getRegisters() returns String[]
RETURNS
Returns an array of register names
Instance Config Parameters |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
// Instance config-params object
// Flash Memory Control Register 1
};
params.baseAddr = UInt undefined;
// Address of the peripheral's control register
// Determine if each Register needs to be forced set or not
{
register: "FCTL1",
regForceSet: false
}
];
params.intNum = UInt undefined;
// Interrupt source number
params.name = String undefined;
// Specific peripheral name given by the device
params.owner = String undefined;
// String specifying the entity that manages the peripheral
config Flash_2xx.FCTL1 // instance |
![](../../../../../Arrow_up.png) |
Flash Memory Control Register 1
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
...
};
config Flash_2xx.baseAddr // instance |
![](../../../../../Arrow_up.png) |
Address of the peripheral's control register
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
...
params.baseAddr = UInt undefined;
DETAILS
A peripheral's registers are commonly accessed through a structure
that defines the offsets of a particular register from the lowest
address mapped to a peripheral. That lowest address is specified by
this parameter.
config Flash_2xx.forceSetDefaultRegister // instance |
![](../../../../../Arrow_up.png) |
Determine if each Register needs to be forced set or not
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
...
{
register: "FCTL1",
regForceSet: false
}
];
config Flash_2xx.intNum // instance |
![](../../../../../Arrow_up.png) |
Interrupt source number
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
...
params.intNum = UInt undefined;
config Flash_2xx.name // instance |
![](../../../../../Arrow_up.png) |
Specific peripheral name given by the device
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
...
params.name = String undefined;
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config Flash_2xx.owner // instance |
![](../../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
XDCscript usage |
meta-domain |
var params = new Flash_2xx.Params;
...
params.owner = String undefined;
Instance Creation |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new Flash_2xx.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
// Create an instance-object