metaonly interface ti.catalog.msp430.peripherals.clock.IClock

MSP430 Master Clock

XDCspec summary sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
metaonly interface IClock {  ...
instance:  ...
XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
 
metaonly interface IClock inherits IPeripheral {
module-wide constants & types
    typedef String StringArray// [];
        String register;
        Bool regForceSet;
    };
module-wide functions
 
instance:
per-instance config parameters
    readonly config Float ACLKHz// Stores ACLK as frequency in float;
    readonly config Float DCOCLKHz// Stores the DCO clock frequency in float = 1000000;
    readonly config Float MCLKHz// Stores MCLK as frequency in float;
    readonly config Float SMCLKHz// Stores SMCLK as frequency in float;
per-instance functions
}
typedef IClock.IPeripheralArray
XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
typedef IPeripheral.Instance IPeripheralArray[];
typedef IClock.StringArray
XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
typedef String StringArray[];
struct IClock.ForceSetDefaultRegister_t

Force Set Default Register

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
metaonly struct ForceSetDefaultRegister_t {
    String register;
    Bool regForceSet;
};
DETAILS
Type to store if each register needs to be forced initialized even if the register is in default state.
SEE
IClock.addPeripheralsMap()  // module-wide

Create a map of all peripherals available on a device

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
Void addPeripheralsMap(ICpuDataSheet.Instance cds);
ARGUMENTS
cds — an xdc.platform.ICpuDataSheet instance
DETAILS
The config parameter peripherals is by default undefined in an xdc.platform.ICpuDataSheet instance. This function gathers all instance configuration parameters that are of the type xdc.platform.IPeripheral into the map peripherals.
IClock.getAll()  // module-wide

Find all peripherals of a certain type

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
DETAILS
The type of the peripherals returned is defined by the type of the caller.
RETURNS
Returns an array of IPeripheral instances
IClock.getRegisters()  // module-wide

Find all registers defined by the peripheral

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
IPeripheral.StringArray getRegisters();
RETURNS
Returns an array of register names
config IClock.ACLKHz  // instance

Stores ACLK as frequency in float

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
readonly config Float ACLKHz;
config IClock.DCOCLKHz  // instance

Stores the DCO clock frequency in float

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
readonly config Float DCOCLKHz = 1000000;
config IClock.MCLKHz  // instance

Stores MCLK as frequency in float

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
readonly config Float MCLKHz;
config IClock.SMCLKHz  // instance

Stores SMCLK as frequency in float

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
readonly config Float SMCLKHz;
config IClock.baseAddr  // instance

Address of the peripheral's control register

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
config UInt baseAddr;
DETAILS
A peripheral's registers are commonly accessed through a structure that defines the offsets of a particular register from the lowest address mapped to a peripheral. That lowest address is specified by this parameter.
config IClock.name  // instance

Specific peripheral name given by the device

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
config String name;
DETAILS
Devices can have more than one peripheral of the same type. In such cases, device data sheets give different names to the instances of a same peripheral. For example, the name for a timer module could be TimerA3, and a device that has two such timers can name them TA0 and TA1.
config IClock.owner  // instance

String specifying the entity that manages the peripheral

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
config String owner;
IClock.computeDCOCLKHz()  // instance

Initialize to the nearest available DCO clock frequency

XDCspec declarations sourced in ti/catalog/msp430/peripherals/clock/IClock.xdc
Void computeDCOCLKHz(Float DCOCLKHz);
generated on Tue, 01 Feb 2011 01:40:32 GMT