![]() |
![]() |
TI-RTOS for TivaC
2.14.04.31
|
CEMAC_Config | EMAC Global configuration |
CEMAC_FxnTable | EMAC Function table structure |
CEMACSnow_HWAttrs | EMACSnow Hardware attributes |
CEMACSnow_Object | EMACSnow Object |
CEMACTiva_HWAttrs | EMACTiva Hardware attributes |
CEMACTiva_Object | EMACTiva Object |
CGPIOCC3200_Config | GPIO device specific driver configuration structure |
CGPIOMSP430_Config | GPIO device specific driver configuration structure |
CGPIOMSP432_Config | GPIO device specific driver configuration structure |
CGPIOTiva_Config | GPIO device specific driver configuration structure |
CI2C_Config | I2C Global configuration |
CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
CI2C_Params | I2C Parameters |
CI2C_Transaction | I2C transaction |
CI2CCC26XX_HWAttrs | I2CCC26XX Hardware attributes |
CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
CI2CCC26XX_Object | I2CCC26XX Object |
CI2CCC3200_HWAttrs | I2CCC3200 Hardware attributes |
CI2CCC3200_Object | I2CCC3200 Object |
CI2CEUSCIB_HWAttrs | I2CEUSCIB Hardware attributes |
CI2CEUSCIB_Object | I2CEUSCIB Object |
CI2CMSP432_HWAttrs | I2CMSP432 Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CI2CMSP432_Object | I2CMSP432 Object |
CI2CTiva_HWAttrs | I2CTiva Hardware attributes |
CI2CTiva_Object | I2CTiva Object |
CI2CUSCIB_HWAttrs | I2CUSCIB Hardware attributes |
CI2CUSCIB_Object | I2CUSCIB Object |
CPIN_State_s | Underlying data structure for type PIN_State |
CPWM_Config | PWM Global configuration |
CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
CPWM_Params | PWM Parameters |
CPWMTimerCC3200_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerCC3200_Object | PWMTimerCC3200 Object |
CPWMTimerMSP432_HWAttrs | PWMTimerMSP432 Hardware attributes |
CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
CPWMTimerTiva_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerTiva_Object | PWMTimerTiva Object |
CPWMTiva_HWAttrs | PWMTiva Hardware attributes |
CPWMTiva_Object | PWMTiva Object |
CPWMTiva_Status | PWMTiva_Status |
CSDSPI_Config | SDSPI Global configuration |
CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
CSDSPI_Params | SDSPI Parameters |
CSDSPICC3200_HWAttrs | SDSPICC3200 Hardware attributes |
CSDSPICC3200_Object | SDSPICC3200 Object |
CSDSPIEUSCIA_HWAttrsV1 | SDSPIEUSCIA Hardware attributes |
CSDSPIEUSCIA_Object | SDSPIEUSCIA Object |
CSDSPIEUSCIB_HWAttrsV1 | SDSPIEUSCIB Hardware attributes |
CSDSPIEUSCIB_Object | SDSPIEUSCIB Object |
CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
CSDSPIMSP432_Object | SDSPIMSP432 Object |
CSDSPITiva_HWAttrs | SDSPITiva Hardware attributes |
CSDSPITiva_Object | SDSPITiva Object |
CSDSPIUSCIA_HWAttrs | SDSPIUSCIA Hardware attributes |
CSDSPIUSCIA_Object | SDSPIUSCIA Object |
CSDSPIUSCIB_HWAttrs | SDSPIUSCIB Hardware attributes |
CSDSPIUSCIB_Object | SDSPIUSCIB Object |
CSPI_Config | SPI Global configuration |
CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
CSPI_Params | SPI Parameters |
CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
CSPICC26XX_HWAttrs | SPICC26XXDMA Hardware attributes |
CSPICC26XX_Object | SPICC26XXDMA Object |
CSPICC3200DMA_HWAttrs | SPICC3200DMA Hardware attributes |
CSPICC3200DMA_Object | SPICC3200DMA Object |
CSPIEUSCIADMA_HWAttrs | SPIEUSCIADMA Hardware attributes |
CSPIEUSCIADMA_Object | SPIEUSCIADMA Object |
CSPIEUSCIBDMA_HWAttrs | SPIEUSCIBDMA Hardware attributes |
CSPIEUSCIBDMA_Object | SPIEUSCIBDMA Object |
CSPIMSP432DMA_HWAttrs | SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CSPIMSP432DMA_Object | SPIMSP432DMA Object |
CSPITivaDMA_HWAttrs | SPITivaDMA Hardware attributes |
CSPITivaDMA_Object | SPITivaDMA Object |
CSPIUSCIADMA_HWAttrs | SPIUSCIADMA Hardware attributes |
CSPIUSCIADMA_Object | SPIUSCIADMA Object |
CSPIUSCIBDMA_HWAttrs | SPIUSCIBDMA Hardware attributes |
CSPIUSCIBDMA_Object | SPIUSCIBDMA Object |
CUART_Config | UART Global configuration |
CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
CUART_Params | UART Parameters |
CUARTCC26XX_HWAttrs | UARTCC26XX Hardware attributes |
CUARTCC26XX_Object | UARTCC26XX Object |
CUARTCC3200_FxnSet | Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only |
CUARTCC3200_HWAttrs | UARTCC3200 Hardware attributes |
CUARTCC3200_Object | UARTCC3200 Object |
CUARTCC3200DMA_HWAttrs | UARTCC3200DMA Hardware attributes |
CUARTCC3200DMA_Object | UARTCC3200DMA Object |
CUARTEUSCIA_BaudrateConfig | UARTEUSCIA Baudrate configuration |
CUARTEUSCIA_HWAttrs | UARTEUSCIA Hardware attributes |
CUARTEUSCIA_Object | UARTEUSCIA Object |
CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
CUARTMSP432_HWAttrs | UARTMSP432 Hardware attributes |
CUARTMSP432_Object | UARTMSP432 Object |
CUARTTiva_FxnSet | Complement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only |
CUARTTiva_HWAttrs | UARTTiva Hardware attributes |
CUARTTiva_Object | UARTTiva Object |
CUARTTivaDMA_HWAttrs | UARTTivaDMA Hardware attributes |
CUARTTivaDMA_Object | UARTTivaDMA Object |
CUARTUSCIA_BaudrateConfig | UARTUSCIA Baudrate configuration |
CUARTUSCIA_HWAttrs | UARTUSCIA Hardware attributes |
CUARTUSCIA_Object | UARTUSCIA Object |
CUSBMSCHFatFs_Config | USBMSCHFatFs Global configuration |
CUSBMSCHFatFs_FxnTable | The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation |
CUSBMSCHFatFs_Params | USBMSCHFatFs Parameters |
CUSBMSCHFatFsTiva_HWAttrs | USBMSCHFatFsTiva Hardware attributes |
CUSBMSCHFatFsTiva_Object | USBMSCHFatFsTiva Object |
CWatchdog_Config | Watchdog Global configuration |
CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
CWatchdog_Params | Watchdog Parameters |
CWatchdogCC26XX_HWAttrs | Watchdog hardware attributes for CC26XX |
CWatchdogCC26XX_Object | Watchdog Object for CC26XX |
CWatchdogCC3200_HWAttrs | Watchdog hardware attributes for CC3200 |
CWatchdogCC3200_Object | Watchdog Object for CC3200 |
CWatchdogMSP430_HWAttrs | Watchdog hardware attributes for MSP430 |
CWatchdogMSP430_Object | Watchdog Object for MSP430 |
CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
CWatchdogMSP432_Object | Watchdog Object for MSP432 |
CWatchdogTiva_HWAttrs | Watchdog hardware attributes for Tiva |
CWatchdogTiva_Object | Watchdog Object for Tiva |
CWiFi_Config | WiFi Global configuration |
CWiFi_FxnTable | The definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation |
CWiFi_Params | WiFi Parameters |
CWiFiCC3100_HWAttrs | WiFiCC3100 Hardware attributes |
CWiFiCC3100_Object | WiFiCC3100 Object |