![]() |
![]() |
TI-RTOS for SimpleLink Wireless MCUs
2.14.03.28
|
CCamera_Config | Camera Global configuration |
CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
CCamera_Params | Camera Parameters |
CCameraCC3200DMA_HWAttrs | CameraCC3200DMA Hardware attributes |
CCameraCC3200DMA_Object | CameraCC3200DMA Object |
CClockP_FreqHz | Frequency-in-hertz struct |
CClockP_Params | Basic ClockP Parameters |
CCryptoCC26XX_AESCCM_Transaction | CryptoCC26XX AES-CCM Transaction |
CCryptoCC26XX_AESECB_Transaction | CryptoCC26XX AES-ECB Transaction |
CCryptoCC26XX_Config | CryptoCC26XX Global Configuration |
CCryptoCC26XX_HWAttrs | CryptoCC26XX Hardware Attributes |
CCryptoCC26XX_Object | CryptoCC26XX Object |
CCryptoCC26XX_Params | CryptoCC26XX Parameters |
CCryptoCC26XX_Transaction | CryptoCC26XX Transaction |
CGPIOCC3200_Config | GPIO device specific driver configuration structure |
CGPIOMSP430_Config | GPIO device specific driver configuration structure |
CGPIOMSP432_Config | GPIO device specific driver configuration structure |
CGPIOTiva_Config | GPIO device specific driver configuration structure |
CHwiP_Params | Basic HwiP Parameters |
CI2C_Config | I2C Global configuration |
CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
CI2C_Params | I2C Parameters |
CI2C_Transaction | I2C transaction |
CI2CCC26XX_HWAttrs | I2CCC26XX Hardware attributes |
CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
CI2CCC26XX_Object | I2CCC26XX Object |
CI2CCC3200_HWAttrs | I2CCC3200 Hardware attributes |
CI2CCC3200_Object | I2CCC3200 Object |
CI2CEUSCIB_HWAttrs | I2CEUSCIB Hardware attributes |
CI2CEUSCIB_Object | I2CEUSCIB Object |
CI2CMSP432_HWAttrs | I2CMSP432 Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CI2CMSP432_Object | I2CMSP432 Object |
CI2CTiva_HWAttrs | I2CTiva Hardware attributes |
CI2CTiva_Object | I2CTiva Object |
CI2CUSCIB_HWAttrs | I2CUSCIB Hardware attributes |
CI2CUSCIB_Object | I2CUSCIB Object |
CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
CI2S_Config | I2S Global configuration |
CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
CI2S_Params | Basic I2S Parameters |
CI2SCC3200DMA_HWAttrs | I2SCC3200DMA Hardware attributes |
CI2SCC3200DMA_Object | I2SCC3200DMA Object |
CI2SCC3200DMA_SerialPinConfig | CC3200 Serial Pin Configuration |
CI2SCC3200DMA_SerialPinParams | CC3200 specific I2S Parameters |
CI2SCC3200DMA_SerialPinVars | I2SCC3200DMA Serial pin variables |
CLCD_Buffer | LCD_Buffer used to store data to be printed on the LCD display |
CLCD_Command | Format of LCD commands used by the LCD controller |
CLCD_Config | The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation |
CLCD_HWAttrs | LCD Hardware attributes |
CLCD_Object | LCD Object |
CLCD_Params | LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init() |
CMutexP_Params | Basic MutexP Parameters |
CPIN_State_s | Underlying data structure for type PIN_State |
CPower_NotifyObj | Power notify object structure |
CPowerCC3200_Config | Power global configuration |
CPowerCC3200_MCURegisters | MCU core registers that need to be save on entering LPDS |
CPowerCC3200_ModuleState | Internal module state |
CPowerCC3200_NVICRegisters | NVIC registers that need to be save on entering LPDS |
CPowerCC3200_SaveRegisters | Struct of context registers to save on entering LPDS |
CPowerCC3200_Wakeup | For wakeup from LPDS or shutdown configuration |
CPowerMSP432_Config | Power global configuration (MSP432-specific) |
CPowerMSP432_Freqs | Structure holding device frequencies (in Hz) |
CPWM_Config | PWM Global configuration |
CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
CPWM_Params | PWM Parameters |
CPWMTimerCC3200_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerCC3200_Object | PWMTimerCC3200 Object |
CPWMTimerMSP432_HWAttrs | PWMTimerMSP432 Hardware attributes |
CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
CPWMTimerTiva_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerTiva_Object | PWMTimerTiva Object |
CPWMTiva_HWAttrs | PWMTiva Hardware attributes |
CPWMTiva_Object | PWMTiva Object |
CPWMTiva_Status | PWMTiva_Status |
CRF_Mode | Struct defining operating mode of RF driver |
CRF_Object | Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver |
CRF_Params | RF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call |
CRF_RadioSetup | Union of the different flavors of RADIO_SETUP commands |
CSDSPI_Config | SDSPI Global configuration |
CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
CSDSPI_Params | SDSPI Parameters |
CSDSPICC3200_HWAttrs | SDSPICC3200 Hardware attributes |
CSDSPICC3200_Object | SDSPICC3200 Object |
CSDSPIEUSCIA_HWAttrsV1 | SDSPIEUSCIA Hardware attributes |
CSDSPIEUSCIA_Object | SDSPIEUSCIA Object |
CSDSPIEUSCIB_HWAttrsV1 | SDSPIEUSCIB Hardware attributes |
CSDSPIEUSCIB_Object | SDSPIEUSCIB Object |
CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
CSDSPIMSP432_Object | SDSPIMSP432 Object |
CSDSPITiva_HWAttrs | SDSPITiva Hardware attributes |
CSDSPITiva_Object | SDSPITiva Object |
CSDSPIUSCIA_HWAttrs | SDSPIUSCIA Hardware attributes |
CSDSPIUSCIA_Object | SDSPIUSCIA Object |
CSDSPIUSCIB_HWAttrs | SDSPIUSCIB Hardware attributes |
CSDSPIUSCIB_Object | SDSPIUSCIB Object |
CSemaphoreP_Params | Basic SemaphoreP Parameters |
CSPI_Config | SPI Global configuration |
CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
CSPI_Params | SPI Parameters |
CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
CSPICC26XX_HWAttrs | SPICC26XXDMA Hardware attributes |
CSPICC26XX_Object | SPICC26XXDMA Object |
CSPICC3200DMA_HWAttrs | SPICC3200DMA Hardware attributes |
CSPICC3200DMA_Object | SPICC3200DMA Object |
CSPIEUSCIADMA_HWAttrs | SPIEUSCIADMA Hardware attributes |
CSPIEUSCIADMA_Object | SPIEUSCIADMA Object |
CSPIEUSCIBDMA_HWAttrs | SPIEUSCIBDMA Hardware attributes |
CSPIEUSCIBDMA_Object | SPIEUSCIBDMA Object |
CSPIMSP432DMA_HWAttrs | SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CSPIMSP432DMA_Object | SPIMSP432DMA Object |
CSPITivaDMA_HWAttrs | SPITivaDMA Hardware attributes |
CSPITivaDMA_Object | SPITivaDMA Object |
CSPIUSCIADMA_HWAttrs | SPIUSCIADMA Hardware attributes |
CSPIUSCIADMA_Object | SPIUSCIADMA Object |
CSPIUSCIBDMA_HWAttrs | SPIUSCIBDMA Hardware attributes |
CSPIUSCIBDMA_Object | SPIUSCIBDMA Object |
CUART_Config | UART Global configuration |
CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
CUART_Params | UART Parameters |
CUARTCC26XX_HWAttrs | UARTCC26XX Hardware attributes |
CUARTCC26XX_Object | UARTCC26XX Object |
CUARTCC3200_FxnSet | Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only |
CUARTCC3200_HWAttrs | UARTCC3200 Hardware attributes |
CUARTCC3200_Object | UARTCC3200 Object |
CUARTCC3200DMA_HWAttrs | UARTCC3200DMA Hardware attributes |
CUARTCC3200DMA_Object | UARTCC3200DMA Object |
CUARTEUSCIA_BaudrateConfig | UARTEUSCIA Baudrate configuration |
CUARTEUSCIA_HWAttrs | UARTEUSCIA Hardware attributes |
CUARTEUSCIA_Object | UARTEUSCIA Object |
CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
CUARTMSP432_HWAttrs | UARTMSP432 Hardware attributes |
CUARTMSP432_Object | UARTMSP432 Object |
CUARTTiva_FxnSet | Complement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only |
CUARTTiva_HWAttrs | UARTTiva Hardware attributes |
CUARTTiva_Object | UARTTiva Object |
CUARTTivaDMA_HWAttrs | UARTTivaDMA Hardware attributes |
CUARTTivaDMA_Object | UARTTivaDMA Object |
CUARTUSCIA_BaudrateConfig | UARTUSCIA Baudrate configuration |
CUARTUSCIA_HWAttrs | UARTUSCIA Hardware attributes |
CUARTUSCIA_Object | UARTUSCIA Object |
CUDMACC26XX_Config | UDMACC26XX Global configuration |
CUDMACC26XX_HWAttrs | UDMACC26XX hardware attributes |
CUDMACC26XX_Object | UDMACC26XX object |
CWatchdog_Config | Watchdog Global configuration |
CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
CWatchdog_Params | Watchdog Parameters |
CWatchdogCC26XX_HWAttrs | Watchdog hardware attributes for CC26XX |
CWatchdogCC26XX_Object | Watchdog Object for CC26XX |
CWatchdogCC3200_HWAttrs | Watchdog hardware attributes for CC3200 |
CWatchdogCC3200_Object | Watchdog Object for CC3200 |
CWatchdogMSP430_HWAttrs | Watchdog hardware attributes for MSP430 |
CWatchdogMSP430_Object | Watchdog Object for MSP430 |
CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
CWatchdogMSP432_Object | Watchdog Object for MSP432 |
CWatchdogTiva_HWAttrs | Watchdog hardware attributes for Tiva |
CWatchdogTiva_Object | Watchdog Object for Tiva |