![]() |
![]() |
|
IPC API
3.40.00.06
|

Files | |
| file | gatempapp_rsc_table_vayu_dsp.h [code] |
| file | GateMPAppCommon.h [code] |
| file | Mx.h [code] |
| Example of a host-side module which uses MmRpc to invoke functions on a remote processor. | |
| file | MxServer.h [code] |
| Example of a slave-side module which implements the Mx module functions. The functions in MxServer are invoked remotely by the Mx module running on the host processor. | |
| file | power_rsc_table_vayu_dsp.h [code] |