IPC API  3.40.00.06
MxServer.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2012-2013, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
43 #ifndef MxServer__include
44 #define MxServer__include
45 
46 #include <stddef.h>
47 #include <stdint.h>
48 
49 #if defined(__cplusplus)
50 extern "C" {
51 #endif
52 
56 #define MxServer_S_SUCCESS (0)
57 
61 #define MxServer_E_FAIL (-1)
62 
66 typedef struct {
67  uint32_t coef;
68  int key;
69  int size;
70  uint32_t * inBuf;
71  uint32_t * outBuf;
73 
77 int32_t MxServer_triple(uint32_t a);
78 
82 int32_t MxServer_add(int32_t a, int32_t b);
83 
88 int32_t MxServer_compute(MxServer_Compute *compute);
89 
90 
91 #if defined(__cplusplus)
92 }
93 #endif
94 #endif /* MxServer__include */
uint32_t * outBuf
Definition: MxServer.h:71
int size
Definition: MxServer.h:69
int32_t MxServer_add(int32_t a, int32_t b)
Sample function which addes two arguments.
uint32_t * inBuf
Definition: MxServer.h:70
int key
Definition: MxServer.h:68
int32_t MxServer_triple(uint32_t a)
Sample function which multiplies argument by three.
Compute structure.
Definition: MxServer.h:66
uint32_t coef
Definition: MxServer.h:67
int32_t MxServer_compute(MxServer_Compute *compute)
Sample function which has pointer parameter to a structure with two embedded pointers.
Copyright 2015, Texas Instruments Incorporated