module ti.sdo.ipc.transports.TransportShmNotify

Transport for MessageQ that acts on shared memory

TransportShmSingle is a simplified version of TransportShm. This transport uses the Notify module to do all the real work. The 'put' function passes the message to the other processor using the 'payload' parameter to Notify_sendEvent(). The receive side simply casts this payload parameter to a MessageQ_Msg and enqueues it locally. [ more ... ]
C synopsis target-domain sourced in ti/sdo/ipc/transports/TransportShmNotify.xdc
#include <ti/sdo/ipc/transports/TransportShmNotify.h>
Functions
Void
Void
Void
Void
Functions common to all IMessageQTransport modules
Bool 
Int 
Bool 
Void 
Functions common to all target instances
Functions common to all target modules
Typedefs
typedef Void 
typedef struct
typedef struct
typedef enum
typedef enum
typedef struct
Constants
extern const UInt16 
 
DETAILS
TransportShmSingle is a simplified version of TransportShm. This transport uses the Notify module to do all the real work. The 'put' function passes the message to the other processor using the 'payload' parameter to Notify_sendEvent(). The receive side simply casts this payload parameter to a MessageQ_Msg and enqueues it locally.
CAVEATS:
The sender will spin in Notify_sendEvent until the receive side has read the previous message. This is Notify-driver specific. NotifyDriverShm will spin before sending a new event if the prior event hasn't been handled. Some Notify drivers may support a FIFO or queue for these events to mitigate this busy-wait affect.
 
enum TransportShmNotify_Reason

Reason for error function being called

C synopsis target-domain
typedef enum TransportShmNotify_Reason {
    TransportShmNotify_Reason_FAILEDPUT,
    TransportShmNotify_Reason_INTERNALERR,
    TransportShmNotify_Reason_PHYSICALERR,
    TransportShmNotify_Reason_FAILEDALLOC
} TransportShmNotify_Reason;
 
DETAILS
First field in the errFxn
 
enum TransportShmNotify_Status

Transport return values

C synopsis target-domain
typedef enum TransportShmNotify_Status {
    TransportShmNotify_S_SUCCESS,
    TransportShmNotify_E_FAIL,
    TransportShmNotify_E_ERROR
} TransportShmNotify_Status;
 
DETAILS
  • S_SUCCESS: Operation was successful
  • E_FAIL: Operation resulted in a failure
  • E_ERROR: Operation resulted in an error.
 
typedef TransportShmNotify_ErrFxn

Typedef for transport error callback function

C synopsis target-domain
typedef Void (*TransportShmNotify_ErrFxn)(IMessageQTransport_Reason,IMessageQTransport_Handle,Ptr,UArg);
 
DETAILS
First parameter: Why the error function is being called.
Second parameter: Handle of transport that had the error. NULL denotes that it is a system error, not a specific transport.
Third parameter: Pointer to the message. This is only valid for Reason_FAILEDPUT.
Fourth parameter: Transport specific information. Refer to individual transports for more details.
 
config TransportShmNotify_errFxn  // module-wide

Asynchronous error function for the transport module

C synopsis target-domain
extern const IMessageQTransport_ErrFxn TransportShmNotify_errFxn;
 
 
config TransportShmNotify_notifyEventId  // module-wide

Notify event ID for transport

C synopsis target-domain
extern const UInt16 TransportShmNotify_notifyEventId;
 
 
TransportShmNotify_setErrFxn()  // module-wide

Sets the asynchronous error function for the transport module

C synopsis target-domain
Void TransportShmNotify_setErrFxn(IMessageQTransport_ErrFxn errFxn);
 
ARGUMENTS
errFxn — Function that is called when an asynchronous error occurs.
DETAILS
This API allows the user to set the function that will be called in case of an asynchronous error by the transport.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TransportShmNotify_Module_id();
// Get this module's unique id
 
Bool TransportShmNotify_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TransportShmNotify_Module_heap();
// The heap from which this module allocates memory
 
Bool TransportShmNotify_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TransportShmNotify_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TransportShmNotify_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct TransportShmNotify_Object TransportShmNotify_Object;
// Opaque internal representation of an instance object
 
typedef TransportShmNotify_Object *TransportShmNotify_Handle;
// Client reference to an instance object
 
typedef struct TransportShmNotify_Struct TransportShmNotify_Struct;
// Opaque client structure large enough to hold an instance object
 
TransportShmNotify_Handle TransportShmNotify_handle(TransportShmNotify_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
TransportShmNotify_Struct *TransportShmNotify_struct(TransportShmNotify_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct TransportShmNotify_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt priority;
    // Which priority messages should this transport manage
} TransportShmNotify_Params;
 
Void TransportShmNotify_Params_init(TransportShmNotify_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config TransportShmNotify_priority  // instance

Which priority messages should this transport manage

C synopsis target-domain
      ...
    UInt priority;
 
Instance Creation

C synopsis target-domain
TransportShmNotify_Handle TransportShmNotify_create(UInt16 procId, const TransportShmNotify_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void TransportShmNotify_construct(TransportShmNotify_Struct *structP, UInt16 procId, const TransportShmNotify_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
procId — Remote processor id that this instance will communicate with.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a transport instance. The transport is responsible for registering with MessageQ via the ti.sdo.ipc.MessageQ.registerTransport API.
Instance Deletion

C synopsis target-domain
Void TransportShmNotify_delete(TransportShmNotify_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void TransportShmNotify_destruct(TransportShmNotify_Struct *structP);
// Finalize the instance object inside the provided structure
 
TransportShmNotify_control()  // instance

Send a control command to the transport instance

C synopsis target-domain
Bool TransportShmNotify_control(TransportShmNotify_Handle handle, UInt cmd, UArg cmdArg);
 
ARGUMENTS
handle — handle of a previously-created TransportShmNotify instance object
cmd — Requested command
cmdArgs — Accompanying field for the command. This is command specific.
RETURNS
TRUE denotes acceptance of the command. FALSE denotes failure of the command.
DETAILS
This is function allows transport to specify control commands. Refer to individual transport implementions for more details.
 
TransportShmNotify_getStatus()  // instance

Status of a Transport instance

C synopsis target-domain
Int TransportShmNotify_getStatus(TransportShmNotify_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created TransportShmNotify instance object
RETURNS
Returns status of Transport instance
DETAILS
This function returns the status of the transport instance.
 
TransportShmNotify_put()  // instance

Put the message to the remote processor

C synopsis target-domain
Bool TransportShmNotify_put(TransportShmNotify_Handle handle, Ptr msg);
 
ARGUMENTS
handle — handle of a previously-created TransportShmNotify instance object
msg — Pointer the message to be sent
RETURNS
TRUE denotes acceptance of the message to be sent. FALSE denotes the message could not be sent.
DETAILS
If the transport can accept the message, it returns TRUE. Accepting a message does not mean that it is transmitted. It simply means that the transport should be able to send the message. If the actual transfer fails, the transport calls the {@#ErrFxn} (assuming it is set up via the {@#setErrFxn} API. If the {@#ErrFxn} is not set, the message is dropped. (also...should an error be raised or just System_printf?).
If the transport cannot send the message, it returns FALSE and a filled in Error_Block. The caller still owns the message.
Instance Convertors

C synopsis target-domain
IMessageQTransport_Handle TransportShmNotify_Handle_upCast(TransportShmNotify_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
TransportShmNotify_Handle TransportShmNotify_Handle_downCast(IMessageQTransport_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int TransportShmNotify_Object_count();
// The number of statically-created instance objects
 
TransportShmNotify_Handle TransportShmNotify_Object_get(TransportShmNotify_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
TransportShmNotify_Handle TransportShmNotify_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
TransportShmNotify_Handle TransportShmNotify_Object_next(TransportShmNotify_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle TransportShmNotify_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *TransportShmNotify_Handle_label(TransportShmNotify_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String TransportShmNotify_Handle_name(TransportShmNotify_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/transports/TransportShmNotify.xdc
var TransportShmNotify = xdc.useModule('ti.sdo.ipc.transports.TransportShmNotify');
module-wide constants & types
        const TransportShmNotify.Reason_FAILEDPUT;
        const TransportShmNotify.Reason_INTERNALERR;
        const TransportShmNotify.Reason_PHYSICALERR;
        const TransportShmNotify.Reason_FAILEDALLOC;
 
        const TransportShmNotify.S_SUCCESS;
        const TransportShmNotify.E_FAIL;
        const TransportShmNotify.E_ERROR;
module-wide config parameters
 
per-instance config parameters
    var params = new TransportShmNotify.Params// Instance config-params object;
per-instance creation
    var inst = TransportShmNotify.create// Create an instance-object(UInt16 procId, params);
 
 
enum TransportShmNotify.Reason

Reason for error function being called

XDCscript usage meta-domain
values of type TransportShmNotify.Reason
    const TransportShmNotify.Reason_FAILEDPUT;
    const TransportShmNotify.Reason_INTERNALERR;
    const TransportShmNotify.Reason_PHYSICALERR;
    const TransportShmNotify.Reason_FAILEDALLOC;
 
DETAILS
First field in the errFxn
C SYNOPSIS
 
enum TransportShmNotify.Status

Transport return values

XDCscript usage meta-domain
values of type TransportShmNotify.Status
    const TransportShmNotify.S_SUCCESS;
    const TransportShmNotify.E_FAIL;
    const TransportShmNotify.E_ERROR;
 
DETAILS
  • S_SUCCESS: Operation was successful
  • E_FAIL: Operation resulted in a failure
  • E_ERROR: Operation resulted in an error.
C SYNOPSIS
 
config TransportShmNotify.errFxn  // module-wide

Asynchronous error function for the transport module

XDCscript usage meta-domain
TransportShmNotify.errFxn = Void(*)(IMessageQTransport.Reason,IMessageQTransport.Handle,Ptr,UArg) null;
 
C SYNOPSIS
 
config TransportShmNotify.notifyEventId  // module-wide

Notify event ID for transport

XDCscript usage meta-domain
TransportShmNotify.notifyEventId = UInt16 2;
 
C SYNOPSIS
 
metaonly config TransportShmNotify.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
TransportShmNotify.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
Instance Config Parameters

XDCscript usage meta-domain
var params = new TransportShmNotify.Params;
// Instance config-params object
    params.priority = UInt 0;
    // Which priority messages should this transport manage
 
config TransportShmNotify.priority  // instance

Which priority messages should this transport manage

XDCscript usage meta-domain
var params = new TransportShmNotify.Params;
  ...
params.priority = UInt 0;
 
C SYNOPSIS
Instance Creation

XDCscript usage meta-domain
var params = new TransportShmNotify.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = TransportShmNotify.create(UInt16 procId, params);
// Create an instance-object
ARGUMENTS
procId — Remote processor id that this instance will communicate with.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a transport instance. The transport is responsible for registering with MessageQ via the ti.sdo.ipc.MessageQ.registerTransport API.
generated on Tue, 22 May 2012 23:45:06 GMT