module ti.sdo.ipc.MessageQ |
|
|
|
Message-passing with queuing
The MessageQ module supports the structured sending and receiving of
variable length messages. This module can be used for homogeneous
(DSP to DSP) or heterogeneous (Arm to DSP) multi-processor messaging.
[
more ... ]
#include <ti/sdo/ipc/MessageQ.h>
Functions |
Void | |
Bool | |
Void | |
Functions common to all target instances |
|
MessageQ_handle// Convert this instance structure pointer into an instance handle,
MessageQ_Handle_label// The label associated with this instance object,
MessageQ_Handle_name// The name of this instance object,
MessageQ_Object_count// The number of statically-created instance objects,
MessageQ_Object_first// The handle of the first dynamically-created instance object, or NULL,
MessageQ_Object_get// The handle of the i-th statically-created instance object (array == NULL),
MessageQ_Object_heap// The heap used to allocate dynamically-created instance objects,
MessageQ_Object_next// The handle of the next dynamically-created instance object, or NULL,
MessageQ_struct// Convert this instance handle into an instance structure pointer
|
Functions common to all target modules |
|
|
Defines |
#define | |
#define | |
#define | |
#define | |
Typedefs |
| |
typedef struct | |
typedef struct | |
typedef UInt32 | |
typedef struct | |
Constants |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
extern const UInt | |
extern const UInt | |
| |
extern const UInt16 | |
extern const Bool | |
DETAILS
The MessageQ module supports the structured sending and receiving of
variable length messages. This module can be used for homogeneous
(DSP to DSP) or heterogeneous (Arm to DSP) multi-processor messaging.
MessageQ provides more sophisticated messaging than other modules. It is
typically used for complex situations such as multi-processor messaging.
The following are key features of the MessageQ module:
- Writers and readers can be relocated to another processor with no
runtime code changes.
- Timeouts are allowed when receiving messages.
- Readers can determine the writer and reply back.
- Receiving a message is deterministic when the timeout is zero.
- Messages can reside on any message queue.
- Supports zero-copy transfers.
- Can send and receive from any type of thread.
- Notification mechanism is specified by application.
- Allows QoS (quality of service) on message buffer pools. For example,
using specific buffer pools for specific message queues.
Messages are sent and received by being placed on and removed from a
message queue. A reader is a thread that gets (reads) messages from a
message queue. A writer is a thread that puts (writes) a message to a
message queue. Each message queue has one reader and can have many writers.
A thread may read from or write to multiple message queues.
Conceptually, the reader thread owns a message queue. The reader thread
creates a message queue. The writer threads open a created message queue
to get access to them.
Message queues are identified by a system-wide unique name. Internally,
MessageQ uses the
ti.sdo.utils.NameServer module for managing
these names. The names are used for opening a message queue.
Messages must be allocated from the MessageQ module. Once a message is
allocated, it can be sent to any message queue. Once a message is sent, the
writer loses ownership of the message and should not attempt to modify the
message. Once the reader receives the message, it owns the message. It
may either free the message or re-use the message.
Messages in a message queue can be of variable length. The only
requirement is that the first field in the definition of a message must be a
MsgHeader structure. For example:
typedef struct MyMsg {
MessageQ_MsgHeader header;
...
} MyMsg;
The MessageQ API uses the MessageQ_MsgHeader internally. Your application
should not modify or directly access the fields in the MessageQ_MsgHeader.
All messages sent via the MessageQ module must be allocated from a
xdc.runtime.IHeap implementation. The heap can also be used for
other memory allocation not related to MessageQ.
An application can use multiple heaps. The purpose of having multiple
heaps is to allow an application to regulate its message usage. For
example, an application can allocate critical messages from one heap of fast
on-chip memory and non-critical messages from another heap of slower
external memory.
The
registerHeap and
registerHeapMeta are APIs used to
assign a MessageQ heapId to a heap. When allocating a message, the heapId
is used, not the heap handle. This heapId is actually placed into the
message (part of the
MsgHeader). Care must be taken when assigning
heapIds. Refer to the
registerHeap and
registerHeapMeta
descriptions for more details.
MessageQ also supports the usage of messages that are not allocated via the
alloc function. Please refer to the
staticMsgInit
function description for more details.
MessageQ supports reads/writes of different thread models. This is
accomplished by having the creator of the message queue specify a
xdc.runtime.knl.ISync.Object via the
synchronizer
configuration parameter. The
xdc.runtime.knl.ISync.signal
portion of the ISync instance is called whenever the
put
is called. The
xdc.runtime.knl.ISync.wait portion is
called in the
get if and only if there are no messages.
Since ISyncs are binary, the reader must drain the message queue of all
messages before waiting for another signal. For example, if the reader
was a SYSBIOS Swi, the
xdc.runtime.knl.ISync instance
could be a SyncSwi. If a
put was called, the Swi_post() would
be called. The Swi would run and it must call
get until no
messages are returned.
In a multiple processor system, MessageQ communicates to other
processors via
ti.sdo.ipc.interfaces.IMessageQTransport instances.
MessageQ supports a high priority and a normal priority transport between
any two processors. The IMessageQTransport instances are created via the
SetupTransportProxy. The instances are responsible for
registering themselves with MessageQ. This is accomplished via the
registerTransport function.
const MessageQ_HIGHPRI |
|
#define MessageQ_HIGHPRI (UInt)1
const MessageQ_NORMALPRI |
|
Message priority values. These must match the values defined in
ti/ipc/MessageQ.h but are needed here for ROV
#define MessageQ_NORMALPRI (UInt)0
const MessageQ_RESERVEDPRI |
|
#define MessageQ_RESERVEDPRI (UInt)2
const MessageQ_URGENTPRI |
|
#define MessageQ_URGENTPRI (UInt)3
typedef MessageQ_QueueId |
|
MessageQ ID
typedef UInt32 MessageQ_QueueId;
config MessageQ_A_cannotFreeStaticMsg // module-wide |
|
Assert raised when attempting to free a static message
extern const Assert_Id MessageQ_A_cannotFreeStaticMsg;
config MessageQ_A_heapIdInvalid // module-wide |
|
Assert raised when using an invalid heapId
extern const Assert_Id MessageQ_A_heapIdInvalid;
config MessageQ_A_invalidContext // module-wide |
|
Assert raised when calling API with wrong handle
extern const Assert_Id MessageQ_A_invalidContext;
DETAILS
Some APIs can only be called with an opened handle (e.g.
close. Some can only be called with a created handle
(e.g.
get).
config MessageQ_A_invalidMsg // module-wide |
|
Assert raised when an invalid message is supplied
extern const Assert_Id MessageQ_A_invalidMsg;
config MessageQ_A_invalidObj // module-wide |
|
Assert raised for an invalid MessageQ object
extern const Assert_Id MessageQ_A_invalidObj;
config MessageQ_A_invalidParam // module-wide |
|
Assert raised for an invalid parameter
extern const Assert_Id MessageQ_A_invalidParam;
config MessageQ_A_invalidQueueId // module-wide |
|
Assert raised when an invalid queueId is supplied
extern const Assert_Id MessageQ_A_invalidQueueId;
config MessageQ_A_invalidUnblock // module-wide |
|
Assert raised when attempting to unblock a remote MessageQ or one that
has been configured with a non-blocking synchronizer
extern const Assert_Id MessageQ_A_invalidUnblock;
config MessageQ_A_procIdInvalid // module-wide |
|
Assert raised when using an invalid procId
extern const Assert_Id MessageQ_A_procIdInvalid;
config MessageQ_A_unregisteredTransport // module-wide |
|
Assert raised when attempting to send a message to a core
where a transport has not been registered
extern const Assert_Id MessageQ_A_unregisteredTransport;
config MessageQ_E_maxReached // module-wide |
|
Error raised if all the message queue objects are taken
extern const Error_Id MessageQ_E_maxReached;
config MessageQ_E_nameFailed // module-wide |
|
Error raised in a create call when a name fails to be added
to the NameServer table. This can be because the name already
exists, the table has reached its max length, or out of memory
extern const Error_Id MessageQ_E_nameFailed;
config MessageQ_E_unregisterHeapId // module-wide |
|
Error raised when heapId has not been registered
extern const Error_Id MessageQ_E_unregisterHeapId;
config MessageQ_LM_alloc // module-wide |
|
Logged when allocating a message
DETAILS
When the
traceFlag is true, all message allocations
are logged.
config MessageQ_LM_free // module-wide |
|
Logged when freeing a message
DETAILS
When the
traceFlag is true, all freeing of messages
are logged. If an individual message's tracing was enabled
via
setMsgTrace, the MessageQ_free is also logged.
config MessageQ_LM_get // module-wide |
|
Logged when a message is received off the queue
DETAILS
When the
traceFlag is true, all getting of messages
are logged. If an individual message's tracing
was enabled via
setMsgTrace, the MessageQ_get is
also logged.
config MessageQ_LM_putLocal // module-wide |
|
Logged when a message is placed onto a local queue
DETAILS
When the
traceFlag is true, all putting of messages
are logged. If an individual message's tracing was enabled
via
setMsgTrace, the MessageQ_put is also logged.
config MessageQ_LM_putRemote // module-wide |
|
Logged when a message is given to a transport
extern const Log_Event MessageQ_LM_putRemote;
DETAILS
When the
traceFlag is true, all putting of messages
to a transport are logged. If an individual message's tracing
was enabled via
setMsgTrace, the MessageQ_put is
also logged.
config MessageQ_LM_rcvByTransport // module-wide |
|
Logged when a transport receives an incoming message
extern const Log_Event MessageQ_LM_rcvByTransport;
DETAILS
When the
traceFlag is true, all incoming messages
are logged. If an individual message's tracing
was enabled via
setMsgTrace, the receiving of a message is
also logged.
config MessageQ_LM_setTrace // module-wide |
|
Logged when setting the trace flag on a message
DETAILS
This is logged when tracing on a message is set via
setMsgTrace.
config MessageQ_LM_staticMsgInit // module-wide |
|
Logged when statically initializing a message
extern const Log_Event MessageQ_LM_staticMsgInit;
DETAILS
When the
traceFlag is true, all messages that
are statically initialized via
staticMsgInit are logged.
config MessageQ_maxNameLen // module-wide |
|
Maximum length for Message queue names
extern const UInt MessageQ_maxNameLen;
config MessageQ_maxRuntimeEntries // module-wide |
|
Maximum number of MessageQs that can be dynamically created
extern const UInt MessageQ_maxRuntimeEntries;
config MessageQ_nameTableGate // module-wide |
|
Gate used to make the name table thread safe
DETAILS
This gate is used when accessing the name table during
a
create,
delete, and
open.
This gate is also used to protect MessageQ when growing
internal tables in the
create.
The table is in local memory, not shared memory. So a
single processor gate will work.
The default will be
xdc.runtime.knl.GateThread
instance.
config MessageQ_numHeaps // module-wide |
|
Number of heapIds in the system
extern const UInt16 MessageQ_numHeaps;
DETAILS
This allows MessageQ to pre-allocate the heaps table.
The heaps table is used when registering heaps.
There is no default heap, so unless the system is only using
staticMsgInit, the application must register a heap.
config MessageQ_traceFlag // module-wide |
|
Trace setting
extern const Bool MessageQ_traceFlag;
DETAILS
This flag allows the configuration of the default module trace
settings.
MessageQ_registerTransport() // module-wide |
|
Register a transport with MessageQ
ARGUMENTS
transport
transport to register
procId
MultiProc id that transport communicates with
priority
priority of transport
RETURNS
Whether the register was successful.
DETAILS
This API is called by the transport when it is created.
MessageQ_unregisterTransport() // module-wide |
|
Unregister a transport with MessageQ
Void MessageQ_unregisterTransport(UInt16 procId, UInt priority);
ARGUMENTS
procId
unregister transport that communicates with
this remote processor
priority
priority of transport
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool MessageQ_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MessageQ_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MessageQ_Module_getMask();
// Returns the diagnostics mask for this module
Void MessageQ_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct MessageQ_Object MessageQ_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct MessageQ_Struct MessageQ_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct MessageQ_Params {
// Instance config-params structure
// Common per-instance configs
// ISync handle used to signal IO completion
} MessageQ_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config MessageQ_synchronizer // instance |
|
ISync handle used to signal IO completion
DETAILS
The ISync instance is used in the
get and
put.
The
xdc.runtime.knl.ISync.signal is called as part
of the
put call. The
xdc.runtime.knl.ISync.wait is
called in the
get if there are no messages present.
Instance Built-Ins |
|
Int MessageQ_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ');
local proxy modules
module-wide constants & types
module-wide config parameters
msg: "A_cannotFreeStaticMsg: Cannot call MessageQ_free with static msg"
};
msg: "A_heapIdInvalid: heapId is invalid"
};
msg: "A_invalidContext: Cannot call with an open/create handle"
};
msg: "A_invalidMsg: Invalid message"
};
msg: "A_invalidObj: an invalid obj is used"
};
msg: "A_invalidParam: an invalid parameter was passed in"
};
msg: "A_invalidQueueId: Invalid queueId is used"
};
msg: "A_invalidUnblock: Trying to unblock a remote MessageQ or a queue with non-blocking synchronizer"
};
msg: "A_procIdInvalid: procId is invalid"
};
msg: "A_unregisteredTransport: transport is not registered"
};
msg: "E_maxReached: All objects in use. MessageQ.maxRuntimeEntries is %d"
};
msg: "E_nameFailed: '%s' name failed to be added to NameServer"
};
msg: "E_unregisterHeapId: Heap id %d not registered"
};
msg: "LM_alloc: Message 0x%x (seqNum = %d, srcProc = %d) was allocated"
};
msg: "LM_free: Message 0x%x (seqNum = %d, srcProc = %d) was freed"
};
msg: "LM_get: Message 0x%x (seqNum = %d, srcProc = %d) was received by queue 0x%x"
};
msg: "LM_putLocal: Message 0x%x (seqNum = %d, srcProc = %d) was placed onto queue 0x%x"
};
msg: "LM_putRemote: Message 0x%x (seqNum = %d, srcProc = %d) was given to processor %d transport"
};
msg: "LM_rcvByTransport: Message 0x%x (seqNum = %d, srcProc = %d) was received"
};
msg: "LM_setTrace: Message 0x%x (seqNum = %d, srcProc = %d) traceFlag = %d"
};
msg: "LM_staticMsgInit: Message 0x%x (seqNum = %d, srcProc = %d) was set in MessageQ_staticMsgInit"
};
module-wide functions
per-instance config parameters
proxy MessageQ.SetupTransportProxy |
|
MessageQ transport setup proxy
XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
const MessageQ.HIGHPRI |
|
XDCscript usage |
meta-domain |
const MessageQ.HIGHPRI = 1;
C SYNOPSIS
const MessageQ.NORMALPRI |
|
Message priority values. These must match the values defined in
ti/ipc/MessageQ.h but are needed here for ROV
XDCscript usage |
meta-domain |
const MessageQ.NORMALPRI = 0;
C SYNOPSIS
const MessageQ.RESERVEDPRI |
|
XDCscript usage |
meta-domain |
const MessageQ.RESERVEDPRI = 2;
C SYNOPSIS
const MessageQ.URGENTPRI |
|
XDCscript usage |
meta-domain |
const MessageQ.URGENTPRI = 3;
C SYNOPSIS
config MessageQ.A_cannotFreeStaticMsg // module-wide |
|
Assert raised when attempting to free a static message
XDCscript usage |
meta-domain |
msg: "A_cannotFreeStaticMsg: Cannot call MessageQ_free with static msg"
};
C SYNOPSIS
config MessageQ.A_heapIdInvalid // module-wide |
|
Assert raised when using an invalid heapId
XDCscript usage |
meta-domain |
msg: "A_heapIdInvalid: heapId is invalid"
};
C SYNOPSIS
config MessageQ.A_invalidContext // module-wide |
|
Assert raised when calling API with wrong handle
XDCscript usage |
meta-domain |
msg: "A_invalidContext: Cannot call with an open/create handle"
};
DETAILS
Some APIs can only be called with an opened handle (e.g.
close. Some can only be called with a created handle
(e.g.
get).
C SYNOPSIS
config MessageQ.A_invalidMsg // module-wide |
|
Assert raised when an invalid message is supplied
XDCscript usage |
meta-domain |
msg: "A_invalidMsg: Invalid message"
};
C SYNOPSIS
config MessageQ.A_invalidObj // module-wide |
|
Assert raised for an invalid MessageQ object
XDCscript usage |
meta-domain |
msg: "A_invalidObj: an invalid obj is used"
};
C SYNOPSIS
config MessageQ.A_invalidParam // module-wide |
|
Assert raised for an invalid parameter
XDCscript usage |
meta-domain |
msg: "A_invalidParam: an invalid parameter was passed in"
};
C SYNOPSIS
config MessageQ.A_invalidQueueId // module-wide |
|
Assert raised when an invalid queueId is supplied
XDCscript usage |
meta-domain |
msg: "A_invalidQueueId: Invalid queueId is used"
};
C SYNOPSIS
config MessageQ.A_invalidUnblock // module-wide |
|
Assert raised when attempting to unblock a remote MessageQ or one that
has been configured with a non-blocking synchronizer
XDCscript usage |
meta-domain |
msg: "A_invalidUnblock: Trying to unblock a remote MessageQ or a queue with non-blocking synchronizer"
};
C SYNOPSIS
config MessageQ.A_procIdInvalid // module-wide |
|
Assert raised when using an invalid procId
XDCscript usage |
meta-domain |
msg: "A_procIdInvalid: procId is invalid"
};
C SYNOPSIS
config MessageQ.A_unregisteredTransport // module-wide |
|
Assert raised when attempting to send a message to a core
where a transport has not been registered
XDCscript usage |
meta-domain |
msg: "A_unregisteredTransport: transport is not registered"
};
C SYNOPSIS
config MessageQ.E_maxReached // module-wide |
|
Error raised if all the message queue objects are taken
XDCscript usage |
meta-domain |
msg: "E_maxReached: All objects in use. MessageQ.maxRuntimeEntries is %d"
};
C SYNOPSIS
config MessageQ.E_nameFailed // module-wide |
|
Error raised in a create call when a name fails to be added
to the NameServer table. This can be because the name already
exists, the table has reached its max length, or out of memory
XDCscript usage |
meta-domain |
msg: "E_nameFailed: '%s' name failed to be added to NameServer"
};
C SYNOPSIS
config MessageQ.E_unregisterHeapId // module-wide |
|
Error raised when heapId has not been registered
XDCscript usage |
meta-domain |
msg: "E_unregisterHeapId: Heap id %d not registered"
};
C SYNOPSIS
config MessageQ.LM_alloc // module-wide |
|
Logged when allocating a message
XDCscript usage |
meta-domain |
msg: "LM_alloc: Message 0x%x (seqNum = %d, srcProc = %d) was allocated"
};
DETAILS
When the
traceFlag is true, all message allocations
are logged.
C SYNOPSIS
config MessageQ.LM_free // module-wide |
|
Logged when freeing a message
XDCscript usage |
meta-domain |
msg: "LM_free: Message 0x%x (seqNum = %d, srcProc = %d) was freed"
};
DETAILS
When the
traceFlag is true, all freeing of messages
are logged. If an individual message's tracing was enabled
via
setMsgTrace, the MessageQ_free is also logged.
C SYNOPSIS
config MessageQ.LM_get // module-wide |
|
Logged when a message is received off the queue
XDCscript usage |
meta-domain |
msg: "LM_get: Message 0x%x (seqNum = %d, srcProc = %d) was received by queue 0x%x"
};
DETAILS
When the
traceFlag is true, all getting of messages
are logged. If an individual message's tracing
was enabled via
setMsgTrace, the MessageQ_get is
also logged.
C SYNOPSIS
config MessageQ.LM_putLocal // module-wide |
|
Logged when a message is placed onto a local queue
XDCscript usage |
meta-domain |
msg: "LM_putLocal: Message 0x%x (seqNum = %d, srcProc = %d) was placed onto queue 0x%x"
};
DETAILS
When the
traceFlag is true, all putting of messages
are logged. If an individual message's tracing was enabled
via
setMsgTrace, the MessageQ_put is also logged.
C SYNOPSIS
config MessageQ.LM_putRemote // module-wide |
|
Logged when a message is given to a transport
XDCscript usage |
meta-domain |
msg: "LM_putRemote: Message 0x%x (seqNum = %d, srcProc = %d) was given to processor %d transport"
};
DETAILS
When the
traceFlag is true, all putting of messages
to a transport are logged. If an individual message's tracing
was enabled via
setMsgTrace, the MessageQ_put is
also logged.
C SYNOPSIS
config MessageQ.LM_rcvByTransport // module-wide |
|
Logged when a transport receives an incoming message
XDCscript usage |
meta-domain |
msg: "LM_rcvByTransport: Message 0x%x (seqNum = %d, srcProc = %d) was received"
};
DETAILS
When the
traceFlag is true, all incoming messages
are logged. If an individual message's tracing
was enabled via
setMsgTrace, the receiving of a message is
also logged.
C SYNOPSIS
config MessageQ.LM_setTrace // module-wide |
|
Logged when setting the trace flag on a message
XDCscript usage |
meta-domain |
msg: "LM_setTrace: Message 0x%x (seqNum = %d, srcProc = %d) traceFlag = %d"
};
DETAILS
This is logged when tracing on a message is set via
setMsgTrace.
C SYNOPSIS
config MessageQ.LM_staticMsgInit // module-wide |
|
Logged when statically initializing a message
XDCscript usage |
meta-domain |
msg: "LM_staticMsgInit: Message 0x%x (seqNum = %d, srcProc = %d) was set in MessageQ_staticMsgInit"
};
DETAILS
When the
traceFlag is true, all messages that
are statically initialized via
staticMsgInit are logged.
C SYNOPSIS
config MessageQ.maxNameLen // module-wide |
|
Maximum length for Message queue names
XDCscript usage |
meta-domain |
MessageQ.maxNameLen = UInt 32;
C SYNOPSIS
config MessageQ.maxRuntimeEntries // module-wide |
|
Maximum number of MessageQs that can be dynamically created
XDCscript usage |
meta-domain |
C SYNOPSIS
config MessageQ.nameTableGate // module-wide |
|
Gate used to make the name table thread safe
XDCscript usage |
meta-domain |
DETAILS
This gate is used when accessing the name table during
a
create,
delete, and
open.
This gate is also used to protect MessageQ when growing
internal tables in the
create.
The table is in local memory, not shared memory. So a
single processor gate will work.
The default will be
xdc.runtime.knl.GateThread
instance.
C SYNOPSIS
config MessageQ.numHeaps // module-wide |
|
Number of heapIds in the system
XDCscript usage |
meta-domain |
MessageQ.numHeaps = UInt16 8;
DETAILS
This allows MessageQ to pre-allocate the heaps table.
The heaps table is used when registering heaps.
There is no default heap, so unless the system is only using
staticMsgInit, the application must register a heap.
C SYNOPSIS
config MessageQ.traceFlag // module-wide |
|
Trace setting
XDCscript usage |
meta-domain |
MessageQ.traceFlag = Bool false;
DETAILS
This flag allows the configuration of the default module trace
settings.
C SYNOPSIS
metaonly config MessageQ.common$ // module-wide |
|
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config MessageQ.tableSection // module-wide |
|
Section name is used to place the names table
XDCscript usage |
meta-domain |
MessageQ.tableSection = String null;
metaonly MessageQ.registerHeapMeta() // module-wide |
|
Statically register a heap with MessageQ
XDCscript usage |
meta-domain |
MessageQ.
registerHeapMeta(
IHeap.Handle heap,
UInt16 heapId)
returns Void
ARGUMENTS
heap
Heap to register
heapId
heapId associated with the heap
DETAILS
Build error if heapId is in use.
metaonly MessageQ.registerTransportMeta() // module-wide |
|
Statically register a transport with MessageQ
XDCscript usage |
meta-domain |
ARGUMENTS
transport
transport to register
procId
procId that transport communicaties with
priority
priority of transport
DETAILS
Build error if remote processor already has a transport
registered.
Instance Config Parameters |
|
XDCscript usage |
meta-domain |
var params = new MessageQ.Params;
// Instance config-params object
// ISync handle used to signal IO completion
config MessageQ.synchronizer // instance |
|
ISync handle used to signal IO completion
XDCscript usage |
meta-domain |
var params = new MessageQ.Params;
...
DETAILS
The ISync instance is used in the
get and
put.
The
xdc.runtime.knl.ISync.signal is called as part
of the
put call. The
xdc.runtime.knl.ISync.wait is
called in the
get if there are no messages present.
C SYNOPSIS
generated on Tue, 22 May 2012 23:45:03 GMT