interface ti.sdo.ipc.interfaces.IMessageQTransport

Interface for the transports used by MessageQ

The transport implementations have to register with ti.sdo.ipc.MessageQ. This is done via the ti.sdo.ipc.MessageQ.registerTransport function. [ more ... ]
XDCspec summary sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
interface IMessageQTransport {  ...
// inherits xdc.runtime.IModule
instance:  ...
XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
 
interface IMessageQTransport {
module-wide constants & types
        Reason_FAILEDPUT,
        Reason_INTERNALERR,
        Reason_PHYSICALERR,
        Reason_FAILEDALLOC
    };
 
        S_SUCCESS,
        E_FAIL,
        E_ERROR
    };
 
module-wide config parameters
 
module-wide functions
 
 
instance:
per-instance config parameters
per-instance creation
    create// Create an instance-object(UInt16 procId);
per-instance functions
    Bool control// Send a control command to the transport instance(UInt cmd, UArg cmdArg);
}
DETAILS
The transport implementations have to register with ti.sdo.ipc.MessageQ. This is done via the ti.sdo.ipc.MessageQ.registerTransport function.
If transports need additional processing during startup, there are multiple hook points to run start-up code that the transport implementation can use.
 
enum IMessageQTransport.Reason

Reason for error function being called

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
enum Reason {
    Reason_FAILEDPUT,
    Reason_INTERNALERR,
    Reason_PHYSICALERR,
    Reason_FAILEDALLOC
};
 
DETAILS
First field in the errFxn
 
enum IMessageQTransport.Status

Transport return values

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
enum Status {
    S_SUCCESS,
    E_FAIL,
    E_ERROR
};
 
DETAILS
  • S_SUCCESS: Operation was successful
  • E_FAIL: Operation resulted in a failure
  • E_ERROR: Operation resulted in an error.
 
typedef IMessageQTransport.ErrFxn

Typedef for transport error callback function

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
typedef Void (*ErrFxn)(IMessageQTransport.Reason,IMessageQTransport.Handle,Ptr,UArg);
 
DETAILS
First parameter: Why the error function is being called.
Second parameter: Handle of transport that had the error. NULL denotes that it is a system error, not a specific transport.
Third parameter: Pointer to the message. This is only valid for Reason_FAILEDPUT.
Fourth parameter: Transport specific information. Refer to individual transports for more details.
 
config IMessageQTransport.errFxn  // module-wide

Asynchronous error function for the transport module

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
config IMessageQTransport.ErrFxn errFxn = null;
 
 
metaonly config IMessageQTransport.common$  // module-wide

Common module configuration parameters

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
metaonly config Types.Common$ common$;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
IMessageQTransport.setErrFxn()  // module-wide

Sets the asynchronous error function for the transport module

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
Void setErrFxn(IMessageQTransport.ErrFxn errFxn);
 
ARGUMENTS
errFxn — Function that is called when an asynchronous error occurs.
DETAILS
This API allows the user to set the function that will be called in case of an asynchronous error by the transport.
 
config IMessageQTransport.priority  // instance

Which priority messages should this transport manage

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
config UInt priority = 0;
 
Instance Creation

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
create(UInt16 procId);
// Create an instance-object
ARGUMENTS
procId — Remote processor id that this instance will communicate with.
DETAILS
This function creates a transport instance. The transport is responsible for registering with MessageQ via the ti.sdo.ipc.MessageQ.registerTransport API.
 
IMessageQTransport.control()  // instance

Send a control command to the transport instance

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
Bool control(UInt cmd, UArg cmdArg);
 
ARGUMENTS
cmd — Requested command
cmdArgs — Accompanying field for the command. This is command specific.
RETURNS
TRUE denotes acceptance of the command. FALSE denotes failure of the command.
DETAILS
This is function allows transport to specify control commands. Refer to individual transport implementions for more details.
 
IMessageQTransport.getStatus()  // instance

Status of a Transport instance

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
Int getStatus();
 
RETURNS
Returns status of Transport instance
DETAILS
This function returns the status of the transport instance.
 
IMessageQTransport.put()  // instance

Put the message to the remote processor

XDCspec declarations sourced in ti/sdo/ipc/interfaces/IMessageQTransport.xdc
Bool put(Ptr msg);
 
ARGUMENTS
msg — Pointer the message to be sent
RETURNS
TRUE denotes acceptance of the message to be sent. FALSE denotes the message could not be sent.
DETAILS
If the transport can accept the message, it returns TRUE. Accepting a message does not mean that it is transmitted. It simply means that the transport should be able to send the message. If the actual transfer fails, the transport calls the {@#ErrFxn} (assuming it is set up via the {@#setErrFxn} API. If the {@#ErrFxn} is not set, the message is dropped. (also...should an error be raised or just System_printf?).
If the transport cannot send the message, it returns FALSE and a filled in Error_Block. The caller still owns the message.
generated on Tue, 22 May 2012 23:44:56 GMT