interface ti.sdo.ipc.interfaces.INotifyDriver

Notify driver interface

Interface implemented by all drivers for the notify module. Modules that implement this interface expect the eventId arguments to be valid.
XDCspec summary sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
interface INotifyDriver {  ...
// inherits xdc.runtime.IModule
instance:  ...
XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
 
interface INotifyDriver {
module-wide config parameters
 
 
instance:
per-instance functions
    Void disableEvent// Disable an event(UInt32 eventId);
    Void enableEvent// Enable an event(UInt32 eventId);
    Void registerEvent// Register a callback to an event(UInt32 eventId);
    Int sendEvent// Send a signal to an event(UInt32 eventId, UInt32 payload, Bool waitClear);
}
 
metaonly config INotifyDriver.common$  // module-wide

Common module configuration parameters

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
metaonly config Types.Common$ common$;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
INotifyDriver.disable()  // instance

Disable a NotifyDriver instance

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Void disable();
 
DETAILS
Disables the ability of a Notify driver to receive events for a given processor. This interface function is called by the Notify_disable function. Refer to its documentation for more details.
 
INotifyDriver.disableEvent()  // instance

Disable an event

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Void disableEvent(UInt32 eventId);
 
ARGUMENTS
eventId — Number of event to disable
DETAILS
This interface function is called by the Notify_disableEvent function. Refer to its documentation for more details.
The Notify module does validation of the eventId. The Notify module enters calls this function within the Notify module gate.
 
INotifyDriver.enable()  // instance

Enable a NotifyDriver instance

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Void enable();
 
DETAILS
Enables the ability of a Notify driver to receive events for a given processor. This interface function is called by the Notify_restore function. Refer to its documentation for more details.
 
INotifyDriver.enableEvent()  // instance

Enable an event

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Void enableEvent(UInt32 eventId);
 
ARGUMENTS
eventId — Number of event to enable
DETAILS
This interface function is called by the Notify_disableEvent function. Refer to its documentation for more details.
The Notify module does validation of the eventId. The Notify module enters calls this function within the Notify module gate.
 
INotifyDriver.registerEvent()  // instance

Register a callback to an event

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Void registerEvent(UInt32 eventId);
 
ARGUMENTS
eventId — Number of event that is being registered
DETAILS
This driver function is called by the Notify_registerEvent function within the Notify module gate. Refer to its documentation for more details.
 
INotifyDriver.sendEvent()  // instance

Send a signal to an event

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Int sendEvent(UInt32 eventId, UInt32 payload, Bool waitClear);
 
ARGUMENTS
eventId — Number of event to signal
payload — Payload (optional) to pass to callback function
waitClear — If TRUE, have the NotifyDriver wait for acknowledgement back from the destination processor.
RETURNS
Notify status
DETAILS
This interface function is called by the Notify_sendEvent function. Notify_sendEvent does not provide any context protection for INotifyDriver_sendEvent, so appropriate measures must be taken within the driver itself.
 
INotifyDriver.unregisterEvent()  // instance

Remove an event listener from an event

XDCspec declarations sourced in ti/sdo/ipc/interfaces/INotifyDriver.xdc
Void unregisterEvent(UInt32 eventId);
 
ARGUMENTS
eventId — Number of event that is being unregistered
DETAILS
This driver function is called by the Notify_unregisterEvent function within the Notify module gate. Refer to it for more details.
generated on Tue, 22 May 2012 23:44:56 GMT