module ti.sdo.ipc.gates.GateMPSupportNull

Module to plug GateMP proxies

C synopsis target-domain sourced in ti/sdo/ipc/gates/GateMPSupportNull.xdc
#include <ti/sdo/ipc/gates/GateMPSupportNull.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
Bool 
Functions common to all IGateMPSupport modules
SizeT 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef enum
typedef struct
typedef struct
typedef struct
Constants
extern const Assert_Id 
 
 
const GateMPSupportNull_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GateMPSupportNull_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GateMPSupportNull_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GateMPSupportNull_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
enum GateMPSupportNull_Action

Error codes returned by certain calls in GateMP

C synopsis target-domain
typedef enum GateMPSupportNull_Action {
    GateMPSupportNull_Action_NONE,
    GateMPSupportNull_Action_ASSERT
} GateMPSupportNull_Action;
 
 
config GateMPSupportNull_A_invalidAction  // module-wide

Assert raised when trying to use GateMPSupportNull's enter or leave

C synopsis target-domain
extern const Assert_Id GateMPSupportNull_A_invalidAction;
 
 
config GateMPSupportNull_action  // module-wide

Assert if the enter and/or leave is called

C synopsis target-domain
extern const GateMPSupportNull_Action GateMPSupportNull_action;
 
 
GateMPSupportNull_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GateMPSupportNull_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
GateMPSupportNull_sharedMemReq()  // module-wide

Amount of shared memory required for creation of each instance

C synopsis target-domain
SizeT GateMPSupportNull_sharedMemReq(IGateMPSupport_Params *params);
 
ARGUMENTS
params — Pointer to the parameters that will be used in the create.
DETAILS
The value returned by this function may depend on the cache alignment requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GateMPSupportNull_Module_id();
// Get this module's unique id
 
Bool GateMPSupportNull_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GateMPSupportNull_Module_heap();
// The heap from which this module allocates memory
 
Bool GateMPSupportNull_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GateMPSupportNull_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GateMPSupportNull_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GateMPSupportNull_Object GateMPSupportNull_Object;
// Opaque internal representation of an instance object
 
typedef GateMPSupportNull_Object *GateMPSupportNull_Handle;
// Client reference to an instance object
 
typedef struct GateMPSupportNull_Struct GateMPSupportNull_Struct;
// Opaque client structure large enough to hold an instance object
 
GateMPSupportNull_Handle GateMPSupportNull_handle(GateMPSupportNull_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GateMPSupportNull_Struct *GateMPSupportNull_struct(GateMPSupportNull_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GateMPSupportNull_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt resourceId;
    // Logical resource id
    Ptr sharedAddr;
    // Physical address of the shared memory
} GateMPSupportNull_Params;
 
Void GateMPSupportNull_Params_init(GateMPSupportNull_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config GateMPSupportNull_resourceId  // instance

Logical resource id

C synopsis target-domain
      ...
    UInt resourceId;
 
 
config GateMPSupportNull_sharedAddr  // instance

Physical address of the shared memory

C synopsis target-domain
      ...
    Ptr sharedAddr;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Instance Creation

C synopsis target-domain
GateMPSupportNull_Handle GateMPSupportNull_create(IGateProvider_Handle localGate, const GateMPSupportNull_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GateMPSupportNull_construct(GateMPSupportNull_Struct *structP, IGateProvider_Handle localGate, const GateMPSupportNull_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
Instance Deletion

C synopsis target-domain
Void GateMPSupportNull_delete(GateMPSupportNull_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GateMPSupportNull_destruct(GateMPSupportNull_Struct *structP);
// Finalize the instance object inside the provided structure
Instance Convertors

C synopsis target-domain
IGateMPSupport_Handle GateMPSupportNull_Handle_upCast(GateMPSupportNull_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GateMPSupportNull_Handle GateMPSupportNull_Handle_downCast(IGateMPSupport_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
IGateProvider_Handle GateMPSupportNull_Handle_upCast2(GateMPSupportNull_Handle handle);
// unconditionally move 2 levels up the inheritance hierarchy
 
GateMPSupportNull_Handle GateMPSupportNull_Handle_downCast2(IGateProvider_Handle handle);
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GateMPSupportNull_Object_count();
// The number of statically-created instance objects
 
GateMPSupportNull_Handle GateMPSupportNull_Object_get(GateMPSupportNull_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GateMPSupportNull_Handle GateMPSupportNull_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GateMPSupportNull_Handle GateMPSupportNull_Object_next(GateMPSupportNull_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GateMPSupportNull_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GateMPSupportNull_Handle_label(GateMPSupportNull_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GateMPSupportNull_Handle_name(GateMPSupportNull_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/gates/GateMPSupportNull.xdc
var GateMPSupportNull = xdc.useModule('ti.sdo.ipc.gates.GateMPSupportNull');
module-wide constants & types
 
        const GateMPSupportNull.Action_NONE;
        const GateMPSupportNull.Action_ASSERT;
module-wide config parameters
        msg: "A_invalidAction: Cannot use ti.sdo.ipc.gates.GateMPSupportNull"
    };
 
module-wide functions
per-instance config parameters
    var params = new GateMPSupportNull.Params// Instance config-params object;
        params.resourceId// Logical resource id = UInt 0;
        params.sharedAddr// Physical address of the shared memory = Ptr null;
per-instance creation
    var inst = GateMPSupportNull.create// Create an instance-object(IGateProvider.Handle localGate, params);
 
 
const GateMPSupportNull.Q_BLOCKING

Blocking quality

XDCscript usage meta-domain
const GateMPSupportNull.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GateMPSupportNull.Q_PREEMPTING

Preempting quality

XDCscript usage meta-domain
const GateMPSupportNull.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
enum GateMPSupportNull.Action

Error codes returned by certain calls in GateMP

XDCscript usage meta-domain
values of type GateMPSupportNull.Action
    const GateMPSupportNull.Action_NONE;
    const GateMPSupportNull.Action_ASSERT;
 
C SYNOPSIS
 
config GateMPSupportNull.A_invalidAction  // module-wide

Assert raised when trying to use GateMPSupportNull's enter or leave

XDCscript usage meta-domain
GateMPSupportNull.A_invalidAction = Assert.Desc {
    msg: "A_invalidAction: Cannot use ti.sdo.ipc.gates.GateMPSupportNull"
};
 
C SYNOPSIS
 
config GateMPSupportNull.action  // module-wide

Assert if the enter and/or leave is called

XDCscript usage meta-domain
 
C SYNOPSIS
 
metaonly config GateMPSupportNull.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
GateMPSupportNull.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GateMPSupportNull.getNumResources()  // module-wide

Returns the number of resources offered by the GateMP delegate

XDCscript usage meta-domain
GateMPSupportNull.getNumResources() returns UInt
 
 
metaonly GateMPSupportNull.queryMeta()  // module-wide

Configuration time test for a particular gate quality

XDCscript usage meta-domain
GateMPSupportNull.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Instance Config Parameters

XDCscript usage meta-domain
var params = new GateMPSupportNull.Params;
// Instance config-params object
    params.resourceId = UInt 0;
    // Logical resource id
    params.sharedAddr = Ptr null;
    // Physical address of the shared memory
 
config GateMPSupportNull.resourceId  // instance

Logical resource id

XDCscript usage meta-domain
var params = new GateMPSupportNull.Params;
  ...
params.resourceId = UInt 0;
 
C SYNOPSIS
 
config GateMPSupportNull.sharedAddr  // instance

Physical address of the shared memory

XDCscript usage meta-domain
var params = new GateMPSupportNull.Params;
  ...
params.sharedAddr = Ptr null;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Instance Creation

XDCscript usage meta-domain
var params = new GateMPSupportNull.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GateMPSupportNull.create(IGateProvider.Handle localGate, params);
// Create an instance-object
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
generated on Tue, 22 May 2012 23:44:53 GMT