module ti.sdo.ipc.gates.GatePeterson

IGateMPSupport gate based on the Peterson algorithm

This module implements the ti.sdo.ipc.interfaces.IGateMPSupport interface using the Peterson Algorithm in shared memory. This implementation works for only 2 processors. [ more ... ]
C synopsis target-domain sourced in ti/sdo/ipc/gates/GatePeterson.xdc
#include <ti/sdo/ipc/gates/GatePeterson.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
Bool 
Functions common to all IGateMPSupport modules
SizeT 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef struct
typedef struct
Constants
extern const Error_Id 
extern const UInt 
 
DETAILS
This module implements the ti.sdo.ipc.interfaces.IGateMPSupport interface using the Peterson Algorithm in shared memory. This implementation works for only 2 processors.
Each GatePeterson instance requires a small piece of shared memory. The base address of this shared memory is specified as the 'sharedAddr' argument to the create. The amount of shared memory consumed by a single instance can be obtained using the sharedMemReq call.
Shared memory has to conform to the following specification. Padding is added between certain elements in shared memory if cache alignment is required for the region in which the instance is placed.
              shmBaseAddr -> --------------------------- bytes
                             |  version                | 4
              (Attrs struct) |  creatorProcId          | 2
                             |  openerProcId           | 2
                             |  (PADDING if aligned)   | 
                             |-------------------------|
                             |  flag[0]                | 2
                             |  (PADDING if aligned)   | 
                             |-------------------------|
                             |  flag[1]                | 2
                             |  (PADDING if aligned)   | 
                             |-------------------------|
                             |  turn                   | 2
                             |  (PADDING if aligned)   | 
                             |-------------------------|
 
const GatePeterson_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GatePeterson_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GatePeterson_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GatePeterson_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
config GatePeterson_E_gateRemotelyOpened  // module-wide

Error raised when gate cannot be opened because of the opener's ID

C synopsis target-domain
extern const Error_Id GatePeterson_E_gateRemotelyOpened;
 
DETAILS
Error raised in open when trying to remotely open a GatePeterson instance whose configured opener processor Id does not match that of the opener's MultiProc id. but it has already been opened/created on two other processors. GatePeterson only works with two processors.
 
config GatePeterson_numInstances  // module-wide

Maximum number of instances supported by the GatePeterson module

C synopsis target-domain
extern const UInt GatePeterson_numInstances;
 
 
GatePeterson_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GatePeterson_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
GatePeterson_sharedMemReq()  // module-wide

Amount of shared memory required for creation of each instance

C synopsis target-domain
SizeT GatePeterson_sharedMemReq(IGateMPSupport_Params *params);
 
ARGUMENTS
params — Pointer to the parameters that will be used in the create.
DETAILS
The value returned by this function may depend on the cache alignment requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GatePeterson_Module_id();
// Get this module's unique id
 
Bool GatePeterson_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GatePeterson_Module_heap();
// The heap from which this module allocates memory
 
Bool GatePeterson_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GatePeterson_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GatePeterson_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GatePeterson_Object GatePeterson_Object;
// Opaque internal representation of an instance object
 
typedef GatePeterson_Object *GatePeterson_Handle;
// Client reference to an instance object
 
typedef struct GatePeterson_Struct GatePeterson_Struct;
// Opaque client structure large enough to hold an instance object
 
GatePeterson_Handle GatePeterson_handle(GatePeterson_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GatePeterson_Struct *GatePeterson_struct(GatePeterson_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GatePeterson_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt resourceId;
    // Logical resource id
    Ptr sharedAddr;
    // Physical address of the shared memory
} GatePeterson_Params;
 
Void GatePeterson_Params_init(GatePeterson_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config GatePeterson_resourceId  // instance

Logical resource id

C synopsis target-domain
      ...
    UInt resourceId;
 
 
config GatePeterson_sharedAddr  // instance

Physical address of the shared memory

C synopsis target-domain
      ...
    Ptr sharedAddr;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Instance Creation

C synopsis target-domain
GatePeterson_Handle GatePeterson_create(IGateProvider_Handle localGate, const GatePeterson_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GatePeterson_construct(GatePeterson_Struct *structP, IGateProvider_Handle localGate, const GatePeterson_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
Instance Deletion

C synopsis target-domain
Void GatePeterson_delete(GatePeterson_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GatePeterson_destruct(GatePeterson_Struct *structP);
// Finalize the instance object inside the provided structure
Instance Convertors

C synopsis target-domain
IGateMPSupport_Handle GatePeterson_Handle_upCast(GatePeterson_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GatePeterson_Handle GatePeterson_Handle_downCast(IGateMPSupport_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
IGateProvider_Handle GatePeterson_Handle_upCast2(GatePeterson_Handle handle);
// unconditionally move 2 levels up the inheritance hierarchy
 
GatePeterson_Handle GatePeterson_Handle_downCast2(IGateProvider_Handle handle);
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GatePeterson_Object_count();
// The number of statically-created instance objects
 
GatePeterson_Handle GatePeterson_Object_get(GatePeterson_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GatePeterson_Handle GatePeterson_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GatePeterson_Handle GatePeterson_Object_next(GatePeterson_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GatePeterson_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GatePeterson_Handle_label(GatePeterson_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GatePeterson_Handle_name(GatePeterson_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/gates/GatePeterson.xdc
var GatePeterson = xdc.useModule('ti.sdo.ipc.gates.GatePeterson');
module-wide constants & types
module-wide config parameters
        msg: "E_gateRemotelyOpened: Gate already in use by two other processors: creator: %d, opener: %d"
    };
 
module-wide functions
per-instance config parameters
    var params = new GatePeterson.Params// Instance config-params object;
        params.resourceId// Logical resource id = UInt 0;
        params.sharedAddr// Physical address of the shared memory = Ptr null;
per-instance creation
    var inst = GatePeterson.create// Create an instance-object(IGateProvider.Handle localGate, params);
 
 
const GatePeterson.Q_BLOCKING

Blocking quality

XDCscript usage meta-domain
const GatePeterson.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GatePeterson.Q_PREEMPTING

Preempting quality

XDCscript usage meta-domain
const GatePeterson.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
config GatePeterson.E_gateRemotelyOpened  // module-wide

Error raised when gate cannot be opened because of the opener's ID

XDCscript usage meta-domain
GatePeterson.E_gateRemotelyOpened = Error.Desc {
    msg: "E_gateRemotelyOpened: Gate already in use by two other processors: creator: %d, opener: %d"
};
 
DETAILS
Error raised in open when trying to remotely open a GatePeterson instance whose configured opener processor Id does not match that of the opener's MultiProc id. but it has already been opened/created on two other processors. GatePeterson only works with two processors.
C SYNOPSIS
 
config GatePeterson.numInstances  // module-wide

Maximum number of instances supported by the GatePeterson module

XDCscript usage meta-domain
GatePeterson.numInstances = UInt 512;
 
C SYNOPSIS
 
metaonly config GatePeterson.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
GatePeterson.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GatePeterson.getNumResources()  // module-wide

Returns the number of resources offered by the GateMP delegate

XDCscript usage meta-domain
GatePeterson.getNumResources() returns UInt
 
 
metaonly GatePeterson.queryMeta()  // module-wide

Configuration time test for a particular gate quality

XDCscript usage meta-domain
GatePeterson.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Instance Config Parameters

XDCscript usage meta-domain
var params = new GatePeterson.Params;
// Instance config-params object
    params.resourceId = UInt 0;
    // Logical resource id
    params.sharedAddr = Ptr null;
    // Physical address of the shared memory
 
config GatePeterson.resourceId  // instance

Logical resource id

XDCscript usage meta-domain
var params = new GatePeterson.Params;
  ...
params.resourceId = UInt 0;
 
C SYNOPSIS
 
config GatePeterson.sharedAddr  // instance

Physical address of the shared memory

XDCscript usage meta-domain
var params = new GatePeterson.Params;
  ...
params.sharedAddr = Ptr null;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Instance Creation

XDCscript usage meta-domain
var params = new GatePeterson.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GatePeterson.create(IGateProvider.Handle localGate, params);
// Create an instance-object
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
generated on Tue, 22 May 2012 23:44:53 GMT