module ti.sdo.ipc.gates.GateHWSpinlock

Multiprocessor gate that utilizes a hardware spinlock

C synopsis target-domain sourced in ti/sdo/ipc/gates/GateHWSpinlock.xdc
#include <ti/sdo/ipc/gates/GateHWSpinlock.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
Bool 
Functions common to all IGateMPSupport modules
SizeT 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef struct
typedef struct
Constants
extern const Assert_Id 
extern const Ptr 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
 
 
const GateHWSpinlock_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GateHWSpinlock_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GateHWSpinlock_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GateHWSpinlock_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
config GateHWSpinlock_A_invSpinLockNum  // module-wide

Assert raised when provided lockNum is invalid for the relevant device

C synopsis target-domain
extern const Assert_Id GateHWSpinlock_A_invSpinLockNum;
 
 
config GateHWSpinlock_LM_close  // module-wide

Logged on gate close

C synopsis target-domain
extern const Log_Event GateHWSpinlock_LM_close;
 
 
config GateHWSpinlock_LM_create  // module-wide

Logged on gate create

C synopsis target-domain
extern const Log_Event GateHWSpinlock_LM_create;
 
 
config GateHWSpinlock_LM_delete  // module-wide

Logged on gate deletion

C synopsis target-domain
extern const Log_Event GateHWSpinlock_LM_delete;
 
 
config GateHWSpinlock_LM_enter  // module-wide

Logged on gate enter

C synopsis target-domain
extern const Log_Event GateHWSpinlock_LM_enter;
 
 
config GateHWSpinlock_LM_leave  // module-wide

Logged on gate leave

C synopsis target-domain
extern const Log_Event GateHWSpinlock_LM_leave;
 
 
config GateHWSpinlock_LM_open  // module-wide

Logged on gate open

C synopsis target-domain
extern const Log_Event GateHWSpinlock_LM_open;
 
 
config GateHWSpinlock_baseAddr  // module-wide

Device-specific base address for HW Semaphore subsystem

C synopsis target-domain
extern const Ptr GateHWSpinlock_baseAddr;
 
 
GateHWSpinlock_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GateHWSpinlock_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
GateHWSpinlock_sharedMemReq()  // module-wide

Amount of shared memory required for creation of each instance

C synopsis target-domain
SizeT GateHWSpinlock_sharedMemReq(IGateMPSupport_Params *params);
 
ARGUMENTS
params — Pointer to the parameters that will be used in the create.
DETAILS
The value returned by this function may depend on the cache alignment requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GateHWSpinlock_Module_id();
// Get this module's unique id
 
Bool GateHWSpinlock_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GateHWSpinlock_Module_heap();
// The heap from which this module allocates memory
 
Bool GateHWSpinlock_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GateHWSpinlock_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GateHWSpinlock_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GateHWSpinlock_Object GateHWSpinlock_Object;
// Opaque internal representation of an instance object
 
typedef GateHWSpinlock_Object *GateHWSpinlock_Handle;
// Client reference to an instance object
 
typedef struct GateHWSpinlock_Struct GateHWSpinlock_Struct;
// Opaque client structure large enough to hold an instance object
 
GateHWSpinlock_Handle GateHWSpinlock_handle(GateHWSpinlock_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GateHWSpinlock_Struct *GateHWSpinlock_struct(GateHWSpinlock_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GateHWSpinlock_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt resourceId;
    // Logical resource id
    Ptr sharedAddr;
    // Physical address of the shared memory
} GateHWSpinlock_Params;
 
Void GateHWSpinlock_Params_init(GateHWSpinlock_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config GateHWSpinlock_resourceId  // instance

Logical resource id

C synopsis target-domain
      ...
    UInt resourceId;
 
 
config GateHWSpinlock_sharedAddr  // instance

Physical address of the shared memory

C synopsis target-domain
      ...
    Ptr sharedAddr;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Instance Creation

C synopsis target-domain
GateHWSpinlock_Handle GateHWSpinlock_create(IGateProvider_Handle localGate, const GateHWSpinlock_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GateHWSpinlock_construct(GateHWSpinlock_Struct *structP, IGateProvider_Handle localGate, const GateHWSpinlock_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
Instance Deletion

C synopsis target-domain
Void GateHWSpinlock_delete(GateHWSpinlock_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GateHWSpinlock_destruct(GateHWSpinlock_Struct *structP);
// Finalize the instance object inside the provided structure
Instance Convertors

C synopsis target-domain
IGateMPSupport_Handle GateHWSpinlock_Handle_upCast(GateHWSpinlock_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GateHWSpinlock_Handle GateHWSpinlock_Handle_downCast(IGateMPSupport_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
IGateProvider_Handle GateHWSpinlock_Handle_upCast2(GateHWSpinlock_Handle handle);
// unconditionally move 2 levels up the inheritance hierarchy
 
GateHWSpinlock_Handle GateHWSpinlock_Handle_downCast2(IGateProvider_Handle handle);
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GateHWSpinlock_Object_count();
// The number of statically-created instance objects
 
GateHWSpinlock_Handle GateHWSpinlock_Object_get(GateHWSpinlock_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GateHWSpinlock_Handle GateHWSpinlock_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GateHWSpinlock_Handle GateHWSpinlock_Object_next(GateHWSpinlock_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GateHWSpinlock_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GateHWSpinlock_Handle_label(GateHWSpinlock_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GateHWSpinlock_Handle_name(GateHWSpinlock_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/gates/GateHWSpinlock.xdc
var GateHWSpinlock = xdc.useModule('ti.sdo.ipc.gates.GateHWSpinlock');
module-wide constants & types
module-wide config parameters
        msg: "A_invSpinLockNum: Invalid hardware spinlock number"
    };
        mask: Diags.USER1,
        msg: "LM_close: Gate (lockNum = %d) closed"
    };
        mask: Diags.USER1,
        msg: "LM_create: Gate (lockNum = %d) created"
    };
        mask: Diags.USER1,
        msg: "LM_delete: Gate (lockNum = %d) deleted"
    };
        mask: Diags.USER1,
        msg: "LM_enter: Gate (lockNum = %d) entered, returning key = %d"
    };
        mask: Diags.USER1,
        msg: "LM_leave: Gate (lockNum = %d) left using key = %d"
    };
        mask: Diags.USER1,
        msg: "LM_open: Remote gate (lockNum = %d) opened"
    };
 
module-wide functions
per-instance config parameters
    var params = new GateHWSpinlock.Params// Instance config-params object;
        params.resourceId// Logical resource id = UInt 0;
        params.sharedAddr// Physical address of the shared memory = Ptr null;
per-instance creation
    var inst = GateHWSpinlock.create// Create an instance-object(IGateProvider.Handle localGate, params);
 
 
const GateHWSpinlock.Q_BLOCKING

Blocking quality

XDCscript usage meta-domain
const GateHWSpinlock.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GateHWSpinlock.Q_PREEMPTING

Preempting quality

XDCscript usage meta-domain
const GateHWSpinlock.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
config GateHWSpinlock.A_invSpinLockNum  // module-wide

Assert raised when provided lockNum is invalid for the relevant device

XDCscript usage meta-domain
GateHWSpinlock.A_invSpinLockNum = Assert.Desc {
    msg: "A_invSpinLockNum: Invalid hardware spinlock number"
};
 
C SYNOPSIS
 
config GateHWSpinlock.LM_close  // module-wide

Logged on gate close

XDCscript usage meta-domain
GateHWSpinlock.LM_close = Log.EventDesc {
    mask: Diags.USER1,
    msg: "LM_close: Gate (lockNum = %d) closed"
};
 
C SYNOPSIS
 
config GateHWSpinlock.LM_create  // module-wide

Logged on gate create

XDCscript usage meta-domain
GateHWSpinlock.LM_create = Log.EventDesc {
    mask: Diags.USER1,
    msg: "LM_create: Gate (lockNum = %d) created"
};
 
C SYNOPSIS
 
config GateHWSpinlock.LM_delete  // module-wide

Logged on gate deletion

XDCscript usage meta-domain
GateHWSpinlock.LM_delete = Log.EventDesc {
    mask: Diags.USER1,
    msg: "LM_delete: Gate (lockNum = %d) deleted"
};
 
C SYNOPSIS
 
config GateHWSpinlock.LM_enter  // module-wide

Logged on gate enter

XDCscript usage meta-domain
GateHWSpinlock.LM_enter = Log.EventDesc {
    mask: Diags.USER1,
    msg: "LM_enter: Gate (lockNum = %d) entered, returning key = %d"
};
 
C SYNOPSIS
 
config GateHWSpinlock.LM_leave  // module-wide

Logged on gate leave

XDCscript usage meta-domain
GateHWSpinlock.LM_leave = Log.EventDesc {
    mask: Diags.USER1,
    msg: "LM_leave: Gate (lockNum = %d) left using key = %d"
};
 
C SYNOPSIS
 
config GateHWSpinlock.LM_open  // module-wide

Logged on gate open

XDCscript usage meta-domain
GateHWSpinlock.LM_open = Log.EventDesc {
    mask: Diags.USER1,
    msg: "LM_open: Remote gate (lockNum = %d) opened"
};
 
C SYNOPSIS
 
config GateHWSpinlock.baseAddr  // module-wide

Device-specific base address for HW Semaphore subsystem

XDCscript usage meta-domain
GateHWSpinlock.baseAddr = Ptr null;
 
C SYNOPSIS
 
metaonly config GateHWSpinlock.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
GateHWSpinlock.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GateHWSpinlock.getNumResources()  // module-wide

Returns the number of resources offered by the GateMP delegate

XDCscript usage meta-domain
GateHWSpinlock.getNumResources() returns UInt
 
 
metaonly GateHWSpinlock.queryMeta()  // module-wide

Configuration time test for a particular gate quality

XDCscript usage meta-domain
GateHWSpinlock.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
metaonly GateHWSpinlock.setReserved()  // module-wide

Reserve a HW spinlock for use outside of IPC

XDCscript usage meta-domain
GateHWSpinlock.setReserved(UInt lockNum) returns Void
 
ARGUMENTS
lockNum — HW spinlock number to reserve
DETAILS
GateMP will, by default, manage all HW spinlocks on the device unless this API is used to set aside specific spinlocks for use outside of IPC.
Instance Config Parameters

XDCscript usage meta-domain
var params = new GateHWSpinlock.Params;
// Instance config-params object
    params.resourceId = UInt 0;
    // Logical resource id
    params.sharedAddr = Ptr null;
    // Physical address of the shared memory
 
config GateHWSpinlock.resourceId  // instance

Logical resource id

XDCscript usage meta-domain
var params = new GateHWSpinlock.Params;
  ...
params.resourceId = UInt 0;
 
C SYNOPSIS
 
config GateHWSpinlock.sharedAddr  // instance

Physical address of the shared memory

XDCscript usage meta-domain
var params = new GateHWSpinlock.Params;
  ...
params.sharedAddr = Ptr null;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Instance Creation

XDCscript usage meta-domain
var params = new GateHWSpinlock.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GateHWSpinlock.create(IGateProvider.Handle localGate, params);
// Create an instance-object
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
generated on Tue, 22 May 2012 23:44:53 GMT