![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters. More...
#include <ividenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDM1_SingleBufDesc | data |
XDM_AlgBufInfo | bufInfo |
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDENC1_Fxns::control()
XDAS_Int32 IVIDENC1_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC1_Status::extendedError |
Extended error information.
XDM1_SingleBufDesc IVIDENC1_Status::data |
Buffer descriptor for data passing.
@remarks If this field is not used, the application <b>must</b> set @c data.buf to NULL. @remarks This buffer can be used as either input or output, depending on the command. @remarks The buffer will be provided by the application, and returned to the application upon return of the IVIDENC1_Fxns.control() call. The algorithm must not retain a pointer to this data. @sa #XDM_GETVERSION
XDM_AlgBufInfo IVIDENC1_Status::bufInfo |
Input and output buffer information.
@remarks This field provides the application with the algorithm's buffer requirements. The requirements may vary depending on the current configuration of the algorithm instance. @remarks When configured to generate reconstruction buffers (see IVIDENC1_Params::reconChromaFormat), the recontruction buffer information will also be reported here. @sa IVIDENC1_Params @sa XDM_AlgBufInfo @sa IVIDENC1_Fxns::process()