![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Data Structures | |
struct | IVIDENC1_Obj |
This must be the first field of all IVIDENC1 instance objects. More... | |
struct | IVIDENC1_Params |
Defines the creation time parameters for all IVIDENC1 instance objects. More... | |
struct | IVIDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
struct | IVIDENC1_InArgs |
Defines the input arguments for all IVIDENC1 instance process function. More... | |
struct | IVIDENC1_Status |
Defines instance status parameters. More... | |
struct | IVIDENC1_OutArgs |
Defines the run time output arguments for all IVIDENC1 instance objects. More... | |
struct | IVIDENC1_MbData |
Defines the structure that contains macroblock related encoding parameter estimates. More... | |
struct | IVIDENC1_Fxns |
Defines all of the operations on IVIDENC1 objects. More... |
Macros | |
#define | IVIDENC1_EOK XDM_EOK |
| |
#define | IVIDENC1_EFAIL XDM_EFAIL |
| |
#define | IVIDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
|
Typedefs | |
typedef struct IVIDENC1_Obj | IVIDENC1_Obj |
This must be the first field of all IVIDENC1 instance objects. | |
typedef struct IVIDENC1_Obj * | IVIDENC1_Handle |
Opaque handle to an IVIDENC1 objects. | |
typedef struct IVIDENC1_Params | IVIDENC1_Params |
Defines the creation time parameters for all IVIDENC1 instance objects. | |
typedef struct IVIDENC1_DynamicParams | IVIDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. | |
typedef struct IVIDENC1_InArgs | IVIDENC1_InArgs |
Defines the input arguments for all IVIDENC1 instance process function. | |
typedef struct IVIDENC1_Status | IVIDENC1_Status |
Defines instance status parameters. | |
typedef struct IVIDENC1_OutArgs | IVIDENC1_OutArgs |
Defines the run time output arguments for all IVIDENC1 instance objects. | |
typedef IALG_Cmd | IVIDENC1_Cmd |
Defines the control commands for the IVIDENC1 module. | |
typedef struct IVIDENC1_MbData | IVIDENC1_MbData |
Defines the structure that contains macroblock related encoding parameter estimates. | |
typedef struct IVIDENC1_Fxns | IVIDENC1_Fxns |
Defines all of the operations on IVIDENC1 objects. |
This is the XDM IVIDENC1 Video Encoder Interface.
#define IVIDENC1_EOK XDM_EOK |
Success.
#define IVIDENC1_EFAIL XDM_EFAIL |
General failure.
#define IVIDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
typedef struct IVIDENC1_Obj IVIDENC1_Obj |
This must be the first field of all IVIDENC1 instance objects.
typedef struct IVIDENC1_Obj* IVIDENC1_Handle |
Opaque handle to an IVIDENC1 objects.
typedef struct IVIDENC1_Params IVIDENC1_Params |
Defines the creation time parameters for all IVIDENC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. typedef struct IVIDENC1_DynamicParams IVIDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
@remarks It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDENC1_Fxns::control()
typedef struct IVIDENC1_InArgs IVIDENC1_InArgs |
Defines the input arguments for all IVIDENC1 instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDENC1_Fxns::process()
typedef struct IVIDENC1_Status IVIDENC1_Status |
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDENC1_Fxns::control()
typedef struct IVIDENC1_OutArgs IVIDENC1_OutArgs |
Defines the run time output arguments for all IVIDENC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDENC1_Fxns::process()
typedef IALG_Cmd IVIDENC1_Cmd |
Defines the control commands for the IVIDENC1 module.
typedef struct IVIDENC1_MbData IVIDENC1_MbData |
Defines the structure that contains macroblock related encoding parameter estimates.
inBufs
parameter to IVIDENC1_Fxns::process() when IVIDENC1_DynamicParams::mbDataFlag is set.typedef struct IVIDENC1_Fxns IVIDENC1_Fxns |
Defines all of the operations on IVIDENC1 objects.