![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <ividdec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | decodeHeader |
Decode entire access unit or only header. | |
XDAS_Int32 | displayWidth |
XDAS_Int32 | frameSkipMode |
Video frame skip features for video decoder. | |
XDAS_Int32 | frameOrder |
Video decoder output frame order. | |
XDAS_Int32 | newFrameFlag |
XDAS_Int32 | mbDataFlag |
This structure defines the codec parameters that can be modified after creation via control() calls.
@remarks It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDDEC1_Fxns::control()
XDAS_Int32 IVIDDEC1_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC1_DynamicParams::decodeHeader |
Decode entire access unit or only header.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa XDM_DecMode
XDAS_Int32 IVIDDEC1_DynamicParams::displayWidth |
Pitch. If set to zero, use the decoded image width. Else, use given display width in pixels.
XDAS_Int32 IVIDDEC1_DynamicParams::frameSkipMode |
Video frame skip features for video decoder.
@remarks This enumeration data type should not be used for storage, but rather only for its constant values. @remarks This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between #XDM_CUSTOMENUMBASE and 0x7FFF.
@sa IVIDEO_FrameSkip
XDAS_Int32 IVIDDEC1_DynamicParams::frameOrder |
Video decoder output frame order.
@sa IVIDDEC1_FrameOrder
XDAS_Int32 IVIDDEC1_DynamicParams::newFrameFlag |
Flag to indicate that the algorithm should start a new frame.
XDAS_Int32 IVIDDEC1_DynamicParams::mbDataFlag |
Flag to indicate that the algorithm should generate MB Data in addition to decoding the data.