![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
IVIDANALYTICS_Grid * | grid |
XDM_Date | date |
IVIDANALYTICS_Rule | rule |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
@remarks It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IVIDANALYTICS_Fxns::control()
XDAS_Int32 IVIDANALYTICS_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
IVIDANALYTICS_Grid* IVIDANALYTICS_DynamicParams::grid |
New overlay grid with analytics enable mask
XDM_Date IVIDANALYTICS_DynamicParams::date |
Set the current time.
IVIDANALYTICS_Rule IVIDANALYTICS_DynamicParams::rule |
Rule associated with this command (if applicable).