![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters. More...
#include <isphdec1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | postFilter |
XDAS_Int32 | extendedError |
Extended error information. | |
XDM1_SingleBufDesc | data |
XDAS_Int16 | compandingLaw |
XDAS_Int16 | packingType |
XDM_AlgBufInfo | bufInfo |
XDAS_Int16 | codecSelection |
XDAS_Int16 | bitRate |
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa ISPHDEC1_Fxns::control()
XDAS_Int16 ISPHDEC1_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int16 ISPHDEC1_Status::postFilter |
Provides the current postFilter setting.
@sa ISPEECH1_PostFilter
XDAS_Int32 ISPHDEC1_Status::extendedError |
Extended error information.
XDM1_SingleBufDesc ISPHDEC1_Status::data |
Buffer descriptor for data passing.
@remarks If this field is not used, the application <b>must</b> set @c data.buf to NULL. @remarks This buffer can be used as either input or output, depending on the command. @remarks The buffer will be provided by the application, and returned to the application upon return of the ISPHDEC1_Fxns.control() call. The algorithm must not retain a pointer to this data. @sa #XDM_GETVERSION
XDAS_Int16 ISPHDEC1_Status::compandingLaw |
Optional, codec-specific companding law. See your codec-specific interface documentation options.
XDAS_Int16 ISPHDEC1_Status::packingType |
Optional, codec-specific packing type. See your codec-specific interface documentation options.
XDM_AlgBufInfo ISPHDEC1_Status::bufInfo |
Input and output buffer information.
@sa XDM_AlgBufInfo
XDAS_Int16 ISPHDEC1_Status::codecSelection |
Optional, codec-specific codec selection. See your codec-specific interface documentation options.
XDAS_Int16 ISPHDEC1_Status::bitRate |
Optional, codec-specific bit rate. See your codec-specific interface documentation options.