![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Enumerations | |
enum | ISPEECH1_G723_BitRate { ISPEECH1_G723_BITRATE_5P3 = 0, ISPEECH1_G723_BITRATE_6P3 = 1, ISPEECH1_G723_BITRATE_DEFAULT = ISPEECH1_G723_BITRATE_6P3 } |
Bit rate selection for G723. More... | |
enum | ISPEECH1_G723_NoisePreProc { ISPEECH1_G723_NOISEPREPROC_OFF = 0, ISPEECH1_G723_NOISEPREPROC_ON = 1, ISPEECH1_G723_NOISEPREPROC_DEFAULT = ISPEECH1_G723_NOISEPREPROC_ON } |
Enable/disable high pass filter for G723. More... |
This is the XDM speech interface shared between the various G.723 codecs.