![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
This header defines all types, constants, and functions shared by all implementations of the "universal" XDM algorithm.
Go to the source code of this file.
Data Structures | |
struct | IUNIVERSAL_Obj |
This must be the first field of all IUNIVERSAL instance objects. More... | |
struct | IUNIVERSAL_Params |
Defines the creation time parameters for all IUNIVERSAL instance objects. More... | |
struct | IUNIVERSAL_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. More... | |
struct | IUNIVERSAL_InArgs |
Defines the input arguments for all IUNIVERSAL instance process function. More... | |
struct | IUNIVERSAL_Status |
Defines instance status parameters (read-only). More... | |
struct | IUNIVERSAL_OutArgs |
Defines the run time output arguments for all IUNIVERSAL instance objects. More... | |
struct | IUNIVERSAL_Fxns |
Defines all of the operations on IUNIVERSAL objects. More... |
Macros | |
#define | IUNIVERSAL_EOK XDM_EOK |
| |
#define | IUNIVERSAL_EFAIL XDM_EFAIL |
| |
#define | IUNIVERSAL_EUNSUPPORTED XDM_EUNSUPPORTED |
|
Typedefs | |
typedef struct IUNIVERSAL_Obj | IUNIVERSAL_Obj |
This must be the first field of all IUNIVERSAL instance objects. | |
typedef struct IUNIVERSAL_Obj * | IUNIVERSAL_Handle |
Opaque handle to an IUNIVERSAL objects. | |
typedef struct IUNIVERSAL_Params | IUNIVERSAL_Params |
Defines the creation time parameters for all IUNIVERSAL instance objects. | |
typedef struct IUNIVERSAL_DynamicParams | IUNIVERSAL_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. | |
typedef struct IUNIVERSAL_InArgs | IUNIVERSAL_InArgs |
Defines the input arguments for all IUNIVERSAL instance process function. | |
typedef struct IUNIVERSAL_Status | IUNIVERSAL_Status |
Defines instance status parameters (read-only). | |
typedef struct IUNIVERSAL_OutArgs | IUNIVERSAL_OutArgs |
Defines the run time output arguments for all IUNIVERSAL instance objects. | |
typedef IALG_Cmd | IUNIVERSAL_Cmd |
Defines the control commands for the IUNIVERSAL module. | |
typedef struct IUNIVERSAL_Fxns | IUNIVERSAL_Fxns |
Defines all of the operations on IUNIVERSAL objects. |