![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters (read-only). More...
#include <iuniversal.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDM1_BufDesc | data |
Defines instance status parameters (read-only).
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IUNIVERSAL_Fxns::control()
XDAS_Int32 IUNIVERSAL_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IUNIVERSAL_Status::extendedError |
Extended error information.
XDM1_BufDesc IUNIVERSAL_Status::data |
Buffer descriptor for data passing.
@remarks These buffers can be used as either input, output, or input/output buffers, depending on the command. @remarks The buffers will be provided by the application, and returned to the application upon return of the control() call. The algorithm must not retain a pointer to this data. @sa #XDM_GETVERSION