Data Structures | Defines | Typedefs

ISPHENC - XDM Speech Encoder Interface

Data Structures

struct  ISPHENC_Obj
 This must be the first field of all ISPHENC instance objects. More...
struct  ISPHENC_Params
 Defines the creation time parameters for all ISPHENC instance objects. More...
struct  ISPHENC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  ISPHENC_InArgs
 Defines the input arguments for all ISPHENC instance process function. More...
struct  ISPHENC_Status
 Defines instance status parameters (read-only). More...
struct  ISPHENC_OutArgs
 Defines the run time output arguments for all ISPHENC instance objects. More...
struct  ISPHENC_Fxns
 Defines all of the operations on ISPHENC objects. More...

Defines

#define ISPHENC_CID   "ti.xdais.dm.ISPHENC"
#define ISPHENC_ERUNTIME   XDM_ERUNTIME
#define ISPHENC_EOK   XDM_EOK
#define ISPHENC_EFAIL   XDM_EFAIL

Typedefs

typedef struct ISPHENC_Obj ISPHENC_Obj
 This must be the first field of all ISPHENC instance objects.
typedef struct ISPHENC_ObjISPHENC_Handle
 Opaque handle to an ISPHENC objects.
typedef struct ISPHENC_Params ISPHENC_Params
 Defines the creation time parameters for all ISPHENC instance objects.
typedef struct
ISPHENC_DynamicParams 
ISPHENC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct ISPHENC_InArgs ISPHENC_InArgs
 Defines the input arguments for all ISPHENC instance process function.
typedef struct ISPHENC_Status ISPHENC_Status
 Defines instance status parameters (read-only).
typedef struct ISPHENC_OutArgs ISPHENC_OutArgs
 Defines the run time output arguments for all ISPHENC instance objects.
typedef IALG_Cmd ISPHENC_Cmd
 Defines the control commands for the ISPHENC module.
typedef struct ISPHENC_Fxns ISPHENC_Fxns
 Defines all of the operations on ISPHENC objects.

Detailed Description

This is the XDM ISPHENC Speech/Voice Encoder Interface.

Deprecated:
This XDM speech encoder interface has been deprecated, and superceeded by newer ISPHENCx speech encoder interfaces.

Define Documentation

#define ISPHENC_CID   "ti.xdais.dm.ISPHENC"

ISPHENC Class ID

#define ISPHENC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define ISPHENC_EOK   XDM_EOK

Success.

#define ISPHENC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct ISPHENC_Obj ISPHENC_Obj

This must be the first field of all ISPHENC instance objects.

typedef struct ISPHENC_Obj* ISPHENC_Handle

Opaque handle to an ISPHENC objects.

Defines the creation time parameters for all ISPHENC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
ISPHENC_Fxns::control()

Defines the input arguments for all ISPHENC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
ISPHENC_Fxns::process()

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
ISPHENC_Fxns::control()

Defines the run time output arguments for all ISPHENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
ISPHENC_Fxns::process()

Defines the control commands for the ISPHENC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
ISPHENC_Fxns::control()
typedef struct ISPHENC_Fxns ISPHENC_Fxns

Defines all of the operations on ISPHENC objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated