![]() |
![]() |
This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <isphenc.h>
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Input frame size in bytes for sample based codecs.
Rate selection for multi_rate codecs
Mode selection for multi_mode codecs
VAD_On =1, VAD_OFF = 0
0 - OFF, 1 = NS-A, 2 = NS-B etc
0 = TTY OFF, 1 = 45.45bauds 2 = 50 bauds
0 = DTMF_OFF, 1 = DTMF_ON
1 = ON, 0 = OFF
0 - DISABLED; 1 - ENABLED