2.6.3. Generic Compiler Pre-Defined Macro Symbols

Table 2.8 Version-Related Predefined Macro Symbols

Symbol

Value Kind

Value / Description

__clang__

<constant>

Defined to 1 if compiler uses Clang-based front-end.

__clang_major__

<version>

Identifies major version number of Clang front-end.

__clang_minor__

<version>

Identifies minor version number of Clang front-end.

__clang_patchlevel__

<version>

Identifies patch number of Clang front-end.

__clang_version__

<string>

String representation of Clang front-end version identification.

__GNUC_MINOR__

<version>

2

__GNUC_PATCHLEVEL__

<version>

1

__GNUC__

<version>

4

__GXX_ABI_VERSION__

<version>

1002

__llvm__

<constant>

Defined to 1 if compiler uses LLVM back-end.

__VERSION__

<string>

Full string representation of Clang front-end version identification.

Table 2.9 C Language-Related Predefined Macro Symbols

Symbol

Value Kind

Value / Description

__GNUC_GNU_INLINE__

<constant>

Defined to 1 if functions declared inline are defined and externally visible in compiler generated object files if such functions are not declared static or extern.

__GNUC_STDC_INLINE__

<constant>

Defined to 1 if functions declared inline are defined and externally visible in compiler generated object files only if such functions are declared extern.

__STDC__

<constant>

Defined to 1 if the compiler conforms to ISO Standard C.

__STDC_HOSTED__

<constant>

Defined to 1 if the target of the compiler is a hosted environment in which the compiler package supplies standard C runtime libraries.

__STDC_UTF_16__

<constant>

Defined to 1 if char16_t type values are UTF-16 encoded.

__STDC_UTF_32__

<constant>

Defined to 1 if char32_t type values are UTF-32 encoded.

__STDC_VERSION__

<version>

Defined to the C Standard being applied for a given compilation based on the -std=<language> option. By default, tiarmclang assumes -std=gnu17 for C source files (<version>=201710L). *

__STRICT_ANSI__

<constant>

Defined to 1 if a strictly-conforming C language variant is specified as the argument to the -std option (c89/90/99/9x/11/1x/17/18).

  • See Pre-defined Compiler Macros for a list of definitions of __STDC_VERSION__ that correspond to versions of the C language standards.

Table 2.10 C++ Language Standard Predefined Macro Symbol (__cplusplus)

Symbol

Value Kind

Value / Description

__cplusplus

<standard>

Indicates the C++ <standard> that is in effect for a given compilation, where <standard> is one of the following values:

value   => C++ Standard
-------    ------------
199711L    C++98
199711L    C++03
201103L    C++11
201402L    C++14
201703L    C++17
Table 2.11 C++ Language Feature Test Predefined Macro Symbols

Symbol / Feature

Available

Value / Adoption

__cpp_aggregate_bases

C++17

201603L

__cpp_aggregate_nsdmi

C++14

201304L

__cpp_alias_templates

C++11

200704L

__cpp_aligned_new

C++17

201606L

__cpp_attributes

C++11

200809L

__cpp_binary_literals

C++14

201304L

__cpp_capture_star_this

C++17

201603L

__cpp_constexpr

C++11 / C++14 / C++17

200704L / 201304L / 201603L

__cpp_contexpr_in_decltype

C++11

201711L

__cpp_decltype

C++11

200707L

__cpp_decltype_auto

C++14

201304L

__cpp_deduction_guides

C++17

201703L

__cpp_delegating_constructors

C++11

200604L

__cpp_digit_separators

C++14

201309L

__cpp_enumerator_attributes

C++17

201411L

__cpp_fold_expressions

C++17

201603L

__cpp_generic_lambdas

C++14

201304L

__cpp_guaranteed_copy_elision

C++17

201606L

__cpp_hex_float

C++17

201603L

__cpp_if_constexpr

C++17

201606L

__cpp_impl_destroying_delete

C++98

201806L

__cpp_inheriting_constructors

C++11

201511L

__cpp_init_captures

C++14

201304L

__cpp_initializer_lists

C++11

200806L

__cpp_inline_variables

C++17

201606L

__cpp_lambdas

C++11

200907L

__cpp_namespace_attributes

C++17

201411L

__cpp_nested_namespace_definitions

C++17

201411L

__cpp_noexcept_function_type

C++17

201510L

__cpp_nontype_template_args

C++17

201411L

__cpp_nontype_template_parameter_auto

C++17

201606L

__cpp_nsdmi

C++11

200809L

__cpp_range_based_for

C++11 / C++17

200907L / 201603L

__cpp_raw_strings

C++11

200710L

__cpp_ref_qualifiers

C++11

200710L

__cpp_return_type_deduction

C++14

201304L

__cpp_rvalue_references

C++11

200610L

__cpp_static_assert

C++11 / C++17

200410L / 201411L

__cpp_structured_bindings

C++17

201606L

__cpp_template_auto

C++17

201606L

__cpp_threadsafe_static_init

C++98

200806L

__cpp_unicode_characters

C++11

200704L

__cpp_unicode_literals

C++11

200710L

__cpp_user_defined_literals

C++11

200809L

__cpp_variable_templates

C++14

201304L

__cpp_variadic_templates

C++11

200704L

__cpp_variadic_using

C++17

201611L

Table 2.12 Compiler Generated Object Format (__ELF__)

Symbol

Value Kind

Value / Description

__ELF__

<constant>

Defined to 1 if compiler generates object code that conforms to the ELF object file format (default).

Table 2.14 Predefined Macro Symbols Related to Endian-ness

Symbol

Value Kind

Value / Description

__BIG_ENDIAN__

<constant>

Defined to 1 if compiler has been instructed to generate big-endian object code.

__LITTLE_ENDIAN__

<constant>

Defined to 1 if compiler has been instructed to generate little-endian object code (default).

__BYTE_ORDER__

<constant>

Matches either __ORDER_BIG_ENDIAN__ (4321) or __ORDER_LITTLE_ENDIAN__ (1234) depending on the endian-ness assumed for a given compilation.

__ORDER_BIG_ENDIAN__

<constant>

4321

__ORDER_LITTLE_ENDIAN__

<constant>

1234

Table 2.15 Predefined Macro Symbols Related to Optimization

Symbol

Value Kind

Value / Description

__FAST_MATH__

<constant>

Defined to 1 if the -ffast-math or -ffp-mode=fast option is enabled (-ffast-math is implied when the deprecated -Ofast optimization level is specified on the compiler command-line).

_INLINE

<constant>

Defined to 1 if automatic inlining optimizations are enabled.

__NO_INLINE__

<constant>

Defined to 1 if automatic inlining optimizations are disabled.

__OPTIMIZE__

<constant>

Defined to 1 if optimization is in use (-O[123szg]).

__OPTIMIZE_SIZE__

<constant>

Defined to 1 if optimizations intended to reduce compiler- generated code size are in use (-Os or -Oz option).

Table 2.17 Predefined Macro Symbols Related to Scalar Types

Symbol

Value Kind

Value / Description

__BIGGEST_ALIGNMENT__

<bytes>

Indicates the largest alignment in <bytes> ever used for any data type on the Arm processor being compiled for. For Cortex-M0/M0+/ M3/M4/M33/R4/R5, <bytes> = 8.

__CHAR16_TYPE__

<type>

unsigned short

__CHAR32_TYPE__

<type>

unsigned int

__CHAR_BIT__

<bits>

8

__CHAR_UNSIGNED__

<constant>

Defined to 1 if “plain” char types (not qualified with a “signed” or “unsigned” keyword) are interpreted by the compiler to be unsigned.

__INT8_FMTd__

<string>

“hhd”

__INT8_FMTi__

<string>

“hhi”

__INT8_MAX__

<constant>

127

__INT8_TYPE__

<type>

signed char

__UINT8_FMTX__

<string>

“hhX”

__UINT8_FMTo__

<string>

“hho”

__UINT8_FMTu__

<string>

“hhu”

__UINT8_FMTx__

<string>

“hhx”

__UINT8_MAX__

<constant>

255

__UINT8_TYPE__

<type>

unsigned char

__SCHAR_MAX__

<constant>

127

__INT_FAST8_FMTd__

<string>

“hhd”

__INT_FAST8_FMTi__

<string>

“hhi”

__INT_FAST8_MAX__

<constant>

127

__INT_FAST8_TYPE__

<type>

signed char

__UINT_FAST8_FMTX__

<string>

“hhX”

__UINT_FAST8_FMTo__

<string>

“hho”

__UINT_FAST8_FMTu__

<string>

“hhu”

__UINT_FAST8_FMTx__

<string>

“hhx”

__UINT_FAST8_MAX__

<constant>

255

__UINT_FAST8_TYPE__

<type>

unsigned char

__INT_LEAST8_FMTd__

<string>

“hhd”

__INT_LEAST8_FMTi__

<string>

“hhi”

__INT_LEAST8_MAX__

<constant>

127

__INT_LEAST8_TYPE__

<type>

signed char

__UINT_LEAST8_FMTX__

<string>

“hhX”

__UINT_LEAST8_FMTo__

<string>

“hho”

__UINT_LEAST8_FMTu__

<string>

“hhu”

__UINT_LEAST8_FMTx__

<string>

“hhx”

__UINT_LEAST8_MAX__

<constant>

255

__UINT_LEAST8_TYPE__

<type>

unsigned char

__INT16_FMTd__

<string>

“hd”

__INT16_FMTi__

<string>

“hi”

__INT16_MAX__

<constant>

32767

__INT16_TYPE__

<type>

short

__UINT16_FMTX__

<string>

“hX”

__UINT16_FMTo__

<string>

“ho”

__UINT16_FMTu__

<string>

“hu”

__UINT16_FMTx__

<string>

“hx”

__UINT16_MAX__

<constant>

65535

__UINT16_TYPE__

<type>

unsigned short

__SHRT_MAX__

<constant>

32767

__SIZEOF_SHORT__

<bytes>

4

__INT_FAST16_FMTd__

<string>

“hd”

__INT_FAST16_FMTi__

<string>

“hi”

__INT_FAST16_MAX__

<constant>

32767

__INT_FAST16_TYPE__

<type>

short

__UINT_FAST16_FMTX__

<string>

“hX”

__UINT_FAST16_FMTo__

<string>

“ho”

__UINT_FAST16_FMTu__

<string>

“hu”

__UINT_FAST16_FMTx__

<string>

“hx”

__UINT_FAST16_MAX__

<constant>

65535

__UINT_FAST16_TYPE__

<type>

unsigned short

__INT_LEAST16_FMTd__

<string>

“hd”

__INT_LEAST16_FMTi__

<string>

“hi”

__INT_LEAST16_MAX__

<constant>

32767

__INT_LEAST16_TYPE__

<type>

short

__UINT_LEAST16_FMTX__

<string>

“hX”

__UINT_LEAST16_FMTo__

<string>

“ho”

__UINT_LEAST16_FMTu__

<string>

“hu”

__UINT_LEAST16_FMTx__

<string>

“hx”

__UINT_LEAST16_MAX__

<constant>

65535

__UINT_LEAST16_TYPE__

<type>

unsigned short

__INT32_FMTd__

<string>

“d”

__INT32_FMTi__

<string>

“i”

__INT32_MAX__

<constant>

2147483647

__INT32_TYPE__

<type>

int

__UINT32_C_SUFFIX__

<text>

U

__UINT32_FMTX__

<string>

“X”

__UINT32_FMTo__

<string>

“o”

__UINT32_FMTu__

<string>

“u”

__UINT32_FMTx__

<string>

“x”

__UINT32_MAX__

<constant>

4294967295U

__UINT32_TYPE__

<type>

unsigned int

__INT_MAX__

<constant>

2147483647

__SIZEOF_INT__

<bytes>

4

__LONG_MAX__

<constant>

2147483647

__SIZEOF_LONG__

<bytes>

4

__INT_FAST32_FMTd__

<string>

“d”

__INT_FAST32_FMTi__

<string>

“i”

__INT_FAST32_MAX__

<constant>

2147483647

__INT_FAST32_TYPE__

<type>

int

__UINT_FAST32_FMTX__

<string>

“X”

__UINT_FAST32_FMTo__

<string>

“o”

__UINT_FAST32_FMTu__

<string>

“u”

__UINT_FAST32_FMTx__

<string>

“x”

__UINT_FAST32_MAX__

<constant>

4294967295U

__UINT32_TYPE__

<type>

unsigned int

__INT_LEAST32_FMTd__

<string>

“d”

__INT_LEAST32_FMTi__

<string>

“i”

__INT_LEAST32_MAX__

<constant>

2147483647

__INT_LEAST32_TYPE__

<type>

int

__UINT_LEAST32_FMTX__

<string>

“X”

__UINT_LEAST32_FMTo__

<string>

“o”

__UINT_LEAST32_FMTu__

<string>

“u”

__UINT_LEAST32_FMTx__

<string>

“x”

__UINT_LEAST32_MAX__

<constant>

4294967295U

__UINT_LEAST32_TYPE__

<type>

unsigned int

__INT64_C_SUFFIX__

<text>

LL

__INT64_FMTd__

<string>

“lld”

__INT64_FMTi__

<string>

“lli”

__INT64_MAX__

<constant>

9223372036854775807LL

__INT64_TYPE__

<type>

long long int

__UINT64_C_SUFFIX__

<text>

ULL

__UINT64_FMTX__

<string>

“llX”

__UINT64_FMTo__

<string>

“llo”

__UINT64_FMTu__

<string>

“llu”

__UINT64_FMTx__

<string>

“llx”

__UINT64_MAX__

<constant>

18446744073709551615ULL

__UINT64_TYPE__

<type>

long long unsigned int

__UINT8_TYPE__

<type>

unsigned char

__SCHAR_MAX__

<constant>

127

__INT_FAST8_FMTd__

<string>

“hhd”

__INT_FAST8_FMTi__

<string>

“hhi”

__INT_FAST8_MAX__

<constant>

127

__INT_FAST8_TYPE__

<type>

signed char

__UINT8_FMTX__

<string>

“hhX”

__UINT8_FMTo__

<string>

“hho”

__UINT8_FMTu__

<string>

“hhu”

__UINT8_FMTx__

<string>

“hhx”

__UINT8_MAX__

<constant>

255

__UINT8_TYPE__

<type>

unsigned char

__SCHAR_MAX__

<constant>

127

__INT_FAST8_FMTd__

<string>

“hhd”

__INT_FAST8_FMTi__

<string>

“hhi”

__INT_FAST8_MAX__

<constant>

127

__INT_FAST8_TYPE__

<type>

signed char

__UINT_FAST8_FMTX__

<string>

“hhX”

__UINT_FAST8_FMTo__

<string>

“hho”

__UINT_FAST8_FMTu__

<string>

“hhu”

__UINT_FAST8_FMTx__

<string>

“hhx”

__UINT_FAST8_MAX__

<constant>

255

__UINT_FAST8_TYPE__

<type>

unsigned char

__INT_LEAST8_FMTd__

<string>

“hhd”

__INT_LEAST8_FMTi__

<string>

“hhi”

__INT_LEAST8_MAX__

<constant>

127

__INT_LEAST8_TYPE__

<type>

signed char

__UINT_LEAST8_FMTX__

<string>

“hhX”

__UINT_LEAST8_FMTo__

<string>

“hho”

__UINT_LEAST8_FMTu__

<string>

“hhu”

__UINT_LEAST8_FMTx__

<string>

“hhx”

__UINT_LEAST8_MAX__

<constant>

255

__UINT_LEAST8_TYPE__

<type>

unsigned char

__INT16_FMTd__

<string>

“hd”

__INT16_FMTi__

<string>

“hi”

__INT16_MAX__

<constant>

32767

__INT16_TYPE__

<type>

short

__UINT16_FMTX__

<string>

“hX”

__UINT16_FMTo__

<string>

“ho”

__UINT16_FMTu__

<string>

“hu”

__UINT16_FMTx__

<string>

“hx”

__UINT16_MAX__

<constant>

65535

__UINT16_TYPE__

<type>

unsigned short

__SHRT_MAX__

<constant>

32767

__SIZEOF_SHORT__

<bytes>

4

__INT_FAST16_FMTd__

<string>

“hd”

__INT_FAST16_FMTi__

<string>

“hi”

__INT_FAST16_MAX__

<constant>

32767

__INT_FAST16_TYPE__

<type>

short

__UINT_FAST16_FMTX__

<string>

“hX”

__UINT_FAST16_FMTo__

<string>

“ho”

__UINT_FAST16_FMTu__

<string>

“hu”

__UINT_FAST16_FMTx__

<string>

“hx”

__UINT_FAST16_MAX__

<constant>

65535

__UINT_FAST16_TYPE__

<type>

unsigned short

__INT_LEAST16_FMTd__

<string>

“hd”

__INT_LEAST16_FMTi__

<string>

“hi”

__INT_LEAST16_MAX__

<constant>

32767

__INT_LEAST16_TYPE__

<type>

short

__UINT_LEAST16_FMTX__

<string>

“hX”

__UINT_LEAST16_FMTo__

<string>

“ho”

__UINT_LEAST16_FMTu__

<string>

“hu”

__UINT_LEAST16_FMTx__

<string>

“hx”

__UINT_LEAST16_MAX__

<constant>

65535

__UINT_LEAST16_TYPE__

<type>

unsigned short

__INT32_FMTd__

<string>

“d”

__INT32_FMTi__

<string>

“i”

__INT32_MAX__

<constant>

2147483647

__INT32_TYPE__

<type>

int

__UINT32_C_SUFFIX__

<text>

U

__UINT32_FMTX__

<string>

“X”

__UINT32_FMTo__

<string>

“o”

__UINT32_FMTu__

<string>

“u”

__UINT32_FMTx__

<string>

“x”

__UINT32_MAX__

<constant>

4294967295U

__UINT32_TYPE__

<type>

unsigned int

__INT_MAX__

<constant>

2147483647

__SIZEOF_INT__

<bytes>

4

__LONG_MAX__

<constant>

2147483647

__SIZEOF_LONG__

<bytes>

4

__INT_FAST32_FMTd__

<string>

“d”

__INT_FAST32_FMTi__

<string>

“i”

__INT_FAST32_MAX__

<constant>

2147483647

__INT_FAST32_TYPE__

<type>

int

__UINT_FAST32_FMTX__

<string>

“X”

__UINT_FAST32_FMTo__

<string>

“o”

__UINT_FAST32_FMTu__

<string>

“u”

__UINT_FAST32_FMTx__

<string>

“x”

__UINT_FAST32_MAX__

<constant>

4294967295U

__UINT32_TYPE__

<type>

unsigned int

__INT_LEAST32_FMTd__

<string>

“d”

__INT_LEAST32_FMTi__

<string>

“i”

__INT_LEAST32_MAX__

<constant>

2147483647

__INT_LEAST32_TYPE__

<type>

int

__UINT_LEAST32_FMTX__

<string>

“X”

__UINT_LEAST32_FMTo__

<string>

“o”

__UINT_LEAST32_FMTu__

<string>

“u”

__UINT_LEAST32_FMTx__

<string>

“x”

__UINT_LEAST32_MAX__

<constant>

4294967295U

__UINT_LEAST32_TYPE__

<type>

unsigned int

__INT64_C_SUFFIX__

<text>

LL

__INT64_FMTd__

<string>

“lld”

__INT64_FMTi__

<string>

“lli”

__INT64_MAX__

<constant>

9223372036854775807LL

__INT64_TYPE__

<type>

long long int

__UINT64_C_SUFFIX__

<text>

ULL

__UINT64_FMTX__

<string>

“llX”

__UINT64_FMTo__

<string>

“llo”

__UINT64_FMTu__

<string>

“llu”

__UINT64_FMTx__

<string>

“llx”

__UINT64_MAX__

<constant>

18446744073709551615ULL

__UINT64_TYPE__

<type>

long long unsigned int

__LONG_LONG_MAX__

<constant>

9223372036854775807LL

__SIZEOF_LONG_LONG__

<bytes>

8

__INT_FAST64_FMTd__

<string>

“lld”

__INT_FAST64_FMTi__

<string>

“lli”

__INT_FAST64_MAX__

<constant>

9223372036854775807LL

__INT_FAST64_TYPE__

<type>

long long int

__UINT_FAST64_FMTX__

<string>

“llX”

__UINT_FAST64_FMTo__

<string>

“llo”

__UINT_FAST64_FMTu__

<string>

“llu”

__UINT_FAST64_FMTx__

<string>

“llx”

__UINT_FAST64_MAX__

<constant>

18446744073709551615ULL

__UINT_FAST64_TYPE__

<type>

long long unsigned int

__INT_LEAST64_FMTd__

<string>

“lld”

__INT_LEAST64_FMTi__

<string>

“lli”

__INT_LEAST64_MAX__

<constant>

9223372036854775807LL

__INT_LEAST64_TYPE__

<type>

long long int

__INT_LEAST64_WIDTH__

<constant>

64

__UINT_LEAST64_FMTX__

<string>

“llX”

__UINT_LEAST64_FMTo__

<string>

“llo”

__UINT_LEAST64_FMTu__

<string>

“llu”

__UINT_LEAST64_FMTx__

<string>

“llx”

__UINT_LEAST64_MAX__

<constant>

18446744073709551615ULL

__UINT_LEAST64_TYPE__

<type>

long long unsigned int

__INTMAX_C_SUFFIX__

<text>

LL

__INTMAX_FMTd__

<string>

“lld”

__INTMAX_FMTi__

<string>

“lli”

__INTMAX_MAX__

<constant>

9223372036854775807LL

__INTMAX_TYPE__

<type>

long long int

__INTMAX_WIDTH__

<bits>

64

__UINTMAX_C_SUFFIX__

<text>

ULL

__UINTMAX_FMTX__

<string>

“llX”

__UINTMAX_FMTo__

<string>

“llo”

__UINTMAX_FMTu__

<string>

“llu”

__UINTMAX_FMTx__

<string>

“llx”

__UINTMAX_MAX__

<constant>

18446744073709551615ULL

__UINTMAX_TYPE__

<type>

long long unsigned int

__UINTMAX_WIDTH__

<constant>

64

__INTPTR_FMTd__

<string>

“d”

__INTPTR_FMTi__

<string>

“i”

__INTPTR_MAX__

<constant>

2147483647

__INTPTR_TYPE__

<type>

int

__INTPTR_WIDTH__

<bits>

32

__UINTPTR_FMTX__

<string>

“X”

__UINTPTR_FMTo__

<string>

“o”

__UINTPTR_FMTu__

<string>

“u”

__UINTPTR_FMTx__

<string>

“x”

__UINTPTR_MAX__

<constant>

4294967295U

__UINTPTR_TYPE__

<type>

unsigned int

__UINTPTR_WIDTH__

<constant>

32

__POINTER_WIDTH__

<constant>

32

_ILP32

<constant>

Defined to 1 if pointer type width and long type width is 32-bits.

__ILP32__

<constant>

Defined to 1 if pointer type width and long type width is 32-bits.

__SIZEOF_POINTER__

<bytes>

4

__PTRDIFF_FMTd__

<string>

“d”

__PTRDIFF_FMTi__

<string>

“i”

__PTRDIFF_MAX__

<constant>

2147483647

__PTRDIFF_TYPE__

<type>

int

__PTRDIFF_WIDTH__

<bits>

32

__SIZEOF_PTRDIFF_T__

<bytes>

4

__SIZE_FMTX__

<string>

“X”

__SIZE_FMTo__

<string>

“o”

__SIZE_FMTu__

<string>

“u”

__SIZE_FMTx__

<string>

“X”

__SIZE_MAX__

<constant>

4294967295U

__SIZE_TYPE__

<type>

unsigned int

__SIZE_WIDTH__

<bits>

32

__SIZEOF_SIZE_T__

<bytes>

4

__WCHAR_MAX__

<constant>

2147483647

__WCHAR_TYPE__

<constant>

int

__WCHAR_WIDTH__

<bits>

32

__SIZEOF_WCHAR_T__

<bytes>

4

__WINT_MAX__

<constant>

2147483647

__WINT_TYPE__

<constant>

int

__WINT_WIDTH__

<bits>

32

__SIZEOF_WINT_T__

<bytes>

4

__FLT_DECIMAL_DIG__

<digits>

9

__FLT_DENORM_MIN__

<constant>

1.40129846e-45F

__FLT_DIG__

<digits>

6

__FLT_EPSILON__

<constant>

1.19209290e-7F

__FLT_MANT_DIG__

<bits>

24

__FLT_MAX_10_EXP__

<constant>

38

__FLT_MAX_EXP__

<constant>

128

__FLT_MAX__

<constant>

3.40282347e+38F

__FLT_MIN_10_EXP__

<constant>

-37

__FLT_MIN_EXP__

<constant>

-125

__FLT_MIN__

<constant>

1.17549435e-38F

__FLT_RADIX__

<constant>

2

__SIZEOF_FLOAT__

<bytes>

4

__DBL_DECIMAL_DIG__

<digits>

17

__DBL_DENORM_MIN__

<constant>

4.9406564584124654e-324

__DBL_DIG__

<digits>

15

__DBL_EPSILON__

<constant>

2.2204460492503131e-16

__DBL_MANT_DIG__

<bits>

53

__DBL_MAX_10_EXP__

<constant>

308

__DBL_MAX_EXP__

<constant>

1024

__DBL_MAX__

<constant>

1.7976931348623157e+308

__DBL_MIN_10_EXP__

<constant>

-307

__DBL_MIN_EXP__

<constant>

-1021

__DBL_MIN__

<constant>

2.2250738585072014e-308

__DECIMAL_DIG__

<constant>

__LDBL_DECIMAL_DIG__

__LDBL_DECIMAL_DIG__

<digits>

17

__LDBL_DENORM_MIN__

<constant>

4.9406564584124654e-324

__LDBL_DIG__

<digits>

15

__LDBL_EPSILON__

<constant>

2.2204460492503131e-16

__LDBL_MANT_DIG__

<bits>

53

__LDBL_MAX_10_EXP__

<constant>

308

__LDBL_MAX_EXP__

<constant>

1024

__LDBL_MAX__

<constant>

1.7976931348623157e+308

__LDBL_MIN_10_EXP__

<constant>

-307

__LDBL_MIN_EXP__

<constant>

-1021

__LDBL_MIN__

<constant>

2.2250738585072014e-308