2.9. Intrinsics¶
The ACLE compiler intrinsics are fully documented in the Arm C Language Extensions - Release ACLE Q3 2020. A summary of each of the ACLE compiler intrinsics that are supported by the tiarmclang compiler is provided below. Note that many of the intrinsics documented in the ACLE specification are only available on Arm processors that are not currently supported by tiarmclang.
Note
#include <arm_acle.h>
The <arm_acle.h> header file should be included in your compilation unit before using any of the ACLE intrinsics.
Note
The floating-point ACLE intrinsics __sqrt, __sqrtf, __fma, __fmaf, __rintn, and __rintnf are not supported by the tiarmclang compiler. Use the corresponding standard C math functions instead.
2.9.1. Data-Processing Intrinsics¶
2.9.1.1. Rotate and Bit-Manipulation Intrinsics¶
- __ror, __rorl, __rorll¶
Signatures
uint32_t __ror(uint32_t x, uint32_t y); unsigned long __rorl(unsigned long x, unsigned long y); uint64_t __rorll(uint64_t x, uint64_t y);
Description
Rotate x by y bits; return the result.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __clz, __clzl, __clzll¶
Signatures
unsigned int __clz(uint32_t x); unsigned int __clzl(unsigned long x); unsigned int __clzll(uint64_t x);
Description
Return the number of leading zero bits in x. If x == 0, then the return value is (width of x).
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __cls, __clsl, __clsll¶
Signatures
unsigned int __cls(uint32_t x); unsigned int __clsl(unsigned long x); unsigned int __clsll(uint64_t x);
Description
Return the number of leading sign bits in x. If x == 0, then the return value is ((width of x) - 1).
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __rev, __revl, __revll¶
Signatures
uint32_t __rev(uint32_t x); unsigned long __revl(unsigned long x); uint64_t __revll(uint64_t x);
Description
Reverse the byte order within the argument x; return the result.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __rev16, __rev16l, __rev16ll¶
Signatures
uint32_t __rev16(uint32_t x); unsigned long __rev16l(unsigned long x); uint64_t __rev16ll(uint64_t x);
Description
Reverse the byte order within each 16-bit half-word of the input argument x; return the result. For example,
__rev16(0x12345678) -> 0x34127856 __rev16ll(0x1122334455667788) -> 0x2211443366558877
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __revsh¶
Signatures
uint16_t __revsh(uint16_t x);
Description
Reverse the byte order within the 16-bit input argument x; return the signed result.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __rbit, __rbitl, __rbitll¶
Signatures
uint32_t __rbit(uint32_t x); unsigned long __rbitl(unsigned long x); uint64_t __rbitll(uint64_t x);
Description
Reverse the bits within the input argument x; return the result.
Availability
Cortex-M0/M0+/R4/R5
2.9.1.2. 16-Bit Multiplication Intrinsics¶
- __smulbb¶
Signatures
int32_t __smulbb(int32_t x, int32_t y);
Description
result = (x & 0xffff) * (y & 0xffff)
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smulbt¶
Signatures
int32_t __smulbt(int32_t x, int32_t y);
Description
result = (x & 0xffff) * (y >> 16)
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smultb¶
Signatures
int32_t __smultb(int32_t x, int32_t y);
Description
result = (x >> 16) * (y & 0xffff)
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smultt¶
Signatures
int32_t __smultt(int32_t x, int32_t y);
Description
result = (x >> 16) * (y >> 16)
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smulwb¶
Signatures
int32_t __smulwb(int32_t x, int32_t y);
Description
result = (x * (int16_t)(y & 0xffff)) >> 16
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smulwt¶
Signatures
int32_t __smulwt(int32_t x, int32_t y);
Description
result = (x * (int16_t)(y >> 16)) >> 16
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
2.9.1.3. Saturating Intrinsics¶
- __ssat¶
Signatures
int32_t __smlawb(int32_t x, int32_t y, int32_t z);
Description Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __usat¶
Signatures
int32_t __smlawb(int32_t x, int32_t y, int32_t z);
Description Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __qadd¶
Signatures
int32_t __qadd(int32_t x, int32_t y);
Description
Add x and y with saturation; return result and set Q bit if the addition saturates.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __qsub¶
Signatures
int32_t __qsub(int32_t x, int32_t y);
Description
Subtract y from x with saturation; return result and set Q bit if the subtraction saturates.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __qdbl¶
Signatures
int32_t __qdbl(int32_t x);
Description
Add x to itself with saturation; return result if the addition saturates.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smlabb¶
Signatures
int32_t __smlabb(int32_t x, int32_t y, int32_t z);
Description
result = ((x & 0xffff) * (y & 0xffff)) + z
Set Q bit if addition overflows.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smlabt¶
Signatures
int32_t __smlabt(int32_t x, int32_t y, int32_t z);
Description
result = ((x & 0xffff) * (y >> 16)) + z
Set Q bit if addition overflows.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smlatb¶
Signatures
int32_t __smlatb(int32_t x, int32_t y, int32_t z);
Description
result = ((x >> 16) * (y & 0xffff)) + z
Set Q bit if addition overflows.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smlatt¶
Signatures
int32_t __smlatt(int32_t x, int32_t y, int32_t z);
Description
result = ((x >> 16) * (y >> 16)) + z
Set Q bit if addition overflows.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smlawb¶
Signatures
int32_t __smlawb(int32_t x, int32_t y, int32_t z);
Description
result = (x * (int16_t)(y & 0xffff)) + z
Set Q bit if addition overflows.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
- __smlawt¶
Signatures
int32_t __smlawt(int32_t x, int32_t y, int32_t z);
Description
result = (x * (int16_t)(y >> 16)) + z
Set Q bit if addition overflows.
Availability
Cortex-M0/M0+/M3/M4/M33/R4/R5
2.9.1.4. 32-Bit SIMD Intrinsics¶
Note
Data Types for 32-Bit SIMD Intrinsics
The <arm_acle.h> header file defines the following types:
typedef int32_t int8x4_t;
typedef int32_t int16x2_t;
typedef uint32_t uint8x4_t;
typedef uint32_t uint16x2_t;
These are used in the descriptions below to indicate that a 32-bit term in an arithmetic operation is being broken into 2 16-bit half-words or 4 8-bit bytes. In the intrinsic descriptions below, terms will refer explicitly to the bits from the 32-bit input argument or return value. For example,
result[16..31] = x[16..31] + (int16_t)y[16..23]
result[0..15] = x[0..15] + (int16_t)y[0..7]
indicates that the top 16-bits of x are added to the y[2] byte and the result is placed in the top 16-bits of the return value, while the bottom 16-bits of x are added to the y[0] byte and the result is placed in the bottom 16-bits of the return value (see the description of the __sctab16 intrinsic below).
- __ssat16¶
Signatures
int16x2_t __ssat16(int16x2_t x, unsigned int y);
Description
Saturate x[16..23] and x[0..15] to a bit width, y, in the range [1..16]. The Q bit is set if either operation saturates.
Availability
Cortex-M4/M33/R4/R5
- __usat16¶
Signatures
int16x2_t __usat16(int16x2_t x, unsigned int y);
Description
Saturate x[16..23] and x[0..15] to a bit width, y, in the range [0..15]. The input values are signed and the output values are non-negative, with all negative inputs going to zero. The Q bit is set if either operation saturates.
Availability
Cortex-M4/M33/R4/R5
- __sxtab16¶
Signatures
int16x2_t __sxtab16(int16x2_t x, int8x4_t y);
Description
result[16..31] = x[16..31] + (int16_t)y[16..23] result[0..15] = x[0..15] + (int16_t)x[0..7]
Availability
Cortex-M4/M33/R4/R5
- __sxtb16¶
Signatures
int16x2_t __sxtb16(int8x4_t x);
Description
result[16..31] = (int16_t)x[16..23] result[0..15] = (int16_t)x[0..7]
Availability
Cortex-M4/M33/R4/R5
- __uxtab16¶
Signatures
uint16x2_t __uxtab16(uint16x2_t x, uint8x4_t y);
Description
result[16..31] = x[16..31] + (uint16_t)y[16..23] result[0..15] = x[0..15] + (uint16_t)y[0..7]
Availability
Cortex-M4/M33/R4/R5
- __uxtb16¶
Signatures
uint16x2_t __uxtb16(uint8x4_t x);
Description
result[16..31] = (uint16_t)x[16..23] result[0..15] = (uint16_t)x[0..7]
Availability
Cortex-M4/M33/R4/R5
- __sel¶
Signatures
uint8x4_t __sel(uint8x4_t x, uint8x4_t y); uint16x2_t __sel(uint16x2_t x, uint16x2_t y);
Description
Selects each byte/half-word of the result from either x or y based on the values of the GE bits. For each byte, if the corresponding GE bit is set, then the byte from the first operand (x) is selected. If the corresponding GE bit is clear, then the byte from the second operand (y) is selected.
In the case of half-word operations, two GE bits are set/cleared per half-word operation, so the __sel* intrinsic can be used for either uint8x4_t or uint16x2_t type data.
Availability
Cortex-M4/M33/R4/R5
- __qadd8¶
Signatures
int8x4_t __qadd8(int8x4_t x, int8x4_t y);
Description
result[24..31] = x[24..31] + y[24..31] result[16..23] = x[16..23] + y[16..23] result[8..15] = x[8..15] + y[8..15] result[0..7] = x[0..7] + y[0..7]
Each signed addition result saturates to the range [-128..127].
Availability
Cortex-M4/M33/R4/R5
- __qsub8¶
Signatures
int8x4_t __qsub8(int8x4_t x, int8x4_t y);
Description
result[24..31] = x[24..31] - y[24..31] result[16..23] = x[16..23] - y[16..23] result[8..15] = x[8..15] - y[8..15] result[0..7] = x[0..7] - y[0..7]
Each signed subtraction result saturates to the range [-128..127].
Availability
Cortex-M4/M33/R4/R5
- __sadd8¶
Signatures
int8x4_t __sadd8(int8x4_t x, int8x4_t y);
Description
result[24..31] = x[24..31] + y[24..31] result[16..23] = x[16..23] + y[16..23] result[8..15] = x[8..15] + y[8..15] result[0..7] = x[0..7] + y[0..7]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __shadd8¶
Signatures
int8x4_t __shadd8(int8x4_t x, int8x4_t y);
Description
result[24..31] = (x[24..31] + y[24..31]) / 2 result[16..23] = (x[16..23] + y[16..23]) / 2 result[8..15] = (x[8..15] + y[8..15]) / 2 result[0..7] = (x[0..7] + y[0..7]) / 2
Availability
Cortex-M4/M33/R4/R5
- __shsub8¶
Signatures
int8x4_t __shsub8(int8x4_t x, int8x4_t y);
Description
result[24..31] = (x[24..31] - y[24..31]) / 2 result[16..23] = (x[16..23] - y[16..23]) / 2 result[8..15] = (x[8..15] - y[8..15]) / 2 result[0..7] = (x[0..7] - y[0..7]) / 2
Availability
Cortex-M4/M33/R4/R5
- __ssub8¶
Signatures
int8x4_t __ssub8(int8x4_t x, int8x4_t y);
Description
result[24..31] = x[24..31] - y[24..31] result[16..23] = x[16..23] - y[16..23] result[8..15] = x[8..15] - y[8..15] result[0..7] = x[0..7] - y[0..7]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __uadd8¶
Signatures
uint8x4_t __uadd8(uint8x4_t x, uint8x4_t y);
Description
result[24..31] = x[24..31] + y[24..31] result[16..23] = x[16..23] + y[16..23] result[8..15] = x[8..15] + y[8..15] result[0..7] = x[0..7] + y[0..7]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __uhadd8¶
Signatures
uint8x4_t __uhadd8(uint8x4_t x, uint8x4_t y);
Description
result[24..31] = (x[24..31] + y[24..31]) / 2 result[16..23] = (x[16..23] + y[16..23]) / 2 result[8..15] = (x[8..15] + y[8..15]) / 2 result[0..7] = (x[0..7] + y[0..7]) / 2
Availability
Cortex-M4/M33/R4/R5
- __uhsub8¶
Signatures
uint8x4_t __uhsub8(uint8x4_t x, uint8x4_t y);
Description
result[24..31] = (x[24..31] - y[24..31]) / 2 result[16..23] = (x[16..23] - y[16..23]) / 2 result[8..15] = (x[8..15] - y[8..15]) / 2 result[0..7] = (x[0..7] - y[0..7]) / 2
Availability
Cortex-M4/M33/R4/R5
- __uqadd8¶
Signatures
uint8x4_t __uqadd8(uint8x4_t x, uint8x4_t y);
Description
result[24..31] = x[24..31] + y[24..31] result[16..23] = x[16..23] + y[16..23] result[8..15] = x[8..15] + y[8..15] result[0..7] = x[0..7] + y[0..7]
Result of each unsigned addition saturates to the range of [0..0xff].
Availability
Cortex-M4/M33/R4/R5
- __uqsub8¶
Signatures
uint8x4_t __uqsub8(uint8x4_t x, uint8x4_t y);
Description
result[24..31] = x[24..31] - y[24..31] result[16..23] = x[16..23] - y[16..23] result[8..15] = x[8..15] - y[8..15] result[0..7] = x[0..7] - y[0..7]
Result of each unsigned subtraction saturates to the range of [0..0xff].
Availability
Cortex-M4/M33/R4/R5
- __usub8¶
Signatures
uint8x4_t __usub8(uint8x4_t x, uint8x4_t y);
Description
result[24..31] = x[24..31] - y[24..31] result[16..23] = x[16..23] - y[16..23] result[8..15] = x[8..15] - y[8..15] result[0..7] = x[0..7] - y[0..7]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __usad8¶
Signatures
uint32_t __usad8(uint8x4_t x, uint8x4_t y);
Description
result = abs(x[24..31] - y[24..31]) + abs(x[16..23] - y[16..23]) + abs(x[8..15] - y[8..15]) + abs(x[0..7] - y[0..7])
Availability
Cortex-M4/M33/R4/R5
- __usada8¶
Signatures
uint32_t __usada8(uint8x4_t x, uint8x4_t y, uint32_t z);
Description
result = abs(x[24..31] - y[24..31]) + abs(x[16..23] - y[16..23]) + abs(x[8..15] - y[8..15]) + abs(x[0..7] - y[0..7]) + z
Availability
Cortex-M4/M33/R4/R5
- __qadd16¶
Signatures
int16x2_t __qadd16(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] + y[16..31] result[0..15] = x[0..15] + y[0..15]
Result of each addition saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __qasx¶
Signatures
int16x2_t __qasx(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] + y[0..15] result[0..15] = x[0..15] - y[16..31]
Result of each operation saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __qsax¶
Signatures
int16x2_t __qsax(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] - y[0..15] result[0..15] = x[0..15] + y[16..31]
Result of each operation saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __qsub16¶
Signatures
int16x2_t __qsub16(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] - y[16..31] result[0..15] = x[0..15] - y[0..15]
Result of each subtraction saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __sadd16¶
Signatures
int16x2_t __sadd16(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] + y[16..31] result[0..15] = x[0..15] + y[0..15]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __sasx¶
Signatures
int16x2_t __sasx(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] + y[0..15] result[0..15] = x[0..15] - y[16..31]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __shadd16¶
Signatures
int16x2_t __shadd16(int16x2_t x, int16x2_t y);
Description
result[16..31] = (x[16..31] + y[16..31]) / 2 result[0..15] = (x[0..15] + y[0..15]) / 2
Availability
Cortex-M4/M33/R4/R5
- __shasx¶
Signatures
int16x2_t __shasx(int16x2_t x, int16x2_t y);
Description
result[16..31] = (x[16..31] + y[0..15]) / 2 result[0..15] = (x[0..15] - y[16..31]) / 2
Availability
Cortex-M4/M33/R4/R5
- __shsax¶
Signatures
int16x2_t __shsax(int16x2_t x, int16x2_t y);
Description
result[16..31] = (x[16..31] - y[0..15]) / 2 result[0..15] = (x[0..15] + y[16..31]) / 2
Availability
Cortex-M4/M33/R4/R5
- __shsub16¶
Signatures
int16x2_t __shsub16(int16x2_t x, int16x2_t y);
Description
result[16..31] = (x[16..31] - y[16..31]) / 2 result[0..15] = (x[0..15] - y[0..15]) / 2
Availability
Cortex-M4/M33/R4/R5
- __ssax¶
Signatures
int16x2_t __ssax(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] - y[0..15] result[0..15] = x[0..15] + y[16..31]
The GE bits are set according to the results.
Availability
Cortex-M4/M33/R4/R5
- __ssub16¶
Signatures
int16x2_t __ssub16(int16x2_t x, int16x2_t y);
Description
result[16..31] = x[16..31] - y[16..31] result[0..15] = x[0..15] - y[0..15]
The GE bits are set according to the results.
Availability
Cortex-M4/M33/R4/R5
- __uadd16¶
Signatures
uint16x2_t __uadd16(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] + y[16..31] result[0..15] = x[0..15] + y[0..15]
The GE bits are set according to the results.
Availability
Cortex-M4/M33/R4/R5
- __uasx¶
Signatures
uint16x2_t __uasx(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] + y[0..15] result[0..15] = x[0..15] - y[16..31]
Set GE bits according to the result of the unsigned addition.
Availability
Cortex-M4/M33/R4/R5
- __uhadd16¶
Signatures
uint16x2_t __uhadd16(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = (x[16..31] + y[16..31]) / 2 result[0..15] = (x[0..15] + y[0..15]) / 2
Availability
Cortex-M4/M33/R4/R5
- __uhasx¶
Signatures
uint16x2_t __uhasx(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = (x[16..31] + y[0..15]) / 2 result[0..15] = (x[0..15] - y[16..31]) / 2
Availability
Cortex-M4/M33/R4/R5
- __uhsax¶
Signatures
uint16x2_t __uhsax(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = (x[16..31] - y[0..15]) / 2 result[0..15] = (x[0..15] + y[16..31]) / 2
Availability
Cortex-M4/M33/R4/R5
- __uhsub16¶
Signatures
uint16x2_t __uhsub16(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = (x[16..31] - y[16..31]) / 2 result[0..15] = (x[0..15] - y[0..15]) / 2
Availability
Cortex-M4/M33/R4/R5
- __uqadd16¶
Signatures
uint16x2_t __uqadd16(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] + y[16..31] result[0..15] = x[0..15] + y[0..15]
Result of each addition saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __uqasx¶
Signatures
uint16x2_t __uqasx(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] + y[0..15] result[0..15] = x[0..15] - y[16..31]
Result of each operation saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __uqsax¶
Signatures
uint16x2_t __uqsax(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] - y[0..15] result[0..15] = x[0..15] + y[16..31]
Result of each operation saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __uqsub16¶
Signatures
uint16x2_t __uqsub16(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] - y[16..31] result[0..15] = x[0..15] - y[0..15]
Result of each subtraction saturates to the range [0..0xffff}.
Availability
Cortex-M4/M33/R4/R5
- __usax¶
Signatures
uint16x2_t __usax(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] - y[0..15] result[0..15] = x[0..15] + y[16..31]
Set GE bits according to the result of unsigned addition.
Availability
Cortex-M4/M33/R4/R5
- __usub16¶
Signatures
uint16x2_t __usub16(uint16x2_t x, uint16x2_t y);
Description
result[16..31] = x[16..31] - y[16..31] result[0..15] = x[0..15] - y[0..15]
Set GE bits according to the results.
Availability
Cortex-M4/M33/R4/R5
- __smlad¶
Signatures
int32_t __smlad(int16x2_t x, int16x2_t y, int32_t z);
Description
result = (x[0..15] * y[0..15]) + (x[16..31] * y[16..31]) + z
Set Q bit if addition overflows.
Availability
Cortex-M4/M33/R4/R5
- __smladx¶
Signatures
int32_t __smladx(int16x2_t x, int16x2_t y, int32_t z);
Description
result = (x[0..15] * y[16..31]) + (x[16..31] * y[0..15]) + z
Set Q bit if addition overflows.
Availability
Cortex-M4/M33/R4/R5
- __smlald¶
Signatures
int64_t __smlald(int16x2_t x, int16x2_t y, int64_t z);
Description
result = (x[0..15] * y[0..15]) + (x[16..31] * y[16..31]) + z
Availability
Cortex-M4/M33/R4/R5
- __smlaldx¶
Signatures
int64_t __smlaldx(int16x2_t x, int16x2_t y, int64_t z);
Description
result = (x[0..15] * y[16..31]) + (x[16..31] * y[0..15]) + z
Availability
Cortex-M4/M33/R4/R5
- __smlsd¶
Signatures
int32_t __smlsd(int16x2_t x, int16x2_t y, int32_t z);
Description
result = (x[0..15] * y[0..15]) - (x[16..31] * y[16..31]) + z
Set Q bit if the addition overflows.
Availability
Cortex-M4/M33/R4/R5
- __smlsdx¶
Signatures
int32_t __smlsdx(int16x2_t x, int16x2_t y, int32_t z);
Description
result = (x[0..15] * y[16..31]) - (x[16..31] * y[0..15]) + z
Set Q bit if the addition overflows.
Availability
Cortex-M4/M33/R4/R5
- __smlsld¶
Signatures
int64_t __smlsld(int16x2_t x, int16x2_t y, int64_t z);
Description
result = (x[0..15] * y[0..15]) - (x[16..31] * y[16..31]) + z
Availability
Cortex-M4/M33/R4/R5
- __smlsldx¶
Signatures
int64_t __smlsldx(int16x2_t x, int16x2_t y, int64_t z);
Description
result = (x[0..15] * y[16..31]) - (x[16..31] * y[0..15]) + z
Availability
Cortex-M4/M33/R4/R5
- __smuad¶
Signatures
int32_t __smuad(int16x2_t x, int16x2_t y);
Description
result = (x[0..15] * y[0..15]) + (x[16..31] * y[16..31])
Set Q bit if the addition overflows.
Availability
Cortex-M4/M33/R4/R5
- __smuadx¶
Signatures
int32_t __smuadx(int16x2_t x, int16x2_t y);
Description
result = (x[0..15] * y[16..31]) + (x[16..31] * y[0..15])
Set Q bit if the addition overflows.
Availability
Cortex-M4/M33/R4/R5
- __smusd¶
Signatures
int32_t __smusd(int16x2_t x, int16x2_t y);
Description
result = (x[0..15] * y[0..15]) - (x[16..31] * y[16..31])
Availability
Cortex-M4/M33/R4/R5
- __smusdx¶
Signatures
int32_t __smusdx(int16x2_t x, int16x2_t y);
Description
result = (x[0..15] * y[16..31]) - (x[16..31] * y[0..15])
Availability
Cortex-M4/M33/R4/R5
2.9.2. Custom Datapath Extension (CDE) Intrinsics¶
Some TI Arm Cortex-M33, M55, and M85 devices may be equipped with a coprocessor that can execute custom datapath extension (CDE) instructions via the use of CDE intrinsics.
To enable the use of CDE intrinsics in your C/C++ source file,
You should include the arm_cde.h header file in your compilation unit prior to any references to a CDE intrinsic. For example,
#include <arm_cde.h> void foo(void) { ... uint32_t = __arm_cx2a(10, 20, 30, 40); ... }
You must enable use of CDE intrinsics using a tiarmclang compiler command-line option.
The recommended way to enable use of CDE intrinsics on Coprocessor 0 is to append +cdecp0 to the -mcpu option argument, like so:
-mcpu=cortex-m33+cdecp0
Alternatively, the use of CDE intrinsics on Coprocessor 0 can also be anabled by specifying one of the following -march compiler options:
-march=thumbv8m.main+cdecp0
-march=thumbv8-m.main+cdecp0
-march=thumbv8.1m.main+cdecp0
-march=thumbv8.1-m.main+cdecp0
You should only enable CDE intrinsics on Coprocessor 0 if the target device is known to have a coprocessor unit on board.
Note
Selecting a Coprocessor for CDE
The tiarmclang compiler will parse and encode CDE intrinsic instructions for any coprocessor numbered 0 through 7. However, there are currently no TI Arm Cortex-M33, M55, or M85 devices that support CDE intrinsic instructions on coprocessors other than coprocessor 0.
This is why “+cdecp0” is used in the -mcpu and -march options specified above.
The available CDE intrinsics include the following:
uint32_t __arm_cxl(int, uint32_t);
uint32_t __arm_cx1a(int, uint32_t, uint32_t);
uint64_t __arm_cx1d(int, uint32_t);
uint64_t __arm_cx1da(int, uint64_t, uint32_t);
uint32_t __arm_cx2(int, uint32_t, uint32_t);
uint32_t __arm_cx2a(int, uint32_t, uint32_t, uint32_t);
uint64_t __arm_cx2d(int, uint32_t, uint32_t);
uint64_t __arm_cx2da(int, uint64_t, uint32_t, uint32_t);
uint32_t __arm_cx3(int, uint32_t, uint32_t, uint32_t);
uint32_t __arm_cx3a(int, uint32_t, uint32_t, uint32_t, uint32_t);
uint64_t __arm_cx3d(int, uint32_t, uint32_t, uint32_t);
uint64_t __arm_cx3da(int, uint64_t, uint32_t, uint32_t, uint32_t);
uint32_t __arm_vcx1_u32(int, uint32_t);
uint32_t __arm_vcx1a_u32(int, uint32_t, uint32_t);
uint64_t __arm_vcx1d_u64(int, uint32_t);
uint64_t __arm_vcx1da_u64(int, uint64_t, uint32_t);
uint32_t __arm_vcx2_u32(int, uint32_t, uint32_t);
uint32_t __arm_vcx2a_u32(int, uint32_t, uint32_t, uint32_t);
uint64_t __arm_vcx2d_u64(int, uint64_t, uint32_t);
uint64_t __arm_vcx2da_u64(int, uint64_t, uint64_t, uint32_t);
uint32_t __arm_vcx3_u32(int, uint32_t, uint32_t, uint32_t);
uint32_t __arm_vcx3a_u32(int, uint32_t, uint32_t, uint32_t, uint32_t);
uint64_t __arm_vcx3d_u64(int, uint64_t, uint64_t, uint32_t);
uint64_t __arm_vcx3da_u64(int, uint64_t, uint64_t, uint64_t, uint32_t);
Each of the CDE intrinsics is defined in arm_cde.h as a static inline function and implemented via a compiler runtime built-in function that is defined in the relevant version of the libclang_rt.builtins.a runtime library, which is included in the tiarmclang compiler tools installation.