2.1. Data Types¶
2.1.1. Scalar Data Types¶
The table below lists the size and range of each scalar type as supported in the tiarmclang compiler. Many of the minimum and maximum values for each range are available as standard macros in the C standard header file limits.h.
The storage and alignment of data types is described in Object Representation.
Type |
Size |
Min Value |
Max Value |
|---|---|---|---|
signed char |
8 bits |
-128 |
127 |
char, unsigned char, bool |
8 bits |
0 |
255 |
short, signed short |
16 bits |
-32768 |
32767 |
unsigned short |
16 bits |
0 |
65535 |
int, signed int, long, signed long |
32 bits |
-2147483648 |
2147483647 |
enum |
packed |
-2147483648 |
2147483647 |
unsigned int, unsigned long, wchar_t |
32 bits |
0 |
4294967295 |
long long, signed long long |
64 bits |
-9223372036854775808 |
9223372036854775807 |
unsigned long long |
64 bits |
0 |
18446744073709551615 |
float |
32 bits |
1.175494e-38 |
3.40282346e+38 |
double, long double |
64 bits |
2.22507385e-308 |
1.79769313e+308 |
pointers, references, data member ptrs |
32 bits |
0 |
0xFFFFFFFF |
Notes:
The “plain” char type has the same representation as either signed char or unsigned char. The -fsigned-char and -funsigned-char options control whether “plain” char is signed or unsigned. The default is unsigned.
The wchar_t type has the same representation as unsigned int. The tiarmclang runtime libraries do not support a 16-bit wchar_t type. Attempts to use the tiarmclang -fshort-wchar option may cause issues when linked with the tiarmclang runtime libraries.
Further discussion about the size of enum types can be found below in the Enum Type Storage.
Specified minimum values for floating-point types in the table above indicate the smallest precision value > 0.
Negative values for signed types are represented using two’s complement.
64-bit data types are aligned to 64-bit (8-byte) boundaries.
Both 32-bit pointers and 64-bit pointers are aligned to 32-bit (4-byte) boundaries.
Arm Cortex-M type processor variants supported by the tiarmclang compiler are little-endian. Arm Cortex-R type processor variants supported by the tiarmclang compiler may be big-endian or little-endian depending on the use of command-line options.
2.1.2. Enum Type Storage¶
The type of the storage container for an enumerated type is the smallest integer type that contains all the enumerated values. The container types for enumerators are shown in the following table:
Lower Bound Range |
Upper Bound Range |
Enumerator Type |
|---|---|---|
0 to 255 |
0 to 255 |
unsigned char |
-128 to 1 |
-128 to 127 |
signed char |
0 to 65535 |
256 to 65535 |
unsigned short |
-128 to 1,
-32768 to -129
|
128 to 32767,
-32768 to 32767
|
signed short |
0 to 4294967295 |
2147483648 to 4294967295 |
unsigned int |
-32768 to -1,
-2147483648 to -32769,
0 to 2147483647
|
32767 to 2147483647,
-2147483648 to 2147483647,
65536 to 2147483647
|
signed int |
The compiler determines the type based on the range of the lowest and highest elements of the enumerator.
For example, the following code results in an enumerator type of int:
enum COLORS {
green = -200,
blue = 1,
yellow = 2,
red = 60000
};
The following code results in an enumerator type of short:
enum COLORS {
green = -200,
blue = 1,
yellow = 2,
red = 30000
};
2.1.3. Enum Type Size¶
An enum type is represented by an underlying integer type. The size of the integer type and whether it is signed is based on the range of values of the enumerated constants.
By default, the tiarmclang uses the smallest possible byte size for the enumeration type. The underlying type is the first type in the following list in which all the enumerated constant values can be represented: signed char, unsigned char, short, unsigned short, int, unsigned int, long, unsigned long, long long, unsigned long long. This default behavior is equivalent to the effect of using the tiarmclang -fshort-enums option.
In strict c89/c99/c11 mode, the compiler will limit enumeration constants to those values that fit in int or unsigned int.
For C++ and gnuXX C dialects (relaxed c89/c99/c11), the compiler allows enumeration constants up to the largest integral type (64 bits).
You can alter the default compiler behavior using the -fno-short-enums option. When the -fno-short-enums option is used in strict c89/c99/c11 mode, the enumeration type used to represent an enum will be int, even if the values of the enumeration constants fit into a smaller integer type.
When the fno-short-enums option is used with C++ or gnuXX C dialects, the underlying enumeration type will be the first type in the following list in which all the enumerated constant values can be represented: int, unsigned int, long, unsigned long, long long, unsigned long long.
The following enum uses 8 bits instead of 32 bits by default (since -fshort-enums option behavior is in effect):
enum example_enum {
first = -128,
second = 0,
third = 127
};
The following enum fits into 16 bits instead of 32 by default:
enum a_short_enum {
bottom = -32768,
middle = 0,
top = 32767
};
Note
Do not link object files compiled with the -fno-short-enums option with object files that were compiled without it. If you use the -fno-short-enums option, you must use it with all of your C/C++ files; otherwise, you will encounter errors that cannot be detected until run time.