6.4.4. List of importProject Options¶
Note that the available options can vary depending on the Code Composer Studio™ version used. For the list of options available for your specific Code Composer Studio version, run the command with the '-ccs.help' option:
ccs-server-cli -noSplash -workspace "<workspace_dir>" -application com.ti.ccs.apps.projectImport -ccs.help
Full list of projectImport options:
-ccs.location <path>
    Absolute or relative path to the location containing the project.
    Relative paths will be assumed to be relative to the working directory.
-ccs.device <id>
    The device-variant ID. Applicable only when '-ccs.location' flag resolves to a .projectspec file.
-ccs.definePathVariable <name> <value> [@scope (global|project)]
    Defines the given path-variable for resolving portable linked file paths (optional)
    (also defines a global build-macro with the same name and value).
    Optionally, specify the scope (defaults to 'global').
-ccs.copyIntoWorkspace
    Copy project folder and contents into the workspace directory (optional).
    Defaults to 'false'.
-ccs.overwrite
    Forces overwrite of existing file-system resources (optional).
-ccs.renameTo
    Rename the imported project to the specified name.
-ccs.autoBuild
    Performs an incremental build on the imported/created project (optional).
-ccs.autoImportReferencedProjects
    If 'true', an attempt is made to automatically import any referenced projects found in the same parent directory as the main project.
-ccs.autoRenameReferencedProjects
    If 'true', and iff the '-ccs.renameTo' flag is present, any imported referenced projects will also be renamed automatically.
-ccs.referencedProjectSearchDirectory
    Directory to search for referenced projects. Applicable only when '-ccs.autoImportReferencedProjects' flag is present.
-ccs.captureCopiedFileOrigins
    Capture the original locations of all resources copied into the project during the import. These will be captured into a text file named 'copiedFileOrigins.txt'.
-ccs.captureProjectspecApplicability
    Capture the list of devices that the imported projectspec is applicable to. These will be captured into a text file named 'projectSpecApplicability.txt'.
-ccs.args <file>
    File containing any extra arguments (optional).
-ccs.help
    Print this help message.