7.9.8.72. GEL_SharedMemHaltOnStepOn

Affected cores are halted when a breakpoint in shared memory is stepped over.

Syntax

GEL_SharedMemHaltOnStepOn( void );

Parameters

None

Description

Multiple cores on a single processor can share a block of memory. When stepping over a software breakpoint that is set in a shared memory block, the breakpoint is first cleared, then the code is stepped, and finally the breakpoint is reset. If other cores execute code in that memory block during this time, they will miss the breakpoint. This function specifies that all cores with executable code on that block are halted until the breakpoint has been stepped over.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_SharedMemHaltOnStepOn();

Related Topics

GEL_SharedMemHaltOnStepOff

GEL_SharedMemHaltOnWriteOff

GEL_SharedMemHaltOnWriteOn