7.9.8.9. GEL_BreakPtDisable

Disables a software breakpoint at the specified address.

Format

GEL_BreakPtDisable(address);

Parameters

address specifies the location of the software breakpoint.

Description

The software breakpoint at the specified address is disabled. If the breakpoint does not exist or is already disabled, no action is taken. This function will not disable the breakpoint if it is a hardware breakpoint.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

GEL_BreakPtDisable(0x2000);

GEL_BreakPtDisable(main + 100);

Related Topics

GEL_BreakPtAdd

GEL_BreakPtDel

GEL_BreakPtDisable

GEL_ClearProfileConfiguration