7.9.8.30. GEL_IsHalted

GEL built-in function that can be called at any time to determine if the target is halted.

Syntax

GEL_IsHalted()

Parameters

None

Description

The function returns 1 if the target is halted and returns 0 otherwise.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Related Topics