7.9.8.98. OnFileLoaded()

GEL callback function called after a program is loaded.

Syntax

OnFileLoaded( int nErrorCode, int bSymbolsOnly );

Parameters

nErrorCode: 0 (zero) indicates success.

bSymbolsOnlyBoolean indicates if only symbols were loaded.

Description

If defined in a loaded GEL file, OnFileLoaded() is called after a program is loaded.

Example

OnFileLoaded(int nErrorCode, int bSymbolsOnly)
{
if (nErrorCode)
GEL_TextOut(“An error occurred while loading a file. -%d-n”,,,,, ErrorCode);
else
GEL_TextOut(“File was loaded successfully. -%d-n”,,,,, nErrorCode);
if (bSymbolsOnly)
GEL_TextOut(“Only symbols were loaded.n”);
else
GEL_TextOut(“Full load.n”);
}