7.9.8.61. GEL_RemoveOutputFile()¶
Removes the output file from the breakpoint at the specified address.
Syntax
GEL_RemoveOutputFile(programAddr, “connectFileName”);
Removes the output file from the breakpoint in the specified file.
Syntax
GEL_RemoveOutputFile(“srcFileName”, lineNumber, “connectFileName”);
Parameters
programAddr: is an expression specifying the memory location of the breakpoint to be removed. This expression should not be enclosed in quotation marks.
srcFileName: is a string value specifying the filename (without path) of the source file in which the breakpoint to be removed is located. A double backslash escape sequence is required to ensure that a backslash is inserted into the filename; for example: “c:\ti\myprojects\sine.dat”
lineNumber: is a long integer value specifying the line number in said file at which the breakpoint to be removed is located.
connectFileName: is a string value specifying the full path and filename of the file connected with the breakpoint. This connection will be severed and the file closed. A double backslash escape sequence is required to ensure that a backslash is inserted into the filename; for example: “c:\ti\myprojects\sine.dat”
Description
This function disconnects the specified file from the appropriate breakpoint, puts the corresponding output FileI/O object into the Stopped state, closes the output file, and removes the breakpoint (whether or not it was originally added by a call to GEL_AddOutputFile).
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Related Topics